FPC PCB Manufacturing: How to Choose the Right FPC Parameters for Optimal Performance
5 min
- What Are FPC Parameters?
- Key Factors to Consider When Choosing FPC Parameters
- Common Processes
What Are FPC Parameters?
FPC flexible printed circuit boards parameters refer to the specific design and material choices that define the performance and functionality of a flexible printed circuit. These parameters include material selection, thickness, layer count, bend radius, and more. Properly selecting these parameters ensures that the FPC meets the requirements of its intended application.
Key Factors to Consider When Choosing FPC Parameters
Board Quantity/Board Size
Board size refers to the dimensions of the board. The maximum size for JLC FPC boards is 234X490mm (limit 250X500mm), while the minimum size is not restricted. However, for sizes smaller than 20X20mm, panelization is recommended.
Number of Layers
The number of layers is generally determined during design, so you can directly select the required number of layers based on design specifications.
FPC boards can be classified into single-layer, double-sided, and multi-layer boards.
- Single-layer boards are the simplest flexible boards and are commonly used in industrial control and electronic instruments.
- Double-sided boards differ from single-layer FPCs by incorporating vias to connect two copper layers, forming electrical pathways. They are typically used in mobile phones, automotive dashboards, and similar products.
- Multi-layer boards consist of multiple single or double-sided FPCs laminated together. Through drilling and plating, they form metallized vias to create electrical pathways between layers. These are commonly used in high-end consumer electronics like smartphones.
Common Processes
Solder Mask Color
- FPC solder masks come in yellow, black, and white. Yellow is recommended.
- Yellow film is suitable for most products, such as various types of flexible ribbon cables.
- Black film is commonly used in high-end applications or products requiring light absorption, such as automotive, mobile phones, and LED displays.
- White film has an additional white coating and is often used in reflective products like lighting equipment, LED displays, and medical beauty devices.
Board Thickness
Board thickness refers to the thickness of the FPC flexible board itself, excluding reinforcement thickness.
If the measured area has no copper or coverlay, the final thickness may be reduced.
If a white coverlay is used, the thickness increases by 18um for single-sided boards and 36um for double-sided boards.
Copper Foil Thickness
This refers to the thickness of the copper foil in the FPC circuit layer, which should match the board thickness.
- Available options for single-sided boards: 18um (0.5oz), 35um (1oz)
- Available options for double-sided boards: 12um (0.33oz), 18um (0.5oz), 35um (1oz)
Minimum Line Width/Spacing
The smaller the width/spacing, the higher the difficulty. The general recommendation is 3/3mil or above.
JLC's limit is around 2/2mil, but it is recommended to avoid designing at this limit.
Minimum Via/Pad
The via outer diameter must be at least 0.2mm larger than the inner diameter, with a recommended margin of 0.25mm or more.
In general, the smaller the via, the more expensive it is. Recommended via inner diameter: 0.3mm, outer diameter: 0.55mm.
Solder Mask Covering
FPC uses a coverlay as the solder mask layer. There are two main types of solder mask coverage: via opening and via tenting.
- Via opening: The via pad is exposed in the final board. However, exposed vias in FPC may cause oxidation and copper fracture.
- Via tenting: The via pad is covered with solder mask to protect the copper from oxidation and to prevent copper fracture during bending. JLC defaults to via tenting. If via opening is required, it must be specifically noted when placing an order.
Minimum Solder Mask Bridge Width
The minimum solder mask bridge width is 0.5mm. That is, pad spacing must be ≥0.5mm to retain the bridge. If the spacing is smaller, JLC will default to exposing the vias.
There are five main types of reinforcement: PI, FR4, steel sheet, 3M double-sided adhesive, and electromagnetic shielding film.
- PI reinforcement is commonly used for gold finger insertion products.
- FR4 is used for reinforcing component hole areas.
- Steel sheet is more expensive but has excellent flatness and does not deform, making it suitable for products requiring chip mounting (since steel sheets have weak magnetism, they are not recommended for products like Hall sensors).
- 3M adhesive is generally used for fixing FPC boards during assembly.
- Electromagnetic shielding film is used to solve EMC issues. It is generally recommended to add grounding openings in the solder mask layer to connect the shielding film to the ground copper, enhancing shielding effectiveness. (Note: Prototype verification is required first, as the shielding film significantly impacts impedance. Improper design may lead to signal abnormalities.)
Total reinforcement thickness = FPC board thickness + reinforcement thickness, but it is not a direct sum. Solder mask thickness and whether the backside of gold fingers has copper must also be considered.
If you don't know how to calculate reinforcement thickness, click the link below to use the Reinforcement Thickness Calculator: https://jlcpcb.com/gold-fingers-PI-thickness
Panelization
The maximum panel size is 234X490mm.
Recommended spacing: 2mm; if steel sheet reinforcement is used, spacing should be 3mm.
Important! Many FPC board outlines are irregularly shaped. Improper panelization may reduce material utilization, increase costs, and complicate production. If you are unsure about panelization, JLC engineers can assist.
In addition to the above standard parameters, FPC production also involves gold fingers, impedance, half-cut holes, and other processes.
Choosing the right FPC parameters is essential for manufacturing high-quality, reliable, and cost-effective flexible printed circuits. By considering factors such as material selection, thickness, bend radius, and thermal performance, you can design FPCs that meet the demands of your application. Whether you're working on consumer electronics, automotive systems, or medical devices, understanding FPC parameters will help you achieve optimal results.
Keep Learning
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......
Polyimide Flex PCB: A Complete Guide for Engineers
A polyimide flex PCB can be folded about 285,000 times when the base film is 25 µm (1 mil) thick. Make that film 75 µm (3 mil), and the same MIT fold test gives up near 6,000 cycles. Bending is a strain problem, not a material problem. Copper sits above the center of the stack, so a bend forces it to stretch around the longer outer path. Figure 1: A polyimide flex circuit folded tight, with a stiffener holding the connector A thicker stack places the copper farther out, resulting in more stretch at th......
Flex PCB Bend Radius: Calculation, Minimum Radius & Design Guidelines
Flex PCB bend radius is the one dimension on an FPC that no design rule check will catch. Bend the circuit tighter than its material allows; the outer copper stretches from its elongation limit, and then it cracks. Figure 1: A flex circuit formed around a mandrel, with bend radius and stack thickness A flex circuit bends around a neutral axis near the middle of its stack. Copper below that line is squeezed, and copper above it is pulled. So the further a layer sits from the line, the harder it is to w......
FPC vs FFC: Understanding the Key Differences Between Flexible Circuit Technologies
The FPC vs FFC decision is really a question about how the copper was made. An FFC consists of flat copper strips laminated between two PET films. Every conductor runs straight from end to end at one fixed pitch, because nothing in that process can make a trace turn or branch. An FPC starts as copper-clad polyimide and is etched exactly like a rigid board. Traces can turn, taper, split onto a second layer, and land under a soldered component. The finished circuit can be as thin as 0.1 mm (4 mil). Figu......