JLCPCB helps simulate rockets to realize precise flight control!
4 min
- Application function
- Design challenges
- How JLCPCB helped
- Conclusion
Beepy is a flight computer specially designed for model rockets. The model rocket is very small in size, but the amount of computation required to achieve its flight is considerable. Beepy differs from traditional flight computers in that it adopts a design where multiple circular PCBS are stacked and connected, and uses ribbon cables to link each module together. This design significantly reduces the space occupied by the flight computer, enabling the device to maintain powerful functions while keeping a compact size. Through such meticulous and unique design and by choosing the reliable PCB manufacturing supplier JLCPCB, Beepy successfully achieved this goal, ensuring the precise flight control of the model rocket.
PCB design diagram of the flight computer
Application function
Beepy consists of 4 circular 4-layer PCBS with a radius of 25mm, connected by mousebites. The size of it is 100x100mm, and connected via 3d printed connections/structure. The main function of Beepy is to guide the model rocket's flight and provide active stability during the flight. Meanwhile, Beepy also integrates a motor driver, which can control the rocket's roll through a flywheel. The versatility of Beepy enables it not only to function as a flight computer but also to be connected to a laptop as a ground station or as a control computer for a launch pad.
Design challenges
During the design process, connecting multiple PCBS and effectively implementing RF modules is a huge challenge. As the design of RF modules requires extensive professional knowledge and is often a technical challenge, the Beepy team overcame this difficulty through precise design and optimization, successfully integrating the RF module. Finally, the online gerber file verification function of JLCPCB was used to ensure the stability and reliability of the flight computer.
How JLCPCB helped
In this project, JLCPCB's precise,rapid manufacturing and considerate service played a crucial role, enabling the team to complete the development with high efficiency and implement the project with high quality.
1.Precision manufacturing that keeps the stack compact and stable
Beepy’s each stacked, circular 4-layer PCBs has a radius of 25 mm and is routed from a 100 × 100 mm panel. JLCPCB’s routing and mouse-bite tabbing produced clean round edges and consistent tab spacing.so the physical stack matched the engineers’ mechanical layout and the ribbon-cable interconnects could be assembled as intended.
2.Fast fabrication that accelerates iteration and verification
JLCPCB’s rapid fabrication can be as fast as 48 hours and global logistics net work that typically arrive 2–4 days sooner than local alternatives. After created the PCB order on JLCPCB official website,the team received fresh prototypes for bench tests quickly, which shortened the build–test–refine cycle and allowed the team to run multiple hardware iterations within their planned test schedule.
3.Practical verification tools and accessible support
The team used JLCPCB’s online Gerber verification to check files before ordering. Combined with JLCPCB's 24 hours online customer service and order-status check tool through the online dashboard/tracking,JLCPCB provides the team with sufficient information reference and assistance.
Conclusion
The innovative flight computer project Beepy demonstrates the reliable service of PCBS in miniaturized and multi-functional design. The project was efficiently implemented through the high-quality manufacturing and rapid delivery of JLCPCB. As a globally leading PCB manufacturer, JLCPCB is always committed to providing makers, engineers and enterprises with high cost-performance, fast and reliable services - from the super value price of 1 to 4-layer boards starting at 2 US dollars, 24-hour online customer service, to a powerful logistics network covering more than 180 countries around the world. In the future, JLCPCB will continue to assist more innovative projects in accelerating their realization, turning ideas into reality more quickly.
Popular Articles
• ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
• From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
• Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
• PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
• Premium Portable Speaker Built with 8-Layer PCBs, DSP & Smart Amps
Keep Learning
From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
Note Motivation: Replaced a dust-prone membrane keyboard with a durable, custom DIY alternative. Specs: 87-key TKL layout powered by Raspberry Pi Pico (RP2040), featuring hot-swap support, QMK, OLED, and an encoder. Design: A unique 3-layer PCB stack featuring symmetrical routing, an exposed controller, and visible "diode art". Support: Designed using EasyEDA and fabricated by JLCPcB, the project was submitted to the EasyEDA Spark program successfully securing parts and materials sponsorship for its d......
Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
In the world of FPGA development, having a reliable, low-cost JTAG programmer used to mean either buying expensive vendor cables or adding high-cost FTDI chips to every board. Maker Khaled Magdy changed that by turning a $4 Raspberry Pi Pico into a fully functional JTAG adapter using DirtyJTAG firmware and OpenFPGALoader — then had his custom FPGA boards professionally assembled by JLCPCB. The entire solution is 100% open-source. You can download the firmware, follow the Windows installation steps, an......
ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
Key Takeaways Accessible Design: ANGELO is an open-source €10 listening aid created to assist everyday voice amplification. Analog Audio Architecture: Uses a TL072 op-amp to boost speech frequencies (1–4 kHz) with low latency and low power. EasyEDA & JLCPCB Workflow: Designed in EasyEDA and produced via JLCPCB SMT assembly for fast, reliable hardware execution. The ANGELO Project Overview ANGELO is an open-source audio hardware project designed to amplify voices and improve everyday communication expe......
Athena: Building a High-Performance 6-Layer PCB for Rocket Avionics
Key Takeaways Athena is an open-source flight computer with a triple-MCU architecture, redundant sensors, and multiple communication interfaces on a compact 6-layer PCB. The 80 × 140 mm board integrates three STM32 MCUs, three IMUs, barometers, GNSS, LoRa, Bluetooth, CAN, USB, flash storage, SD card, and power management. The 6-layer PCB provides routing capacity, organized power distribution, signal organization, and compact functional integration for this complex design. The project demonstrates how......
PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
Key Takeaways The piBrick Pocket-CM5 is a fully functional, smartphone-sized Raspberry Pi CM5 handheld PC with a physical QWERTY keyboard, AMOLED display, and M.2 NVMe SSD The project utilizes JLCPCB's 4-layer PCB fabrication with controlled impedance (90-ohm for USB, 100-ohm for PCIe/MIPI DSI) to maintain signal integrity Designed using EasyEDA and fabricated by JLCPCB, the project was submitted to the EasyEDA Spark program, successfully securing parts and materials sponsorship for its development. J......
Designing a Precision 72-LED Wearable Watch: Building a 40mm Round PCB with JLCPCB SMT Assembly
Key Takeaways This case study explores the design and fabrication of a 72-LED wearable watch built on a precision 40mm round PCB. Learn how JLCPCB SMT assembly eliminated hand-soldering 70+ 0603 LEDs, how ENIG surface finish ensures reliability in wearable applications, and how a clever panelization strategy with mouse-bite breakaway tabs enabled automated assembly of a circular board. The project demonstrates a complete workflow from EasyEDA schematic capture to firmware optimization and commercial-g......