Flex PCB Manufacturing Process: From Prototyping To Mass Production
7 min
- Application of Flex PCBs:
- Manufacturing Steps Of Flex PCBs :
- Detailed Manufacturing Process
- Transition to Mass Production :
- FAQ about Flex PCB Manufacturing
- Conclusion :
Flexible Printed Circuit Board commonly known as flex PCBs are a revolutionary step in modern electronics that offer compact, lightweight, dynamic and precise designs. Flex PCBs are designed to bend, twist, and fold, which rigid boards are incapable of. These characteristics have led to their widespread adoption in industries like wearable technology to consumer electronics to aerospace and medical technologies.
With demands increasing day by day for miniaturized and ergonomic product designs, understanding the process of a flex PCB from its prototyping phase to mass production has become a must. In this article the journey of a flex PCB from prototype to mass production will be covered.
Application of Flex PCBs:
The rise of flex PCBs is because of their versatility. They're mostly used in -
● Medical Devices: Pacemaker, Cochlear implants and Wearable diagnostics.
● Consumer Electronics: Smartphones, Foldable Screens and Fitness bands and so on.
● Automotive Systems : Airbag Controllers, Dashboard interfaces and sensors.
● Aerospace: Satellite, Avionics and high reliability communication systems.
Manufacturing Steps Of Flex PCBs :
Flex PCB manufacturing is almost similar to the traditional PCB manufacturing process but here the use of specialized materials and procedures are needed to ensure flexibility, durability and quality control. Here are the steps to do this right-
Flex PCB Core Capability Parameters:
| Process Item | JLCPCB Standard Capability |
|---|---|
| Layer Count | 1-Layer / 2-Layer |
| Base Material | Polyimide (PI) |
| Base PI Thickness | 12.5um / 25um |
| Finished Thickness | 0.07mm / 0.11mm / 0.12mm / 0.20mm |
| Copper Weight | 1/3 oz (12um) / 0.5 oz (18um) / 1 oz (35um) |
| Min Trace Width/Spacing | 0.075mm / 0.075mm |
| Surface Finish | Electroless Nickel Immersion Gold (ENIG - Default) |
| Coverlay Color | Yellow / Black / White |
| Stiffener Material | Polyimide (PI) / FR4 / Stainless Steel |
| Min Drilling Hole Size | Mechanical Drilling: 0.2mm / Laser Drilling: 0.1mm |
1. Material Selection: The most suitable base substrate is Polyimide. It is chosen because of its top notch thermal stability and amazing flexibility. It is actually copper-clad on one or both sides, depending on requirements.
2. Cleaning and Preparation : The copper-clad polyimide is thoroughly cleaned to remove oxidation and contaminants before proceeding to the next step.
3. Photo Imaging and Patterning : The Copper surface is laminated with a Photoresist . A UV light source projects the circuit pattern into a photomask which hardens the exposed areas.
4. Etching and Stripping : The unwanted copper is etched away, and the remaining photoresist is stripped, leaving only the designed circuit traces.
5. Drilling and Plating : In multilayer designs precise drilling is performed then the vias are plated with copper to create electrical connection between layers.
6. Coverlay Application : Here a coverlay made of Polyimide and adhesive is applied to protect the circuit. It's laminated and cured to bond securely with substrate.
7. Surface Finish: Immersion Silver or OSP or ENIG surface finish is applied to prepare the pads for soldering this also protects the exposed copper from oxidation.
8. Laser or Die Cutting : The board outline is cut using laser for precision.
9. Electrical Testing : Automated test equipment ensures that all traces and vias are correctly placed and checks for violations.
10. Inspection and Quality Control : The board now undergoes flex testing and visual inspection according to industry standards.
Detailed Manufacturing Process
Material Cutting & Pre-treatment
The production begins with cutting advanced roll-based flexible copper-clad laminates (FCCL), typically consisting of polyimide film base bonded with copper foil (0.5 oz or 1 oz). JLCPCB uses adhesive-less base materials to ensure thinner profiles and superior thermal stability during lead-free soldering.
CNC Drilling & Automated Copper Plating
Micro-vias are drilled using high-speed mechanical CNC drilling machines operating at up to 200,000 RPM, or advanced UV lasers for high-density interconnect (HDI) designs. To establish electrical continuity between layers, specialized roll-to-roll or vertical conveyorized plating systems deposit a uniform layer of copper inside the drilled vias.
Photolithography & Etching
A photosensitive dry film (photoresist) is laminated onto the cleaned copper surfaces under heat and pressure. Using Laser Direct Imaging (LDI) technology, the precise circuit pattern is digitally exposed via UV light, hardening the trace areas. The unexposed film is developed away, and the board passes through a high-precision acid etching chemical line to remove unwanted copper, perfectly forming traces down to 0.05mm/0.05mm width/spacing.
Coverlay Alignment & Vacuum Lamination
Unlike rigid PCBs that use liquid photoimageable solder mask, flex PCBs require a solid coverlay (a combination of polyimide film and thermo-setting acrylic adhesive) to protect the delicate copper traces from oxidation and dynamic bending fatigue. Openings for SMT pads are pre-cut via CNC laser, aligned precisely over the circuit, and bonded using high-temperature industrial vacuum presses to eliminate air traps.
Surface Finish & Stiffener Application
Electroless Nickel Immersion Gold (ENIG) is applied as the standard surface finish at JLCPCB. This provides a perfectly flat surface for fine-pitch SMT components and excellent shelf life. Following this, FR4, PI, or Aluminum stiffeners are precisely bonded to the designated areas (such as underneath ZIF connectors or heavy components) using thermosetting or pressure-sensitive tape to provide localized rigidity.
Laser Contour Cutting & 100% Electrical Test
Individual boards are profiled out of the panels using precise UV Laser Cutting machines, which prevent any mechanical stress or delamination at the flexible edges. Finally, 100% Flying Probe or dedicated fixture Electronic Testing is executed alongside Automated Optical Inspection (AOI) to guarantee zero open or short circuit defects before shipping.
Transition to Mass Production :
Once the prototypes are done and pass all performance and durability tests the product then goes into mass production.
Steps in Mass Production :
1. Design Freeze: Lock in all specifics after rigorous testing and stakeholder approval.
2. Tooling Setup: Create precise stencils for high speed fabrication and assembly.
3. Process Optimization: Fine tune lamination, drilling and plating processes for volume efficiency.
4. Quality Control Scaling: Implement in line testing and automated visual inspection.
5. Planning: Coordinate supply of polyimide, adhesive and finishes.
FAQ about Flex PCB Manufacturing
Q: What is the main difference between the materials used in rigid PCBs and Flex PCBs?
Rigid PCBs primarily use FR4 (fiberglass and epoxy resin) as the rigid substrate. In contrast, Flex PCBs use Polyimide (PI) as the base material, which provides excellent thermal stability, electrical insulation, and the ability to bend and twist dynamically.
Q: Does JLCPCB use adhesive or adhesive-less base materials for FPC production?
JLCPCB utilizes premium adhesive-less base materials (FCCL) for flexible PCBs. This ensures a thinner overall profile, superior flexibility, and better thermal stability to prevent delamination during high-temperature lead-free reflow soldering.
Q: What coverlay options and colors are available at JLCPCB?
Coverlay serves as the flexible equivalent of a rigid board's solder mask. JLCPCB offers standard solid polyimide coverlays in three colors: Yellow (standard), Black, and White, protecting the underlying copper traces from oxidation and dynamic bending fatigue.
Q:Why are stiffeners added to flexible PCBs, and what types does JLCPCB support?
Stiffeners are added to provide localized rigidity in areas that require mechanical strength, such as underneath heavy SMT components or ZIF connectors. JLCPCB supports three primary stiffener materials: Polyimide (PI), FR4, and Stainless Steel.
Q: What are the minimum trace width and drilling hole limits for JLCPCB's Flex PCB process?
To ensure excellent manufacturing yield and stability, JLCPCB's flexible PCB process supports a minimum trace width and spacing of 0.075mm / 0.075mm, and a minimum mechanical drilling hole size of 0.2mm.
Conclusion :
Flex PCBs are an indispensable part of modern electronics enabling innovation across diverse sectors. Their ability to combine flexibility, durability and compact design unlocks new possibilities for product engineers and system designers.
From the initial stages of design and prototyping to the demands of high volume manufacturing each step of the flex PCB process requires precision, expertise and careful coordination. By understanding the intricacies of the flex PCB manufacturing process, organizations can harness the full potential of this powerful technology and bring next generation products to life faster, smaller and smarter than ever before.
Keep Learning
Best Flex PCB Design Software: CAD Tools & Setup Guide
The right flex PCB design software would rely on the complexity and construction of your circuit. Altium Designer, Cadence Allegro X, OrCAD X, and Siemens Xpedition are professional tools that offer advanced capabilities for flexible and rigid-flex PCB designs, such as stackup management, bend regions, and mechanical constraints. In the meantime, for more basic flexible circuits, tools such as KiCad or EasyEDA Pro might be viable options, though they may require some manual setup and verification. Fle......
Custom FPC Fabrication: Design Rules & Manufacturing Guide
Custom FPC fabrication is the process of making flexible printed circuits in accordance with a customer's design requirements, such as board outline, layer stackup, copper thickness, openings for coverlay, and stiffener placement. Custom flexible circuits differ from traditional rigid PCBs in that they must be carefully designed and planned for materials and layout to meet flexibility and stress requirements and to fit into smaller assemblies. These design decisions are directly related to manufactura......
Polyimide Flexible PCB Fabrication: Materials and Process Guide
Polyimide flexible PCB fabrication is a process of creating thin polyimide film and copper-foil-based circuits that will bend, fold, and withstand soldering temperatures. But the same flexibility that comes from the thin film material used on these boards, and which is sensitive to moisture, makes production slightly more difficult than rigid PCBs. Polyimide can expand or contract during processing, absorb moisture before reflow soldering, and suffer from copper fatigue or cracking if the bend radius ......
Flexible PCB Price: Key Cost Factors and Ways to Save
The price of a flexible PCB has no single fixed figure, as it depends mainly on the panel area occupied by the design, the number of copper layers, and the order quantity. Other features such as stiffeners, EMI shielding film, tight outline tolerance, and a complex via structure may further increase manufacturing costs. The majority of these cost factors are fixed by the PCB layout stage, and even at the time of the first quotation. Figure: Polyimide flexible PCB with ENIG contact pads and a bonded st......
Flex PCB Design Guide: Preventing Mechanical Failures
Key Takeaways Reliable flex PCB design requires more than electrical performance. Proper bend radius control, trace routing, via placement, stiffener selection, and DFM considerations are essential to prevent mechanical failures such as copper cracking and delamination. By following proven flexible PCB design practices, engineers can improve durability and achieve reliable production results with JLCPCB. Ever wonder how the circuit in a foldable phone, fitness tracker, or camera module manages to rema......
FPC Electronics: What Is It, How It Works, Applications, and Benefits
FPC electronics is the reason your phone camera still works after a hundred open-and-close cycles. Peel apart almost any modern device, and you will find a thin amber ribbon carrying signals around corners no rigid board could turn. In this guide, you will learn: What does FPC stand for, and what are the differences between FFC and FPC? A flexible circuit that conducts a signal as it flexes The materials include one polyimide, copper, coverlay, and stiffener FPC manufacturing process (etching to elect......