How to Design Effective PCB Layouts for Switching Regulators
8 min
Switching regulators are the unsung workhorses of modern electronics. They efficiently convert power, enabling our devices to function seamlessly while minimizing energy loss. Yet, they have one notorious flaw: noise, such as electromagnetic interference (EMI). If you’ve ever heard a faint buzz or watched your oscilloscope struggle against spikes, you know what I'm talking about.
This blog delves into designing effective PCB layouts for switching regulators to keep the noise gremlins at bay and your circuits humming happily. To help you avoid these problems, here are some layout guidelines for switching power supplies:
- Potential problems with power supplies in PCB layouts.
- Setting up PCB parameters for power supply layout.
- Component placement and routing tips for an optimum layout.
What Are Switching Regulators?
Switching regulators are power converters that use high-frequency switches (transistors) and passive components (inductors, capacitors) to step up (boost), step down (buck), or invert voltage. They’re highly efficient, typically operating at 80–95%, making them ideal for battery-operated and high-power applications.
Common Types of Switching Regulators:
Buck Converter: Steps down voltage.
Boost Converter: Steps up voltage.
Buck-Boost Converter: Can step up or down voltage depending on the input-output relationship.
Why Noise is the Villain in Switching Regulators?
All switching regulators generate noise at their dV/dt node and dI/dt loop. Noise in switching regulators arises primarily due to rapid switching and high di/dt (rate of change of current) in components. For more complex topologies, like half-bridge/full-bridge topologies, the switching node can move between different locations in the design depending on the phase difference between switching FETs. Here’s how it works:
1. Electromagnetic Interference (EMI): High-frequency noise radiates into nearby components or circuits.
2. Signal Integrity Issues: Noise can corrupt sensitive signals in analog or RF sections of your PCB.
3. Heat and Efficiency Losses: Excess noise can lead to power loss and heating, reducing overall system efficiency.
So, how do we tame this noisy beast? The answer lies in thoughtful PCB design. Here is our design blog on full custom PCB design.
Components in a Switching Regulator:
1) Inductor: Use low-EMI inductors like ferrite core types (e.g., toroids). Avoid open cores near low-power traces, and orient poles perpendicular to the PCB for better noise control.
2) Feedback Traces: Keep feedback traces far from inductors and noisy traces. Place them on the opposite PCB side with a ground plane in between.
3) Filter Capacitors: Position input capacitors close to the IC to reduce noise. Use surface-mount capacitors to minimize inductance.
4) Compensation Components: Place these near the IC and avoid proximity to inductors to reduce noise.
5) Heat Sinking: Use PCB copper layers as heat sinks for power ICs by following the device datasheet for optimal heat dissipation.
Problems with Incorrect layout of Switching Power Supplies
A switch-mode power supply is often the preferred way to generate power on a printed circuit board. Using a switching regulator to convert the power, an SMPS will generate current more efficiently and with less heat than a linear power supply, which relies on larger heat-producing parts. However, the normal switching operation of the SMPS has the potential to radiate noise, which if not controlled properly, will add to or create the following problems:
- Electromagnetic Interference (EMI): Rapid voltage switching generates EMI, which disrupts both external electronics and internal circuitry, potentially degrading signal and power integrity.
- Ground Bounce: Fast switching can elevate the circuit board's ground reference, causing incorrect signal switching and data errors.
- Power Ripples: Switching may create ripples that induce crosstalk in nearby circuits, overpowering weaker signals and disrupting functionality.
To avoid these problems, it is important to follow good power supply layout guidelines starting with how the board will be configured in the layout tools.
How Layout Reduces Noise in Switching Regulators
A good layout is like a well-organized kitchen: everything is in its place, minimizing unnecessary movement (and mess). Proper PCB design minimizes noise by reducing parasitics, optimizing current paths, and shielding sensitive components.
Understanding Critical paths in Switching Topologies:
In a switching regulator PCB design, the most important rule is to route the traces that carry high switched currents to be as short as possible. If this rule is successfully implemented, a large part of the board layout for a switching regulator will be addressed properly. The first step is to find out which paths in a switching regulator topology are critical. In these paths, the current flow changes with the switch transitions.
Buck Topology:
As per the general schematics of buck converter, the critical paths(where switching is performed) are shown in red. They are connecting lines in which either the full current or no current flows, depending on the states of the power switches. These paths should be as short as possible. For a buck converter, the input capacitor should be situated as close as possible to the VIN pin and GND pin of the switching regulator IC.
Boost Topology:
Here, a low voltage is converted to a higher voltage. Once again, the current paths in which the current flow changes with switching of the power switches are shown in red. Interestingly, the placement of the input capacitor is not critical at all. The most crucial is the placement of the output capacitor. It must be as close as possible to the flyback diode (or the high-side switch) as well as to the ground connection of the low-side switch.
10 Quick Design Tips for Switching Regulators layout:
1. Current Path Design
- In a buck converter, the current paths change depending on the ON/OFF state of the switching element.
- Pay close attention to areas with rapidly changing currents, as they generate harmonics that can introduce noise.
2. PCB Layout Procedure
- Place critical components like input capacitors and free-wheel diodes close to the IC on the same PCB surface.
- Use thermal vias to enhance heat dissipation if necessary.
- Minimize the copper area of the switching node to reduce radiation noise.
3. Input Capacitor and Free-Wheel Diode Placement
- Use a high-frequency bypass capacitor (e.g., 0.1µF to 0.47µF ceramic) close to the IC for noise suppression.
- Large input capacitors can be placed slightly further away but ensure the bypass capacitor is nearby.
- Avoid placing capacitors and diodes on the bottom layer through vias, as it increases ripple voltage and noise.
4. Thermal Via Implementation
- Thermal vias under the IC’s thermal pad help efficiently dissipate heat to the opposite PCB layer.
- Small-diameter vias (e.g., 0.3mm) filled with solder are preferred to enhance conductivity.
5. Inductor Placement
- Place the inductor near the IC but avoid oversized copper areas to prevent it from acting as an EMI antenna.
- Avoid placing ground or sensitive signal traces directly beneath the inductor to reduce eddy current losses.
6. Output Capacitor Placement
- Position output capacitors close to the inductor for smooth current flow.
- Maintain a 1–2cm distance between input and output capacitors to prevent high-frequency noise coupling.
7. Feedback Route Wiring
- Feedback wiring should be short, direct, and far from noise sources like the switching node or inductor.
- Avoid routing feedback traces directly beneath or parallel to high-current paths to minimize noise coupling.
- For multilayer boards, use vias to route feedback traces on a separate layer if needed.
8. Ground Design
- Separate analog (signal) ground and power ground planes to minimize noise interference.
- Use multiple vias to connect top-layer ground to inner-layer ground planes, reducing impedance.
9. Resistance and Inductance of Copper Traces
- Calculate resistance and inductance for trace dimensions to ensure proper current handling.
- Use wider traces for high-current paths (e.g., 1mm width per 1A for 35µm copper thickness).
10. Corner Wiring
- Avoid sharp right-angle bends in traces as they increase EMI and signal reflections.
- Use 45° bends or rounded traces for better impedance matching and reduced noise.
Conclusion:
By following these guidelines, you can design robust, noise-free PCBs for switching regulators that perform reliably in even the most demanding applications. A well-designed layout not only improves electrical performance but also ensures thermal efficiency and EMI compliance. Get in touch with us, see how PCBs are manufactured in JLCPCB factory.
Inexperienced circuit designers often consider the board layout for a switching regulator to be black magic. The most important rule is to design the traces, in which the current flow changes with the switch transitions, to be as short and compact as possible. This can be explained easily, follows logical relationships, and is the basis for an optimized board layout in a switch-mode power supply design.
Popular Articles
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
PCB Terminal Blocks : A Design Engineer’s Guide to Reliable Wire-to-Board Connections
Key Takeaways Address Failure Modes: Select proper clamps and mounts to stop loose wiring, joint fatigue, and arcing. Screw vs Spring: Screw blocks provide strong clamping for high vibration, while spring blocks speed up wiring. Safety Distances: Keep proper clearance distances for voltages over 15V to prevent electrical arcing. Optimized Footprint: Use larger annular rings and 2 oz copper to handle mechanical strain and heavy currents. Automated Assembly: Selective wave soldering prevents cold joints......
PCB Panelization Explained: Tips and Techniques
PCB panelization is a crucial process in modern electronics manufacturing, designed to streamline production and reduce costs. In this way smaller circuit boards are produced in bulk and joined to one another to form a single array. This bulk production fosters the easy movement of PCBs through an assembly line. CNC (Computer Numerical Control) machines are utilized in PCB production and assembly facilities. These CNC machines can design PCBs that are rather large in size. But typically, electronic pr......
PCB Card Edge Connectors : Design Essentials, Gold Finger Optimization, and Manufacturing Strategies for Reliable Integration
PCB card-edge connectors are the unsung heroes of modular electronics. By providing a gold-plated finger interface along a circuit board edge, they allow plug‑and‑play connections between motherboards, expansion cards, and memory modules. Unlike soldered or wired joints, card-edge contacts offer easy replacement and upgrade of components. You imagine swapping a graphics card or SSD by simply unplugging one board and plugging in another. This edge-based interconnect enables high-speed, high-density rou......
How to Design a PCB with Flux.ai (Step-by-Step Guide)
Key Takeaways This step-by-step Flux PCB design tutorial demonstrates the complete workflow by creating a compact 15 × 15 mm USB 2.0 hub, refining the layout, routing high-speed differential traces, and preparing manufacturing files for JLCPCB PCB fabrication and assembly. We are all hearing news; new AI models are being released every month. And it has finally reached the schematic editor. Flux.ai is a browser-based AI PCB design tool with a built-in AI agent that behaves like a junior hardware engin......
Mastering PCB Footprints: Design Best Practices for Reliable Manufacturing
Key Takeaways A PCB footprint (land pattern) translates component datasheet dimensions into copper pads, solder mask openings, paste apertures, silkscreen, and clearance areas that enable reliable soldering and assembly. Follow IPC-7351 standards and manufacturer DFM rules for pad dimensions, spacing, and layer design to minimize defects like solder bridging, tombstoning, and cracked joints. Choose between through-hole (THT) and surface mount (SMT) footprints based on electrical needs, thermal perform......
How to Design Your Own Keyboard PCB: From Layout to Firmware
Designing a custom keyboard PCB is one of the most rewarding entry points into practical electronics. You not only get a really useful product on your desk, but also you learn schematic capture, matrix scanning, footprint selection, USB, and firmware. Most of the hardware engineers use the same skills that show up on professional boards. This guide walks the entire build from choosing switches, wiring the diode matrix, adding the microcontroller and USB-C, laying out the board, and flashing QMK or VIA......