5 Common PCB Design Mistakes to Avoid as a Beginner
7 min
- 1. Poor Planning and Component Placement
- 2. Ignoring Power Distribution and Decoupling
- 3. Poor Signal Integrity: Impedance, Return Paths and Crosstalk
- 4. Thermal and Power Dissipation Oversight
- 5. Not Designing for Manufacturability
- Conclusion:
- Frequently Asked Questions (FAQ)
PCB design is both an art and a science. Every electronics engineer wants to turn their circuit into a reliable printed circuit board. However, beginners often make the same mistakes that lead to noisy signals, overheating, failed prototypes, or costly redesigns. In this guide, we’ll examine the 5 most common PCB design mistakes and how to avoid them — with practical explanations and simple rules you can apply right away.
1. Poor Planning and Component Placement
In mixed-signal systems (analog + digital), poor placement can cause noise coupling. Analog parts are slower but noise-sensitive; digital parts operate at high frequencies, generating noise. To avoid this, follow the 20H rule: separate digital and analog sections by at least 20 times the layer thickness (H). For example, on a JLCPCB standard 1.6mm FR-4 board (layer spacing ~0.2mm), this means a minimum 4mm gap.
Bad placement also increases trace length (higher loss and EMI) and worsens thermal dissipation. It complicates power routing and often forces many vias during routing.
How to avoid it:
- Group functional blocks (power, analog, digital, RF) and orient them for short connections between related pins.
- Use the 20H rule for mixed signal
- Reserve space for test points, programming headers and polarity markings.
- JLCPCB’s free DFM checker can flag placement issues early.
2. Ignoring Power Distribution and Decoupling
Power integrity is the most important factor in multilayer PCBs. If there is an error in the power supply or noise in the power, then the product's quality and performance can be compromised. The two main causes for power supply failure can be the placement of the decoupling capacitor and the distribution. Power distribution issues are there because of improper trace width; thin VIN/VOUT traces heat up and create voltage droop under load. Usually, in power supplies, different value decoupling capacitors are used to eliminate the high-frequency and lower-frequency noises. There are some recommended steps to improve the power integrity of a PCB.
A common mistake is using only one type or value of capacitor, or placing them too far from the IC pins. Different frequencies require different capacitor values — small ceramic capacitors handle high-frequency noise, while larger electrolytic or tantalum capacitors handle lower-frequency ripple.
There are some recommended steps to improve the power integrity of a PCB.
Recommended Steps:
- Use wide traces or dedicated power planes for high-current nets. On 4-layer boards, dedicate an inner plane to ground and another to power if needed.
- Place at least one 0.1 μF ceramic decoupling cap right beside each power pin. Add 1 μF–10 μF bulk caps near regulators. Keep traces as short as possible (millimeters, not centimeters).
- Use ferrite beads or LC filters to isolate noisy domains (e.g., switching regulator to analog).
3. Poor Signal Integrity: Impedance, Return Paths and Crosstalk
Beginners route fast signals like any other wire on random layers, abrupt layer transitions, and long stubs. They also split planes without handling return paths. Let's talk about them one by one. If the impedance of two lines does not match, then the signal will reflect from the discontinuity end, and impedance mismatch will be there. It usually occurs because of vias, trace discontinuity, and component placement in the signal path. Cross-talk is there due to the overlapping of signal magnetic fields with other trace magnetic fields. And return paths are required to ground the signal and complete the path from generation to sinking back. There are all factors that decide the signal integrity of a PCB.
- Impedance mismatch creates reflections that distort the waveform.
- Discontinuous return paths force current to take long detours, increasing EMI and noise.
- Crosstalk occurs when magnetic or electric fields from one trace interfere with adjacent traces
Here are some guidelines to avoid:
- Plan stackup up front. For typical designs, use a 4-layer stackup (Top signal / GND / PWR / Bottom signal) so every high-speed trace has a close reference plane.
- Use controlled impedance (50 Ω single-ended, ~100 Ω differential) for high-speed traces and route differential pairs together with consistent spacing.
- Avoid splitting ground planes under a signal; a signal's return should be continuous and directly under the trace. If you must split planes, route signals so return currents aren't forced to jump over voids.
- Use 45° bends and gentle curves for RF/fast traces rather than 90° turns.
4. Thermal and Power Dissipation Oversight
Many beginners focus only on electrical connections and forget that components generate heat during operation. They rely on small copper pads or thin traces without thermal vias or proper heatsinking. This causes ICs and power components to run hotter than expected, leading to performance throttling, shortened lifespan, or sudden failures.
How to avoid it:
- Identify heat sources (power MOSFETs, linear regulators, processors). Provide adequate copper area and thermal vias beneath power ICs or BGAs to transfer heat to internal planes.
- Use thermal reliefs where needed, but avoid isolating thermal pads completely from planes. For BGAs, place an array of thermal vias under the pad and ensure they are plugged or tented if the fab requires it.
- Add thermal pads and heatsink mounting if dissipation exceeds what copper planes can handle. Run a quick thermal estimate (power × thermal resistance) to check temperatures.
5. Not Designing for Manufacturability
Clean schematics and finished GERBERs don’t guarantee a manufacturable PCB. Common issues can be wrong footprints and silkscreen over the pads. Sometimes we also have to look for missing fiducials and insufficient clearances for wave/hand soldering. PCB house rejects files, reworks cost time and money, assembly fails, and debugging becomes painful.
How to avoid it:
- Use verified footprints from the vendor or libraries and always check the datasheet if it is matching with the component parameters.
- Add fiducials, paste mask openings, and keep component spacing compatible with pick-and-place machines.
- BOM (bill of materials) should be included with the placement file.
Conclusion:
Avoiding these five common mistakes will save you countless hours of debugging, reduce prototype failures, and help you create more reliable and professional PCBs from the very beginning. Good PCB design is about careful planning, understanding the physics behind each decision, and thinking ahead about both electrical performance and real-world manufacturing.
Start with simple projects, check your work at every step, and don’t be afraid to learn from each prototype. With practice and attention to these basics, you will quickly develop the skills needed to design high-quality electronics.
Frequently Asked Questions (FAQ)
1. What is the most common beginner mistake in PCB design?
Poor component placement, especially mixing analog and digital sections too closely, causing noise and interference.
2. Why is decoupling important and how to do it right?
It stabilizes power and reduces noise. Place 0.1 μF capacitors close to every IC power pin and add bulk capacitors near regulators.
3. How can I avoid signal integrity problems?
Use proper layer stackup, keep high-speed traces close to ground planes, and match lengths for differential pairs.
4. What should I check before sending my design for manufacturing?
Run DFM checks, verify footprints, add fiducials, and ensure clearances for assembly and soldering.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......