How to Create Your Own PCB Trace Width Calculator with Python
6 min
- Parameters to Consider
- Features of the Python Trace Width Calculator
- How to Run the Trace Calculator in an Online Python Compiler
- Python Code:
- Final Thoughts:
PCB traces are critical for current carrying, signal integrity, and thermal performance in any design. While IPC-2152 provides the standard formulas, manual calculations are time-consuming. In this tutorial, we’ll create a lightweight Python trace width calculator based on IPC-2152. You can run it in any online compiler and cross-verify results with JLCPCB’s free online impedance calculator for real-world manufacturing accuracy.
Let's start with an example: if I am designing a power PCB and my trace is 10mm long and consists of a current of 5 A, then what will be the thickness? So we have to calculate by going into IPC, but in the era of computers, hand calculations are not done! Oh yes, you can use any online calculator, but why rely on them? We will design our independent code.
Coming back to the main question - How wide should my copper trace be? The answer depends on several factors, like the current it must carry, the acceptable temperature rise, the copper thickness, and whether the trace is on an internal or external layer. To streamline this process, I developed a Trace Width Calculator in Python based on IPC-2152 guidelines. In this post, I’ll walk you through the design process, the parameters considered, and the features of the tool. And finally, how you can run it in any online Python compiler.
Parameters to Consider
When designing the calculator, the following key parameters (based on IPC-2152 and JLCPCB capabilities) were included:
1. Current Capacity (A) – The amount of current the trace must safely carry.
2. Temperature Rise (°C) – How much the trace temperature is allowed to increase above ambient.
3. Layer Type – External traces dissipate heat better than internal traces, so their formulas differ.
4. Copper Weight (oz/ft²) – Commonly 1 oz or 2 oz copper; affects thickness and resistance.
5. Trace Length (mm) – Important for calculating resistance and voltage drop.
6. Trace Width (mm) – Used when calculating maximum current from a given size.
JLCPCB minimum trace width/spacing is 0.10 mm (4 mil) for standard 1 oz copper.
Features of the Python Trace Width Calculator
The code is very lightweight, hence it does not have any UI. So it can be run online using any Python compiler. Here’s what my calculator can do:
Two Modes:
1) Width from Current – Enter current, get the required trace width.
2) Current from Width – Enter width, get the maximum supported current.
Additional Calculations:
- Trace resistance (Ω)
- Voltage drop (V) for a given load
- Power loss in the trace (W)
After calculation, always cross-check results with JLCPCB’s free online impedance calculator and select “Controlled Impedance” during quoting for ±10% tolerance verification.
How to Run the Trace Calculator in an Online Python Compiler
You don't need a local Python setup to use this tool. Just copy the code below given code and here is how to run the guide:
1. Visit any online Python compiler and paste the code into it. I am using Programiz just for example, you can choose any local one.
2. Click Run.
3. Follow the prompts in the terminal window to input your parameters.
First, it will ask the user to select between the two given modes: Width from Current or Current from Width. The respective output and prompts are given below:
Width from Current:
Current from Width:
This makes it possible to run the calculator from any device, even without installing Python.
Python Code:
import math
def calculate_trace_width(current, temp_rise=10, is_external=True):
# IPC-2152 constants
if is_external:
k = 0.048
b = 0.44
c = 0.725
else:
k = 0.024
b = 0.44
c = 0.725
width_mils = (current / (k * (temp_rise ** b))) ** (1 / c)
width_mm = width_mils * 0.0254
return width_mm
def calculate_trace_properties(width_mm, length_mm, copper_oz):
# Constants
copper_thickness_mm = {1: 0.035, 2: 0.07} # in mm
resistivity = 1.68e-8 # Ohm-meter for copper
# Get thickness
thickness_mm = copper_thickness_mm.get(copper_oz, 0.035)
cross_section_mm2 = width_mm * thickness_mm
# Convert to meters
length_m = length_mm / 1000
area_m2 = cross_section_mm2 * 1e-6
# Resistance
resistance = resistivity * length_m / area_m2
return resistance
# --- Main Program ---
mode = input("Choose mode (1 = Width from Current, 2 = Current from Width): ")
if mode == '1':
current = float(input("Enter current (A): "))
temp_rise = float(input("Enter temperature rise (°C, default 10): ") or 10)
layer = input("Is it external layer? (y/n): ").lower() == 'y'
length_mm = float(input("Enter trace length (mm): "))
copper_oz = int(input("Copper weight (1 or 2 oz): "))
width_mm = calculate_trace_width(current, temp_rise, layer)
resistance = calculate_trace_properties(width_mm, length_mm, copper_oz)
voltage_drop = current * resistance
power_loss = current ** 2 * resistance
print(f"\n--- Results ---")
print(f"Required trace width: {width_mm:.3f} mm")
print(f"Trace resistance: {resistance:.4f} Ω")
print(f"Voltage drop: {voltage_drop:.4f} V")
print(f"Power loss: {power_loss*1000:.2f} mW")
elif mode == '2':
width_mm = float(input("Enter trace width (mm): "))
temp_rise = float(input("Enter temperature rise (°C, default 10): ") or 10)
layer = input("Is it external layer? (y/n): ").lower() == 'y'
length_mm = float(input("Enter trace length (mm): "))
copper_oz = int(input("Copper weight (1 or 2 oz): "))
width_mils = width_mm / 0.0254
if layer:
k = 0.048
else:
k = 0.024
b = 0.44
c = 0.725
current = k * (temp_rise ** b) * (width_mils ** c)
resistance = calculate_trace_properties(width_mm, length_mm, copper_oz)
voltage_drop = current * resistance
power_loss = current ** 2 * resistance
print(f"\n--- Results ---")
print(f"Maximum supported current: {current:.2f} A")
print(f"Trace resistance: {resistance:.4f} Ω")
print(f"Voltage drop: {voltage_drop:.4f} V")
print(f"Power loss: {power_loss*1000:.2f} mW")
else:
print("Invalid option.")Final Thoughts:
This is a simple yet powerful Python project based on IPC-2152. To make it work, a designer needs to have proper parameter information and needs to go through the IPC guidelines for the trace calculator. The results may differ from the online calculators because some of them are running a previous version of the code.
For real manufacturing on JLCPCB:
- Use the calculator for quick prototyping.
- Verify final values with JLCPCB’s free impedance calculator.
- Select “Controlled Impedance” when ordering for ±10% tolerance (or ±5% optional) and TDR testing.
You can easily extend the code with a GUI using Tkinter or Streamlit. Feel free to share your version and tag JLCPCB — we love seeing community tools!
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......