Role of Break Out Boards in Electronics Prototyping
6 min
- Breakout board basics
- Types of Breakout Boards
- Why to prefer Breakouts over Custom PCBs:
- Transitioning from Breakout Boards to Custom PCBs
- Conclusion
Breakout boards are the heart of prototyping, they are almost available in all kinds. From sensors to modules are dev boards. When we have to realize a circuit without actually connecting it through soldering the breakout boards are the ones that do the job. As an example we have seen Arduino it has a very wide community support and nowadays it covers almost all the sensor breakout in the kit itself. You can buy several kits which contain different modules and sensor breakout boards which are compatible with Arduino. In this tutorial here we will focus more on types of breakout boards and how to choose the right one. Finally we will discuss some applications and how to do a transition from breakout board to actual custom PCB.
Breakout board basics
A breakout board basically onboards 3 components. First the PCB itself on which all the things are going to be set up. Then the main IC or sensor whatever. In the end to make everything working together we need some interfacing circuit like resistor capacitors are all. All these things together make a breakout board. Compatibility with different microcontrollers is another important aspect to think over. Now because we have a header which can be directly plugged into the breadboard or female header we do not need to solder it. Which makes the breakout board a gamechanger.
Say I want to use the same module somewhere else, what I can do is just simply unplug it from the first source and insert it to the second one. For standard we use 2.54mm header pins which are also compatible with breadboards. We will discuss their types. Usually they cover a lot of temperature, pressure, acceleration… If you can name it, you can most likely measure it with a breakout board.
Types of Breakout Boards
For this you need to know a lot about the ICs and working principle, but some basic ones cover:
1. Sensor Breakout Boards
These boards house a specific sensor such as temperature, humidity, pressure or light. The sensor is soldered on the PCB one side and the interfacing the circuit on the backside of the same PCB. I/O pins for easy access, examples include:
- BMP180/280 (Barometric pressure)
- MPU6050 (Accelerometer + Gyroscope)
- DHT11/DHT22 (Temperature and humidity)
2. Communication Breakout Boards
Used to integrate communication protocols into a project. They are the boards which are used to perform the operation on data output or input. They often contain level shifting circuits such as the 12C protocol, in which resistors are used to pull up the both SDA and SCL lines. Some of the world wire adopted communication protocol examples are:
- I2C / SPI / UART Breakouts
- RS232 / RS485 / CAN Bus Breakouts
3. Power Management Breakout Boards
Provide regulated power or manage battery charging/distribution. They are designed in such a way that in the small form factor deliver the same kind of performance as the custom PCB. Some factors like current carrying capacity and heat dissipation should be considered when using a power management board. They are of different kinds, some examples are stated as:
- DC-DC Converters (Buck or Boost modules like LM2596, MT3608)
- Battery Charging Modules (TP4056 for Li-ion)
4. Display Breakout Boards
Allow easy interface with display modules through SPI or I2C. This is I think the most used module, screen directly carries a user interface and when it comes to display there are a lot of options:
- OLED Display Modules (SSD1306)
- LCD Modules (1602/2004 with I2C backpack)
- TFT Displays (ILI9341, ST7735)
Some one can consider one option as per the project requirements and cost analysis.
5. Audio Breakout Boards
Used for audio playback, recording or processing. The audio breakout boards should consider a lot of things such as signal integrity and impedance matching. Overall we somehow implement a digital protocol on an analog speaker system. Which needs extra care because mixing the two sections causes unwanted noise and crosstalk of signals. Some examples of audio based breakout boards are:
- I2S Audio Modules
- Amplifier Boards (e.g., PAM8403, TPA3116D2)
- DAC/ADC Boards (PCM5102, MCP3008)
6. Storage and Memory Breakout Boards
These types of modules are used for data logging purposes. Say we want to store some kind of information related to a sensor then they are the only source to store. Some really cool libraries are available which can make a good excel representation out of it. Btw the protocols are:
- SD Card Breakout Boards
- EEPROM/Flash Memory Modules
7. Clock and Timing Breakout Boards
Offer timing and synchronization support. When it comes to synchronizing or logging the time based data into SD cards then RTC comes into play. They have their own battery yet they are very power efficient and work well if power is disconnected from the source. Some examples are:
- RTC Modules (DS3231, DS1307)
- Oscillator/Clock Generator Breakouts
Why to prefer Breakouts over Custom PCBs:
I think I have answered this question before, it is because of its reusability in other projects and somehow if it got damaged we can replace it with a new one. It is very convenient with breakout boards. On the other hand if you have a custom PCB they need a proper soldering kit to desolder and remove and then again solder the new one. Breakout boards also save space on a PCB, because now we are mounting a small breakout PCB onto another main PCB so it has a lot of space underneath where some sort of interfacing circuitry can be placed.
Now as the design matured we somehow reduced the overall cost of a product move to custom design rather than this 2 PCB design. Which is complex and different yet this is a job to do.
Transitioning from Breakout Boards to Custom PCBs
Breakout boards are ideal for early-stage development. But as the project moves toward production it is essential to transition to custom PCB layouts. These custom designs offer improved reliability, compactness and performance.
Conclusion
As technology continues to advance, breakout boards evolve as well. As per time it integrates more features and supports a broader range of functions. Not only their utility is enhanced but also fuels innovation. Which helps to grow in both hobbyist projects and industrial-grade systems.
While breakout boards may not always be suitable for final product designs due to size or reliability constraints. But their importance in the prototyping phase is unmatched. They allow engineers to quickly validate concepts, test functionality and iterate designs. They help to significantly reduce development time and cost. Whether you're building a personal project or developing a commercial solution the breakout boards remain an essential part of the modern electronics workflow.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
• Design Guidelines for PCB Using FR4 Substrates
Keep Learning
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......
A Practical Guide to Circuit Design from Concept to PCB
Key Takeaways Define clear circuit requirements and select suitable components based on electrical ratings, performance, and availability. Follow a structured design workflow from schematic capture and simulation to PCB layout and validation. Optimize component placement, routing, power distribution, and signal integrity to improve circuit performance. Apply DFM guidelines and complete ERC/DRC checks to prevent design errors and ensure smooth PCB manufacturing. Choose appropriate PCB materials, layer ......
PCB Silkscreen: All You Need to Know
Key Takeaways The PCB Silkscreen Guide demonstrates that a properly designed legend layer is essential to prevent assembly failures and ensure long-term hardware reliability. By mastering modern manufacturing methodologies like Direct Legend Printing (DLP) and aligning layouts with JLCPCB's strict DFM design rules—including the absolute 0.8 mm character height limit and the automated 0.15 mm silkscreen clipping protocol driven by solder mask precedence—engineers can seamlessly eliminate cold joints an......
The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
Note Need a quick reference while reading schematics? Download our free, printable Circuit Symbols Cheat Sheet (PDF), featuring the most common IEC and ANSI symbols organized by category. Keep it on your desktop or print it for easy reference at your workbench. ⬇ Download the Free Circuit Symbols Cheat Sheet (PDF) Every electronic diagram is written in a visual language, and circuit symbols are its alphabet. From your first electrical schematic to a multi-layer board, knowing circuit symbols can make ......
Understanding Electrical Schematics: A Comprehensive Guide
Key Takeaways Schematics vs. Block Diagrams: Schematics detail exact components and connections; block diagrams only show high-level functions. Mark Polarity: Essential to prevent circuit failure and automated SMT placement errors at JLCPCB. Clean Layout: Use modular blocks and net labels (VIN, GND) to eliminate visual clutter. Manufacturing Ready: Follow DFM trace rules and export standard Gerber, BOM (LCSC C-IDs), and CPL files. Fast Troubleshooting: Isolate schematic blocks to test expected voltage......
PCB Board Design: A Step-by-Step Guide for Beginners
Key Takeaways This PCB Design Guide offers beginners a practical step-by-step approach to designing a compact 3A IP2312 lithium battery charger PCB — an upgraded alternative to the popular TP4056 module. It focuses on key techniques like schematic creation, optimized layout, proper trace routing for 3A current, and ground planes to build efficient and reliable boards. Printed Circuit Boards (PCBs) form the backbone of most modern electronic devices, providing a platform to connect electronic component......