Design Process of a Surface Mount PCB
8 min
- How is Surface Mount Technology Different From Through Hole?
- Design Process of a Surface Mount PCB
- Get your Hands on PCB Assembly Service in just 3 steps:
- FAQ about Surface Mount PCB
- Conclusion:
Key Takeaways
Mastering the surface mount PCB design process is essential for creating compact, high-density, and reliable electronic boards. This comprehensive guide walks through the complete SMT workflow — from schematic capture and component selection to optimized layout, precise routing, DRC/ERC verification, and Gerber file generation — enabling designers to achieve superior performance, better manufacturability, and cost efficiency compared to traditional through-hole methods. By following these structured steps and best practices, you can successfully develop professional-grade SMT PCBs ready for efficient assembly and high-volume production.
Surface-mount technology (SMT) is a planar technique used to directly attach components to the surface of a printed circuit board (PCB). Unlike traditional through-hole technology, which requires inserting component leads into holes on the PCB, SMT mounts components directly onto the board's surface. SMT offers benefits like smaller component sizes, enhanced manufacturing efficiency, and better compatibility with automated assembly processes.
It also allows for more components to fit on a given area of substrate. Surface-mount technology enables higher component density, with modern SMT designs often achieving 2-10 times more components per unit area compared to through-hole. It supports automated high-speed assembly, reducing production costs significantly for volumes over 100 pieces. According to industry data, over 90% of modern electronics use SMT due to miniaturization and performance benefits.
How is Surface Mount Technology Different From Through Hole?
Surface Mount Technology (SMT) and Through-Hole Technology (TH) are two methods of attaching components to a PCB. SMT mounts components directly on the board's surface, allowing for compact and high-density designs, typically using automated assembly and reflow soldering. TH involves inserting component leads through holes in the PCB and soldering them on the opposite side, offering stronger mechanical bonds, making it ideal for stress-prone components. SMT is favored in modern, high-volume electronics for its efficiency and miniaturization, while TH is used in applications requiring robustness and easier repair, such as aerospace and prototyping.
SMDs cannot be used directly with plug-in breadboards (a quick snap-and-play prototyping tool), requiring either a custom PCB for every prototype or the mounting of the SMD upon a pin-leaded carrier. For prototyping around a specific SMD component, a less-expensive breakout board may be used.
Design Process of a Surface Mount PCB
1. Schematic Design
The first step in designing an SMT PCB is creating a schematic diagram. This schematic serves as the blueprint of your circuit and defines how each component is connected. Recently I have covered a project the EasyEDA software and here are some important details. To know more about, electric schema capturing see your comprehensive guide on it.
- Select appropriate surface-mount components from the available libraries.
- Ensure all connections between components (called "nets") are properly mapped out.
- Label key signals and power distribution for easy reference.
The schematic is critical, as it forms the foundation for the entire design and ensures all components will interact as intended.
2. Selecting Components and Libraries
Surface-mount components are typically smaller than through-hole components, making them suitable for compact designs. When selecting components for your SMT PCB:
- Choose components with the proper package sizes for SMT.
- Ensure the components are readily available and suit the assembly process.
Most PCB design software provides built-in libraries of standard surface-mount components, which saves time in the design process.
3. PCB Layout and Component Placement
Once the schematic is complete, the next step is to transfer it to the PCB layout. This stage involves arranging the components and creating electrical connections (traces). Key considerations for SMT PCB layout include:
- Optimize Component Placement: Group functional blocks (digital, analog, power) together. Place critical components like MCUs, crystals, and power regulators first. Maintain at least 0.3mm clearance between SMD components and 1mm from board edges for JLCPCB assembly.
- Thermal Management: Use copper pours, thermal vias (min 0.2mm drill for JLCPCB), and heatsinks for power components. For high-power designs, consider 2oz copper or aluminum-backed PCBs.
- Avoid Crosstalk and EMI: Keep high-speed traces short (<λ/10), separate analog/digital grounds, and use ground planes. JLCPCB supports up to 32 layers with controlled impedance (±10%).
4. Routing the PCB
Routing is the process of creating copper traces that connect components. Key considerations include:
- Trace Width and Spacing: For standard 1oz copper on 2-layer boards, JLCPCB minimum trace/space is 5mil (0.127mm). Use wider traces (e.g., 20-50mil) for power lines based on current requirements.
- Power and Ground Planes: Implement solid ground planes to reduce noise and improve return paths.
- Via Placement: JLCPCB minimum via diameter 0.45mm (drill 0.2mm). Use via-in-pad (POFV on higher layers) for dense designs.
| Feature | Capability | Notes |
|---|---|---|
| Layers | 1-32 Layers | Standard FR-4 |
| Min Trace/Space (2L) | 5mil / 5mil | 1oz copper |
| Min Via | 0.45mm dia (0.2mm drill) | - |
| Board Thickness | 0.4 – 4.5 mm | Common: 1.6mm |
5. Design Rule Check (DRC) and Electrical Rule Check (ERC)
Before finalizing the design, run Design Rule Checks (DRC) and Electrical Rule Checks (ERC) to verify that the PCB adheres to both electrical and manufacturing guidelines. DRC ensures proper spacing, trace width, and component placement, while ERC checks for unconnected nets or other potential issues.
6. Generating Gerber Files
It is essential to include all necessary layers and use standard Gerber format (RS-274X) to avoid miscommunication during production. After generation, carefully review the files with a Gerber viewer to confirm trace integrity, pad sizes, and alignment. Proper Gerber output ensures accurate reproduction of your SMT design, particularly the fine-pitch component footprints and solder paste patterns critical for successful assembly.
Get your Hands on PCB Assembly Service in just 3 steps:
Upload: Upload your Gerber, BOM & CPL files to get an instant quote on PCB.
Select: Select the parts and components to be placed for assembly. Assembly Prices start at $8.00 setup fee, and a minimal assembly fee of $0.0017 per joint.
Receive: A streamlined process from ordering, sourcing parts and PCB prototyping allowing you to iterate, improve and deliver on time.
FAQ about Surface Mount PCB
Q: What are the main advantages of SMT over through-hole technology?
SMT allows for much smaller component sizes and higher component density on the PCB, enabling compact designs. It also supports faster automated assembly and generally offers better price-to-performance ratio for high-volume production.
Q: How do I choose the right package size for SMT components?
Select packages based on your board space, current requirements, and assembly capabilities. Common sizes include 0402, 0603, and 0805 for passive components. Smaller packages (like 0201) save space but require more precise assembly, while larger ones are easier to handle and solder.
Q: What are the most important considerations during component placement?
Group components by function, place critical parts like microcontrollers and power ICs first, ensure adequate spacing for heat dissipation, and separate analog and digital sections to minimize interference.
Q: Why is it important to run DRC and ERC before generating Gerber files?
DRC and ERC help detect manufacturing violations (such as insufficient trace spacing or via sizes) and electrical errors (unconnected pins or shorts) early. Catching these issues prevents costly fabrication mistakes and improves the reliability of your SMT board.
Q: What files are needed for professional SMT PCB assembly?
You will typically need Gerber files for fabrication, a Bill of Materials (BOM) listing all components, and a Component Placement List (CPL) showing the position and orientation of each part.
Q: Can I mix SMT and through-hole components on the same board?
Yes, many designs use a combination of both technologies. SMT is ideal for most components to achieve high density, while through-hole is often used for connectors, large capacitors, or power components that require stronger mechanical strength.
Conclusion:
Designing a Surface Mount PCB is a multifaceted process that requires careful planning, precise component placement, and attention to manufacturing details. From creating the schematic to generating Gerber files and prototyping, each step plays a crucial role in ensuring the success of your design. See how any why SMT offer better price to performance ratio.
By following these steps and JLCPCB best practices, you can create reliable, high-performance SMT PCBs... See how and why SMT offers a better price-to-performance ratio for most modern applications.
Keep Learning
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......
The Role of PCB Test Fixtures in High-Volume Manufacturing
In high-volume manufacturing of Printed Circuit Boards (PCBs), quality, efficiency, and reliability are paramount. One of the most crucial tools in achieving these goals is the PCB test fixture. These fixtures play a vital role in ensuring that PCBs meet the required performance standards before they are integrated into electronic devices. This article delves into the importance of PCB test fixtures, their types, and how they contribute to the efficiency of high-volume manufacturing. Specialized and c......
SMT or Through Hole Technology?Which is Better for Your Project?
When designing and manufacturing electronics, one of the most important steps is selecting the appropriate assembly method. Nowadays we have through-hole technology and surface mount technology, which become the industry standards and are the two main approaches. The surface-mount technology (SMT) uses components that are perfectly aligned with the PCB surface. On the other hand through-hole technology (THT) uses leads that are placed into pre-drilled holes in the PCB and thereafter soldered. Consider......
PCB temperature: Tips regarding improving the thermal management of PCBs
Thermal management is of utmost importance while designing PCBs. This is because the temperature of PCBs can guarantee the reliability, performance, and longevity of PCBs and the electronic equipment of which they are an integral component. Thus, enhanced Printed Circuit Board heat management is a necessity for reliable operation and to protect against damage to electronic components. In the upcoming chapter, we will discuss several approaches to strengthen PCB temperature management. Reasons of heat ......
Design for Manufacturing (DFM): A Comprehensive Guide for Optimizing Production
Maintaining quality while improving the manufacturing process is critically important in the competitive fields of electronics and industry. Design for Manufacturing (DFM) here comes in handy. DFM is a design tool stressing the simplicity of manufacturing during the product development stage. Early on manufacturing limitations help DFM to guarantee that goods are not only useful but also reasonably priced, dependable, and easily produced at large-scale production. This article covers the importance of......
Design for Manufacturing and Assembly: A Complete DFMA for PCB Design Guide
Key Takeaways DFMA covers both PCB fabrication and assembly: DFM addresses bare-board fabrication, while DFA addresses component assembly and related process constraints. The biggest decisions happen early: Package choice, layer count, and board outline are usually set well before Gerber export and become expensive to change later. Passing DRC does not guarantee a good footprint: Design rules can verify clearances and copper geometry, but they cannot confirm that a footprint matches the component data......