What is a Blank Circuit Board (Bare PCB) and How is it Used
7 min
- 1. Difference Between Zero PCB and Blank PCB:
- 2. Structure of a Bare PCB
- 3. How to Make a Blank PCB at JLCPCB
- 4. Types of blank PCBs:
- 5. Design Guidelines of a Mixed Signal Bare PCB:
- 6. Benefits of Using Blank PCB:
- Conclusion
A printed circuit board (PCB) that doesn't have any electronic parts on it is called a blank PCB, bare PCB. A PCBA, on the other hand, is a PCB that has all the electronic parts that it needs. Because there is a layer of copper covering the circuit board, blank PCB boards are sometimes called "copper clad" circuit boards. A blank PCB is a computer board that is made up of layers of epoxy fibreglass, copper foil, and PCB inks. Before the copper sheets, there are non-conductive prepreg layers on a blank printed circuit board. The board also has a base sheet. Copper-filled holes link the several layers of copper traces.
Single-sided, double-sided, and multi-layered bare PCBs are some of the different types. It is possible to choose the stackup based on its complexity and usefulness. To make them, they use base materials like FR-4 (fibreglass epoxy), polyimide (for flexible boards), or metal-core materials for heavy-duty uses. Some of the things will be talked about in the next section of this post. This piece talks about what a blank PCB is, what it can be used for, and how it is made. It also shows how to use JLCPCB's fabrication services to make a blank PCB.
1. Difference Between Zero PCB and Blank PCB:
A zero PCB (also called a general-purpose or perf board) is a pre-made board with a grid of holes and copper pads. It is used for manual circuit prototyping. Components are inserted into the holes and connected using wires or solder bridges. Zero PCBs are ideal for quick, small-scale experiments but do not support complex or high-density circuits.
A blank PCB, on the other hand, is a custom-manufactured board. It does not have pre-drilled holes or copper traces. It is fabricated according to a specific circuit design, for any shape, size, or number of layers. Blank PCBs are used for professional prototyping and production.
2. Structure of a Bare PCB
A typical blank circuit board consists of the following layers:
⦁ Substrate (Base Material): Provides mechanical support and insulation.
⦁ Copper Layer(s): Conductive pathways that interconnect electronic components.
⦁ Solder Mask: Protects copper traces and prevents solder bridging during component placement.
⦁ Silkscreen: Printed text or symbols indicating component placement and reference designators.
3. How to Make a Blank PCB at JLCPCB
JLCPCB is a widely used PCB fabrication service known for its affordability, fast turnaround, and comprehensive design-to-production workflow. Creating a blank PCB through JLCPCB involves the following steps:
1. Prepare Your Gerber Files
Design your circuit in a PCB design software such as KiCad, Altium Designer, or Eagle. Export the Gerber files, which include layer data for copper, solder mask, silkscreen, and drill information.
2. Visit the JLCPCB Website
Log in to your account and begin a new PCB order. Upload the Gerber files to their platform. The interface will automatically render a preview of your blank board layout.
3. Configure PCB Specifications
Choose your board properties, such as:
⦁ Dimensions and quantity
⦁ Number of layers
⦁ Board thickness
⦁ Copper weight
⦁ Surface finish (HASL, ENIG, etc.)
⦁ Solder mask color
Since you are ordering a blank PCB, you do not need to include a Bill of Materials (BOM) or pick-and-place files for component mounting.
4. Place the Order
Once all parameters are confirmed, proceed to checkout. Choose a shipping method based on your delivery timeline and budget.
5. Receive and Use Your Blank PCB
Upon delivery, your blank PCBs will be ready for component assembly—either manually or via an automated pick-and-place system, depending on your setup.
4. Types of blank PCBs:
1. FR-4
The most often used blank PCB is FR4 PCB. Although FR4 is level 4 flame retardancy rather than a substance.FR4 PCB is actually a fourth class flame retardant rated epoxy glass fibre PCB. Though it is partially cured, the pre-impregnated layer between the copper layers is likewise epoxy glass fibre.
Manufactured easily, FR4 blank PCBs are less expensive than other PCBs with the same number of layers and circuit complexity.
2. Metal core PCB
Copper and aluminium core PCBs are among metal core PCBs. Mostly utilised for LED lighting and other power applications, metal core PCBs offer far higher heat conductivity than FR4 cores.
3. Rigid-Flex PCB
PI or PET-based empty PCBs that can bend are flexible or rigid-flex PCBs. Special flexible PCBs, rigid-flex PCBs have laminated FR4 PCB layers on their flex region.
4. High Frequency PCB
Furthermore a high-speed and RF microwave PCB is a high-frequency PCB. Transmitting and receiving high-frequency signals, this PTFE-based blank PCB From radars to anti-collision systems to GPS to cellphones to missile systems, high-frequency PCBs find use in antennas, radars, etc.
5. Design Guidelines of a Mixed Signal Bare PCB:
Make Sections: When designing PCB wiring, the following principles should be followed: separating analog signals from clock signals, maintaining a separation of 20H between both sections. Where H refers to the spacing of the top layer to the next ground returning layer.
Impedance Matching: When completing PCB design, it is necessary to ensure that the PCB has uniform impedance and low electromagnetic interference. This will lower down the signal reflections and keep the proper signal integrity.
6. Benefits of Using Blank PCB:
First of all, it lets designers test circuits and try out new ideas at very little cost; once the circuit is perfect, it is then moved to a completed board for soldering and assembly. Second, DIY electronics aficionados extensively use bare PCBs since they can be made from scratch when a public PCB cannot fit your design requirements. Here are some primary advantages:
Modern electronics production depends on the diversity and adaptability of the blank PCB board, which is the pillar of circuit design and offers a strong basis for innovative electronic products.
Blank PCB Testing:
Shape and Size: Although rare, the bare PCB may already have flaws before components are introduced; failure of the PCB as a circuit board frame after installation can cause various issues.
Manufacturing Issues: Among the more often occurring issues are under-etching, over-etching, and holes. Manufacturing failures can result from even little flaws. Bare board testing becomes even more crucial as demand for multilayer PCB boards rises from growing component density.
The components of the board are the organs and muscles if the bare PCB is its skeleton. Since components can be somewhat costly and often vital, a strong frame helps to avoid long-term waste of high-end items.
Conclusion
Blank printed circuit boards are the basics of all electronics and electrical devices and products. Using services like JLCPCB, creating custom blank PCBs is more accessible than ever. With just a design file and a few configuration steps, users can transform a digital circuit layout into a tangible, production-ready board. Whether you're a professional engineer or an electronics enthusiast, understanding and utilizing blank PCBs is foundational to successful hardware development. If you have any questions about blank or bare printed circuit boards, such as stackup, layers or regarding any design issue, please contact JLCPCB support team.
Popular Articles
• Choosing the Right Electronic Components for Your Electronic Design: Tips and Best Practices
• PCBs Explained: A Simple Guide to Printed Circuit Boards
• Guide to the Top 10 Commonly Used Electronic Components
• Understanding the Basics of Electronic Devices and Circuits
• Digital 101: Fundamental Building Blocks of Digital Logic Design
Keep Learning
Basic Electronics Components: 10 Essential Parts Every Beginner Must Know
Basic electronics components are the fundamental building blocks of any electronic circuit. The most common components include resistors, capacitors, inductors, diodes, and transistors, each playing a specific role in controlling current, storing energy, or processing signals. In this beginner-friendly guide, we'll walk through 10 essential electronic components and explain how they work in real circuits. Whether you're just getting started or need a quick refresher, this guide will help you understan......
Dimensional Stability in PCB Manufacturing: Precision Solutions for Reliable PCBs
Dimensional stability is the ability of a PCB substrate and finished board to maintain its intended dimensions under varying temperatures, humidity, mechanical stress, and chemical exposure during fabrication, assembly, and operation. For engineers designing high-reliability electronics, this property directly determines registration accuracy in multilayer boards, solder joint integrity, and long-term field performance. Poor dimensional stability can cause trace misalignment, via cracking, or board wa......
Types of PCB Boards: Ultimate Reference with Specs & Use Cases
A printed circuit board (PCB) consists of laminated insulating and conductive materials that connect multiple electrical devices. A PCB can be thought of as a layered composite of fibreglass and epoxy with copper patterns etched onto it. These serve as electrical conductors and pathways for signals and power. A PCB can be Simple (one layer of conductive material), Double-Sided (two conductive layers), or Complex (three or more conductive layers) to allow numerous circuit paths on a small piece of hard......
PCB Layers Explained : Building Better Boards Through Smart Stackup, Standards, and Design Practices
A PCB is a sandwich of copper and insulating sheets that are stacked together to form a circuit board. Each PCB layer has a specific purpose; for example, some carry signals (traces connecting components), while others serve as solid planes for power or ground. Think of PCB layers like the floors in a building, where each floor can have a different role. We can think of it as offices (signals) on one floor and storage (ground/power) on another. The number of layers varies by design complexity, from ju......
Understanding the Role of Thermal Pads in PCB Cooling
Introduction Maintaining ideal temperatures in different electronic systems depends critically on thermal pads, which are also a fundamental part of the effective cooling of electronic equipment. Acting as a thermal interface material (TIM), these pads guarantee efficient heat flow between heat sinks or other cooling systems and electronic components. It is impossible to overestimate the importance of thermal pads in preserving device dependability and performance given the rising power densities and ......
Understanding the Role of Thermal Pads in Electronics Cooling
Introduction Maintaining ideal temperatures in different electronic systems depends critically on thermal pads, which are also a fundamental part of the effective cooling of electronic equipment. Acting as a thermal interface material (TIM), these pads guarantee efficient heat flow between heat sinks or other cooling systems and electronic components. It is impossible to overestimate the importance of thermal pads in preserving device dependability and performance given the rising power densities and ......