How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?
4 min
- Temperature for Wave Soldering
- Factors
- Soldering Temperature Standards
- Conclusion
Wave soldering is a process used for soldering electronic components by inserting them into the holes on a Printed Circuit Board (PCB) and securing the components to the board using a molten solder wave generated by a wave soldering machine. Temperature is a crucial parameter during the wave soldering process, as it directly affects the quality and efficiency of soldering. Therefore, setting the temperature correctly for wave soldering is essential.
Temperature for Wave Soldering
Wave soldering machines typically employ radiant heating for preheating, with the most commonly used methods being forced hot air convection, electric hotplate convection, electric heating rods, and infrared heating. Among these methods, forced hot air convection is generally considered the most effective method for heat transfer in most processes. After preheating, the PCB is soldered with either a single wave (λ wave) or dual waves (turbulent wave and λ wave). For through-hole components, a single wave is usually sufficient. When the PCB enters the wave, the direction of solder flow is opposite to the board's movement, creating eddies around component pins. This acts like a washing action, removing residues of flux and oxide films and forming proper wetting as the solder reaches its wetting temperature.
Factors
Setting the temperature for wave soldering involves considering multiple factors, including the solder's melting point, the material of the PCB, and the type of components being soldered. Generally, the temperature for wave soldering should be set near the melting point of the solder and slightly higher to ensure complete melting and good wetting on the soldering surface. However, the temperature should not be too high to avoid damage to the PCB and components.
Usually, the temperature setting for wave soldering needs to be adjusted based on the type of solder used and specific equipment parameters. When adjusting the temperature, it's advisable to gradually increase the temperature while continuously observing the color changes on the soldering surface and recording the temperature variations. In general, the temperature of the soldering surface should fall within the range of 240°C to 260°C, with a maximum temperature not exceeding 280°C.
In addition to temperature, the soldering time is also a critical factor affecting soldering quality. Too short a soldering time can result in incomplete soldering, while excessive time may damage components. Therefore, adjustments should be made according to specific circumstances to achieve the optimal soldering effect.
To sum up, setting the temperature for wave soldering involves considering various factors, including the type of solder, PCB material, and component types. When adjusting the temperature, it's important to gradually increase it while monitoring the color changes on the soldering surface and recording temperature variations to achieve the best soldering results.
Soldering Temperature Standards
Soldering temperature standards refer to the temperature range that should be achieved during the soldering process. For wave soldering, the soldering temperature standard typically falls in the range of 240°C to 260°C. Within this temperature range, the solder, when molten, can flow adequately and wet the soldering surface properly, resulting in stable solder joints.
In addition to the temperature range, soldering temperature standards also need to consider other environmental factors such as humidity and airflow. High humidity and airflow can impact soldering effectiveness. Therefore, adjustments should be made based on the specific production environment to ensure soldering quality and efficiency.
Conclusion
In summary, soldering temperature standards are of paramount importance for the quality and efficiency of wave soldering. Adjustments should be made based on the specific production conditions and environment to ensure soldering quality and efficiency. Regular maintenance and upkeep of wave soldering equipment are also essential to maintain stability and production efficiency. Wave soldering has a history dating back to 1956 when the British company Fry's Metal introduced the concept of printed circuit board wave soldering. It revolutionized the soldering process from manual soldering with soldering irons to automated, large-scale, and highly efficient soldering by machines. Wave soldering offers advantages such as speed, accuracy, and efficiency. It has made significant contributions to reducing soldering defects, improving the reliability of electronic products, lowering production costs, reducing the labor intensity of workers, and increasing production efficiency.
Popular Articles
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Everything You Need to Know About Solder Wire
The Latin word solidare means "to make solid," this is where the term solder gets its start. For joining two metal parts, this alloy is used because of its low melting point. Solder is a substance that is used to attach items, basically we can say wires and leads components together. Soldering is considered a skill in electronics for assembly of components onto a bare board PCB. The solder wire used has a significant impact on how well a soldering project turns out. It consists of alloys, mostly based......
SMT vs Through Hole: Which PCB Assembly is Most Cost-Effective?
Performance and cost in the realm of electronics production depend on choosing the correct assembly method. Of the several approaches accessible, Surface Mount Technology (SMT) and Through-Hole Technology (THT) are the two most often used ones for PCB assembly. These two assemblies can be combined to create some products or used as individual technologies. Though seemingly little, this variance affects several aspects including board design, materials and techniques employed, heat dissipation, and rel......
PCB Soldering Basic Techniques and Overview
Soldering means joining metal components with a melted metal called solder, which has a low melting point compared to other metals. Soldering is crucial in the electronics industry and is the primary method of joining electrical components. There are different types of soldering materials based on quality and their melting points. The most common combination is a tin or lead metal alloy mixed with silver or brass. The soldering iron melts the metal so it can be used like glue to connect two pieces. On......
Lead-Free Solder vs Lead Solder : What is the Difference?
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties ......
How to Repair a Burnt Circuit Board (and When to Replace It)
Key Takeaways Find out why the board burnt before you repair anything. The part that charred is often a victim of a fault somewhere else. Charred FR-4 conducts. A repair only lasts if every trace of carbon is cut out and the area measures as an insulator again. Heat that went through the board, blistering, or a burn among vias or under a BGA usually means replacing the board. Rebuild a burnt trace heavier than the original, and keep conductive epoxy off power paths. Power the repaired board from a cur......
How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?
Wave soldering is a process used for soldering electronic components by inserting them into the holes on a Printed Circuit Board (PCB) and securing the components to the board using a molten solder wave generated by a wave soldering machine. Temperature is a crucial parameter during the wave soldering process, as it directly affects the quality and efficiency of soldering. Therefore, setting the temperature correctly for wave soldering is essential. Temperature for Wave Soldering Wave soldering machin......