SMT Stencil Design Tips for Improving Solder Paste Deposition
5 min
- 5 Key Design Guidelines for Standard SMT Stencils:
- 4 Key Design Guidelines for Standard SMT Stencils:
- Conclusion
Solder paste deposition through stencil is a method to mass produce the units. Even with advanced placement machines and reflow profiles. Defects like bridging - tombstoning and insufficient solder joints can often be traced back to poor stencil design. Proper stencil design helps in achieving consistent and high-quality solder joints. As component sizes continue to shrink and circuit densities increase, JLCPCB provides high-precision stencils with options like step designs, electropolishing, and nano-coating to help ensure reliable solder paste deposition and reduce assembly defects.
An effective SMT stencil ensures consistent, repeatable and accurate solder paste printing. In this article we’ll explore practical and proven SMT stencil design tips. Which helps you optimize solder paste deposition and reduce defects in PCB assembly. This article basically consists of two parts, one is guidelines for design and other on a POV of manufacturing.
5 Key Design Guidelines for Standard SMT Stencils:
1. Aperture Design Guidelines
To prevent solder flaws like bridging and solder beads, this is crucial. For accurate deposition the apertures are made to be a bit smaller than the pads. However, for certain parts, an aperture with a specific design is required to deposit less paste on the inner edge of the part, which helps to prevent the formation of "mid-chip" solder balls. Here are a few instances:
2. Aperture Reduction (Pad-to-Aperture Ratio)
Apertures are frequently made slightly smaller than the actual pad dimensions in order to prevent bridging and extra solder. Here is a table of selection:
Recommended Thickness Rules:
- For most components, the typical reduction is between 5 and 7%.
- For dependable printability, IPC-7525 suggests a stencil-to-pad area ratio >0.66.
Formula:
Area Ratio = (Aperture Area) / (Aperture Wall Height × Aperture Perimeter)
Keep this ratio above 0.66 to ensure clean paste release.
3. Fiducial Marks
When printing solder paste onto pads, it is very important that the pattern is lined up correctly with the PCB. This is accomplished by applying fiducial marks, which are registration marks, to the PCB and stencil. As you can see from our most recent comprehensive piece on fiducial marks, adding them to the stencil will guarantee proper alignment. JLCPCB provides stencils with fiducial marks included, helping ensure accurate alignment and reliable solder paste printing.
4. Stencil Frame and Border
Stencils can be frameless (for rapid prototyping or manual printing) or framed (glued into aluminum frames).
- Typical frame dimensions are 23 x 23 inches.
- Keep the distance between the aperture area and the frame edge at least 10 mm.
- Mark the stencil's position, thickness, and part number clearly.
5. Window Effect design:
There are instances where the PCB design features big copper pads underneath the component. Devices that use power electronics typically experience this. In this case, a window effect is present to ensure a good electrical link and to let the device's heat escape. The device may lift and the outer leads may not solder if solder paste is placed over the entire pad. A "window effect" in the design can be used to decrease the solder volume, which is shared in the image above.
4 Key Design Guidelines for Standard SMT Stencils:
1. Stencil Thickness Selection
The thickness of the design determines how much solder paste is applied. Focus primarily on the smallest pitch component on the board. Solder paste may adhere to the inner walls of the aperture in a thick stencil because of a phenomenon known as surface tension. A basic rule is that there should ideally be at least five solder particles in the smallest aperture.
2. Stencil Material
The type of material used to make the stencil will determine how well it removes solder paste from the apertures. Even though stainless steel is typically utilized, PCB designs that use fine pitch components can employ nickel, which is around 50% more expensive than stainless steel.
The first generation of stencils were made by chemical etching, which was effective for larger apertures but became increasingly challenging to remove solder from as component sizes decreased. This resulted in the creation of laser-cut stencils, which enhanced paste release by producing a much finer, trapezoidal-shaped aperture. As component sizes shrank, the potential for electropolishing the aperture walls and, later, the method of electro-forming the stencil were developed.
3. Apply Nano-Coating for Improved Paste Release
Hydrophobic coatings are used in contemporary nano-coated stencils to lessen solder paste adhesion to the aperture walls. This is essentially a straightforward procedure used to apply a layer of nanomaterial on a plain stencil. What is this layer going to do? It increases solder paste release, prolongs stencil life, and lowers cleaning frequency.
4. Consider Step Stencils for Mixed Assemblies
This is further divided into two parts:
Step-up stencils: Thicker regions for larger components.
Step-down stencils: Thinner regions for fine-pitch components.
It is used with boards having 0201 passive components and large connectors. We have covered a full detailed article on this topic, see from here.
Conclusion
SMT stencil design is not just about cutting shapes in metal. It is a strategic process that directly influences yield, defect rates and assembly quality. By following these stencil design tips from optimizing thickness and aperture size to using advanced coatings you can significantly improve solder paste deposition. The fundamental principles of aspect ratio and area ratio provide the foundation for aperture sizing. And component-specific strategies ensure optimal performance across diverse assembly requirements. Advanced technologies such as step stencils and multi-print systems address complex applications. While proper process optimization and maintenance practices sustain long-term performance.
As SMT continues evolving toward miniaturization we have to follow IPC guidelines and leveraging technologies. Like nowadays nano-coatings and step stencils become essential for maintaining production quality and cost efficiency.JLCPCB offers a full range of customizable stencils, including nano-coated and step stencils, to help engineers achieve reliable and cost-effective SMT assembly.
Keep Learning
DFN Package Guide: Footprint, Soldering & Stencil Tips
Key Takeaways What a DFN is: A DFN (Dual Flat No-Lead) package is a leadless chip-scale IC package with connection pads on two opposing sides of its underside, usually plus a central exposed thermal pad. Assembly requirements: DFN joints sit hidden under the body, so it needs reflow soldering with a stencil and X-ray or AOI inspection, not hand soldering. Design essentials: Follow IPC-7351 land patterns and IPC-7525 aperture rules, use a thinner stencil foil around 0.1-0.12 mm, and segment the thermal......
Paste Mask vs. Solder Mask: What Each Layer Does (and Why It Matters)
Key Takeaways Two layers, opposite jobs: The solder mask is the physical polymer coating that insulates copper and keeps pads solderable, while the paste mask is data-only manufacturing information that never appears on the finished board. Opposite pad adjustments: A mask opening is drawn slightly larger than the pad (mask expansion) while a paste aperture is drawn equal to or smaller than the pad (paste reduction), and these mirror-image rules cause most of the confusion. The paste mask is the stenci......
BGA Stencil Design: Apertures, Thickness & Tips
On a ball grid array, every solder joint hides underneath the package where you cannot see it, touch it, or easily rework it. That is exactly why BGA stencil design decides whether the board works: the paste you print is the paste you get, and a print that is slightly too heavy or too light turns into hidden bridges, voids, or starved balls that only an X-ray will reveal. Get the stencil right and the joints reflow clean the first time. Get it wrong and you are chasing intermittent faults after assemb......
Stencil Aperture Design: Geometry, Area Ratio & Tips
Key Takeaways Stencil aperture design controls paste volume, deposit shape, and print registration — it's the key controllable variable in SMT print quality. As per IPC-7525B, two math rules are non-negotiable: stencil area ratio ≥ 0.66 and stencil aspect ratio ≥ 1.5. Aperture geometry is component-dependent: 1:1 with pad for BGA, window-pane splits for QFN/BGA thermal pads, home-plate shapes for 0201/01005 chips, and modest reductions for fine-pitch QFP. Aperture reductions intentionally decrease the......
Red Glue Stencil: Types, Thickness & Ordering Guide
Key Takeaways A red glue stencil deposits adhesive dots under component bodies, not solder paste on electrical pads. Its main use is holding bottom-side SMD parts during wave soldering of through-hole leads. SMT red glue is commonly dyed red so operators can confirm each deposit during inspection. Printable adhesive families include epoxy, acrylic, and UV- or dual-cure materials. Glue stencils are commonly thicker than paste stencils because the dot must reach the component underside. A custom o......
A Beginners Guide to Step-Up and Step-Down Stencils
As everyone knows, companies are moving down to 2nm, and electronics are at their peak right now. The component sizes of a PCB likewise drastically shrink during a ten-year period. From 1206, BGAs have shrunk to 0402, 0201, and even smaller. Due to the small size of the components and the requirement for high throughput, defects such as tombstoning, bridging, or poor connections may occur during the soldering process. To address these challenges, specialized stencil technologies such as step-up and st......