Order Custom Stencils for PCB Assembly: How to Make, Buy, and Choose the Right Supplier
4 min
- What Does It Mean to Order Custom Stencils for PCB Assembly
- How to Make and Buy Custom Stencils
- How to Choose a Custom Cut Stencil Company
Surface Mount Technology (SMT) stencils are essential tools in modern PCB assembly. They are thin sheets of metal, usually stainless steel, with precise cut-outs that allow solder paste to be applied accurately to PCB pads. The quality of the stencil directly affects solder paste deposition, which in turn impacts the reliability of the final assembled PCB.
Engineers often need to order custom stencils instead of relying on generic options. Every PCB design has unique pad layouts, component densities, and soldering requirements, so a one-size-fits-all stencil cannot ensure precise solder paste application. Custom stencils guarantee that solder paste is deposited exactly where needed, minimizing defects and improving production yield. Leading manufacturers like JLCPCB provide high-quality custom stencils that integrate seamlessly with their PCB production services, making it easy for engineers to get reliable results.
What Does It Mean to Order Custom Stencils for PCB Assembly
Definition of Custom SMT Stencils
Custom SMT stencils are stencils specifically designed to match a particular PCB layout. Unlike standard or generic stencils, they are tailored to the exact pad size, pitch, and geometry of the PCB components. This ensures that the right amount of solder paste is deposited on each pad, which is critical for solder joint quality and minimizing defects such as bridging or insufficient solder.

Why Engineers Order Custom Stencils
Engineers typically order custom stencils for several reasons:
High component density and fine-pitch designs require precise paste deposition.
Unique PCB layouts or specialized components cannot be reliably assembled using generic stencils.
Consistency and repeatability in production runs are necessary for commercial or large-scale manufacturing.
Companies like JLCPCB allow engineers to order custom stencils directly alongside their PCB orders, streamlining the process and ensuring compatibility.
Common Applications in PCB Manufacturing
Custom stencils are widely used in:
Consumer electronics, where small, high-density components are common.
Industrial equipment PCBs, requiring precise soldering for reliability.
Prototype and low-volume PCB production, where each layout may be unique.
How to Make and Buy Custom Stencils
How Custom Stencils Are Made

Custom stencils are usually fabricated from stainless steel using one of several methods:
Laser-cut stencils – precise and fast, ideal for high-density boards.
Electro-polished stencils – smooth aperture walls for consistent paste release.
Step stencils – used for boards with components of varying heights.
The stencil thickness and aperture design are calculated to match solder paste volume requirements. Professional stencil suppliers, including JLCPCB, provide advanced laser-cut and electro-polished stencils to ensure reliable solder paste application.
DIY vs Professional Custom Stencils
While hobbyists can attempt to make custom stencils using thin metal sheets and laser cutters, professional stencils offer:
Higher precision and repeatability.
Superior material quality (stainless steel with controlled surface finish).
Support for fine-pitch components down to 0.3 mm or smaller.
For critical PCBs or high-volume production, ordering professional custom stencils is strongly recommended.
How to Buy Custom Stencils Online or Locally
Engineers can buy custom stencils in two main ways:
Online suppliers – platforms like JLCPCB allow direct ordering with PCB designs, providing instant quoting and fast shipping.
Local suppliers – may offer faster turnaround for urgent orders, but often with limited options for step or fine-pitch stencils.
Searching for “custom stencils near me” can help locate nearby suppliers, but for consistent quality, a trusted online provider like JLCPCB is often preferred.

How to Choose a Custom Cut Stencil Company
Technical Capabilities to Look For
When selecting a custom cut stencil company, consider:
Laser cutting precision and aperture tolerance.
Ability to produce step stencils or multiple thicknesses.
Options for electro-polishing or anti-stick coatings.
Quality, Consistency, and Engineering Support
A reliable supplier should guarantee high-quality stencils with consistent aperture dimensions and smooth release properties. Engineering support is crucial for reviewing PCB files, optimizing aperture design, and preventing solder paste issue
Cost, Lead Time, and Scalability
Evaluate the total cost, including shipping, and the supplier’s lead time. Scalability is also important if you plan to increase production. Companies like JLCPCB combine competitive pricing with fast turnaround and global shipping, making them a convenient choice for both prototypes and volume production.
Ordering custom stencils is a vital step in achieving reliable PCB assembly. Custom stencils ensure precise solder paste deposition, reduce defects, and improve production yield. Whether you decide to make custom stencils yourself, buy custom stencils online, or search for “custom stencils near me,” selecting a professional and experienced custom cut stencil company is key.
For engineers looking for high-quality, convenient solutions, JLCPCB offers comprehensive services that allow you to order custom stencils alongside your PCB orders, ensuring compatibility, precision, and efficiency.

Keep Learning
How to Choose an SMT Stencil
What is an SMT stencil? SMT Stencil is a thin metal sheet used in the soldering process for SMT (Surface Mount Technology) and it plays an essential role in the SMT soldering process. Smt Stencil allows the direct placement of solder paste onto the SMD pads of PCB, which can help prevent errors and defects during the reflow soldering process. This results in a precise amount of tin coverage once the work is completed. Types of SMT Stencils Depending on the application of solder paste, there are three ......
DIY PCB Stencil: How to Make a Solder Paste Stencil
Key Takeaways DIY is possible: You can make a working solder paste stencil from Kapton, Mylar, or vinyl using a craft knife, vinyl cutter, or laser for larger SMD components and low-volume prototyping. 0.5 mm pitch is the practical boundary: DIY stencils work well above 0.5 mm pitch but struggle with finer QFNs, QFPs, and BGAs due to poor aperture quality and paste release. Match thickness to your smallest pad: Use 0.10–0.15 mm (4–6 mil) sheet stock, choosing thinner material for smaller pads and thic......
Order Custom Stencils for PCB Assembly: How to Make, Buy, and Choose the Right Supplier
Surface Mount Technology (SMT) stencils are essential tools in modern PCB assembly. They are thin sheets of metal, usually stainless steel, with precise cut-outs that allow solder paste to be applied accurately to PCB pads. The quality of the stencil directly affects solder paste deposition, which in turn impacts the reliability of the final assembled PCB. Engineers often need to order custom stencils instead of relying on generic options. Every PCB design has unique pad layouts, component densities, ......
Custom Stencils for PCB Assembly: Design, Ordering, and Usage Guide
Have you ever faced solder bridging or insufficient solder issues that ruined an entire production batch? In many cases, the problem is not the pick-and-place machine, but the very first step of the process: solder paste printing. This is where custom stencils make the difference between a reliable product and one that requires extensive rework. Unlike rigid standard stencils, a custom SMT stencil gives engineers full control over solder paste volume, allowing precise adjustment to match increasingly ......
SMT Stencil Thickness Guide 2026: How to Choose the Right Solder Paste Stencil
In SMT assembly, the stencil quietly decides whether a production run succeeds or fails. Problems like bridging, tombstoning, and insufficient wetting are frequently traced back not to PCB design errors, but to incorrect stencil selection or poorly controlled paste volume. Quick Answer: How to Choose a Solder Paste Stencil If you need to define your stencil parameters immediately, follow this quick decision guide: Select thickness based on component pitch: Use component density as your primary baselin......
Custom Cut Stencils for PCB Assembly: How to Cut, Use and Choose the Right PCB Stencil
Custom-cut stencil and Solder paste printing are two of the most vital processes in Surface Mount Technology (SMT) PCB assembly, concerning solder joint quality, electrical performance, and product reliability over time. SMT stencils are used to deposit solder paste in accurate amounts onto PCB pads, or for depositing and compressing adhesive pastes which are arranged in the form of a column on components such as connectors and sockets. While PCB designs have seen a trend toward increased density, fin......