Role of a Circuit Simulator in Electronics Design
8 min
- What is Circuit Simulation?
- Need for Circuit Simulation:
- Types of Circuit Simulation:
- Levels of Simulation:
- Types of Analysis in Simulation:
- Advantages of Circuit Simulation:
- Popular Simulation Software:
- Conclusion:
Making electronic and electrical circuits can be time-consuming and technologically demanding, not to mention expensive. After creating an electronic circuit, designers must test the circuit’s functionality in order to confirm its functionality and make any necessary adjustments. What if, instead of creating the circuit with real board and components, we were able to obtain a mathematical description of the circuit? This is the idea behind Circuit Simulation. We will go over the subject in this article and take a look at various types of circuit simulations.
It should come as no surprise that the growth of circuit simulation, both in sophistication and power, has vastly increased productivity during design. The result is not just faster development speeds, but also more thorough designs due to the ease at which users can quickly build, probe, and analyze circuitry. Whether proof-of-concept or revision, circuit simulation provides an indisputable framework for modern PCB design. In this way test and verify the performance of different components replacing them in the circuit. See what type of electronics components and symbols are there on which we can run simulations, and how they work.
What is Circuit Simulation?
Due to the huge amount of appliances, devices and gadgets that are released day-to-day it is essential to ensure a smooth manufacturing process, and also adhere to different standards of technology and rules. Not only in the PCB design but the simulation plays a very important role in every sector of engineering. In electronics we create a mathematical model of a circuit in order to study the performance of the circuit, without actually making it (with actual, tangible components). This method of modeling circuits using mathematical equations to verify and check the circuit’s design for electronic and electrical circuits is referred to as Circuit Simulation.
When we evaluate circuit simulation against other kinds of simulation like Logic Simulation and Functional Simulation It employs a detailed physical model (in the shape of mathematical equations) of the various circuit components to solve complicated algebraic and differential equations. The result is a precise simulation using precise time waveforms of node voltages as well as component currents. So at a basic level a simulator is solving mathematical equations and then giving results in the form of different plots.
Need for Circuit Simulation:
It is obvious that with circuit simulation, we are able to evaluate the capabilities of circuits without making the circuit.
- Cost effectiveness: Circuit simulation is cost effective as well as time-saving. We can quickly design complicated circuits with the help of the software. This can save design engineers and businesses a significant amount both time and cash.
- Easy verification: We are able to easily redesign the circuit based on simulation results. Each stage of simulation and design, engineers can check the performance of the circuit and compare it with the theoretical response.
- Easy modifications: Circuit Simulation Software is the beginning point for a new idea or concept. It is also possible to modify existing ones without creating PCBs.
Like physical probing and watching the waveforms of an oscilloscope you can perform similar things in circuit simulation. It is easy to probe various locations in a circuit and see the waveforms in the simulation.
Types of Circuit Simulation:
Let's now look at different kinds that circuit simulations can be found. Simulation can be classified into the following three ways:
1) Analog Circuit Simulation
2) Digital Circuit Simulation
3) Mixed-Mode Circuit Simulation
1) Analog Simulation:
Like the name implies, analog simulations typically employ the analog component and signal. In this type of simulation the mathematical models have to be extremely precise to operate in the frequency domain (AC) and temporal domain (transient) and non-linear quiescent (DC) modes. SPICE FastSPICE and FastSPICE are two well-known analog simulators that make use of extremely precise linear and non-linear component models to study the circuit’s behavior.
2) Digital Simulation:
When we contrast the intricate mathematical models of analog simulators with digital simulators, they are comparatively straightforward. HDL like Verilog and VHDL constitute the foundation for digital simulation. In contrast to analog simulators, in which we require continuously changing signals and signals, in digital simulation we are actually working using two distinct voltage levels. When we talk about digital electronics, they refer to them as Logic 0 and Logic 1. Only functional check is not done here, but the STA (static timing analysis) plays an important role. Which helps in determining the setup, hold and max propagation delay.
3) Mixed-Mode Simulation:
It’s a blend of both digital and analog simulations. This type of simulation can be highly beneficial for mixed circuit system design and analysis. Through the mixed-mode simulation, the digital and analog parts are distinct entities that have their own instruments and sources.
Levels of Simulation:
In the last section, we discussed various types of simulation circuits. These types define the nature of the circuit, as well as the analysis steps that we must follow. You can also specify various levels of simulation, by the abstraction and complexity of circuits.
Block-Level Simulation: The simulation we used separated the functional parts into different blocks and performed simulation on the blocks in a unified manner. This is vital to a modular design, and assists in the reuse of functional blocks already in place in other circuits.
Chip-Level Simulation: The name suggests In a chip-level simulator it is the case that we take one integrated circuit (a chip) and model its function as a single unit. This helps ensure that the chip operates in the way it was intended to.
Types of Analysis in Simulation:
1. Transient Analysis:
This simulation examines circuit behavior over time, helping engineers understand signal fluctuations, startup conditions, and time-dependent behaviors. The output is plotted with respect to time.
2. AC Analysis:
AC analysis is used to study frequency response and stability, particularly in amplifiers and filter designs. The output is plotted with respect to frequency sweep.
3. DC Analysis:
DC analysis helps evaluate steady-state voltage and current levels, ensuring proper biasing and power distribution. Used to find the DC biasing conditions and operating point of transistors and MOSFETs.
4. Thermal Simulation:
Thermal analysis predicts heat dissipation and temperature rise in components, essential for reliability in high-power applications. Thermal analysis plays a crucial role in designing several thermal independent circuits inside an IC.
Advantages of Circuit Simulation:
The majority of the most popular circuit simulation software like SPICE, LTspice etc. are available for free. There are some tools that are proprietary however, they are all developed with the SPICE algorithm.
- Testing of Memory Related Processes: Specifically designed analog simulation allows the speed and latency of memory related processes to be analyzed.
- Troubleshooting Made More Efficient: In terms of time, discovering and troubleshooting a faulty circuit digitally requires far less time than it would take to solve the values (e.g. voltage, current, and power) by hand.
- Noise and Crosstalk modelling: Simulators are also available to study cross talk in more complex RF as well as high speed designs.
In addition to regular circuits simulators also come with tools to test designs for power supply (SMPS) or power distribution networks. Digital Simulators monitor the voltage levels of logic 0, and when using Analog Simulators. you can measure the time of the change between these levels of logic.
Popular Simulation Software:
There are a variety of circuit simulator software and tools available on the market. SPICE, which stands for Simulation Program With Integrates Circuit emphasis, is a well-known circuit simulator. The University of Berkeley’s Electronics Research Laboratory developed this software initially for the U.S. Department.
Because it's an open-source software, it has become popular among other designers who developed their own simulators with SPICE algorithms. One of these tools is LTspice. Another very popular SPICE circuit simulator that is based on SPICE is the NI’s Multisim. It is, however, different from LTspice; it's an expensive software. Here are a few well-known circuit simulators.
- SPICE
- Ngspice
- LTspice (SPICE)
- PSIM
- Multisim (SPICE)
- Cadence Spectre
- Synopsys PrimeSim (SPICE and FastSPICE)
Conclusion:
Circuit Simulation is a crucial part of creating electronic products. With the aid of simulators, you are able to create electronic and electrical circuits, check their operation as well as analyze their performance. You can make the necessary adjustments prior to proceeding with the manufacturing. This helps companies save a lot of time and cash. In this article we looked at the fundamentals about Circuit Simulation and its advantages. We also looked at different kinds of circuit simulation, as well as several popular simulator programs.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......