Role of Impedance Equation in High Speed Designs
5 min
- Impedance vs Resistance, Inductance, and Capacitance
- What is Impedance?
- The Triangle of Impedance
- Factors Affecting Impedance in PCB Design:
- What is Characteristic Impedance?
- Using JLCPCB Impedance Calculator:
- Conclusion
Impedance is one of the most important ideas that controls how signals behave in systems. Signal integrity issues arise from reflections in the signal caused by impedance mismatches. To guarantee that there is no signal loss, reflection, or distortion, engineers must carefully control impedance. The resistance of an electric circuit to the application of alternating current is measured by its impedance. It is the result of combining high-frequency induction and capacitance in an electric circuit. Like resistance, impedance is measured in ohms. Different impedances cause attenuation and reflections, which weaken the signal. The definition of impedance, its differences from other circuit factors such as resistance, inductance, and capacitance, and the significance of its equation for high-speed PCB design are all covered in this article.
Impedance vs Resistance, Inductance, and Capacitance
Impedance is the total equivalent resistance that prevents current from flowing through circuits that contain resistors, inductors, and capacitors. Reactive and resistive components make up impedance. The energy in a circuit is released as heat by resistors. The electromagnetic fields that surround and penetrate conductors, inductors, and capacitors in a circuit contain the recoverable energy.
Depending on the circuit architecture and frequency, impedance combines all of these features. Inductance and capacitance only play a role in AC circuits. But resistance influences both DC and AC circuits. The following parts provide the equation and diagram depiction.
What is Impedance?
The symbol Z stands for impedance, which is the amount of resistance an AC circuit poses to its flow. It contains both reactive (imaginary) and resistive (actual) components. Impedance changes with frequency because of inductance and capacitance. Whereas resistance opposes current consistently. Like resistance the impedance is also measured in ohms (Ω), but it also includes phase shift and frequency dependency.
The general formula for impedance in an AC circuit is:
Z = R + jX
- R is resistance,
- X is reactance (which can be inductive or capacitive),
- j is the imaginary unit (√-1), and
- ω (omega) is the angular frequency (2πf)
Here, jw (or jω) represents the frequency-dependent component of the impedance. It signifies that the impedance changes with the signal's frequency due to the reactive components. The reactance part can be further expanded as:
- For an inductor: Xl = ωL = jwL
- For a capacitor: Xc = -1/ωC = -j/(wC)
The Triangle of Impedance
In a vector diagram, impedance is often represented as a triangle:
- The horizontal axis shows resistance (R)
The vertical axis shows reactance (X) - The hypotenuse represents the magnitude of impedance (|Z|)
Helps in visualizing how the total impedance is due to resistance versus reactance.
Factors Affecting Impedance in PCB Design:
What is Characteristic Impedance?
Characteristic impedance (Z0) refers to the impedance of a transmission line. It exhibits when it is infinitely long or properly terminated. It remains constant regardless of the trace length as long as the cross-sectional and dielectric properties remain the same. A sudden change in impedance causes part of the signal to reflect back. This is vital for designing transmission lines that carry high-speed digital signals without reflections. It can corrupt data integrity. It is not influenced by length but determined by the geometry and materials of the PCB trace:
Z0 = √((R + jωL)/(G + jωC))
In practical high-speed PCB designs, R and G (conductance) are often negligible, so it simplifies to:
Z0 ≈ √(L/C)
Characteristic impedance is typically set at standard values like 50Ω (single-ended) or 100Ω (differential). And sometimes for USB differential pair data routing the value is taken 90Ω.
Using JLCPCB Impedance Calculator:
Launch the "Impedance Calculator" in JLCPCB, choose the appropriate layer stack-up, and enter the impedance values along with other pertinent data such board thickness. In your engineering data, create the appropriate line width and spacing.
Important Manufacturer's Note: Our factory will manage the impedance within a tolerance of ±10% for orders with "Impedance Control" chosen as "Yes." Selecting "No" will not allow us to regulate the impedance, but we will make sure that the line width and spacing are within a +/-20% tolerance. Double-sided boards do not currently have impedance control.
Conclusion
A key component of high-speed PCB design is the impedance equation. Knowing the formation, calculation and measurement of impedance. This will lessen jitter and assist engineers preserve signal integrity. In order to attain the intended impedance values and expedite the design process, impedance-controlled lines and tools such as JLCPCB's Impedance Calculator can be used.
The optimum value you determined from a schematic may not match the impedance signals seen on an actual PCB layout. The existence of the substrate and the tracing layout of the board are the primary causes of this. Crosstalk is one effect of this that deviates from the ideal impedance levels. Circuits that switch at high frequencies may experience problems with power integrity, such as ringing. The impedance of your power delivery network will also deviate from the ideal capacitive behavior at higher frequencies, which could lead to problems with both power and signal integrity.
Popular Articles
Keep Learning
Navigating the Impedance Landscape: Selecting the Right Impedance for USB, Ethernet, HDMI, and SD Card Interfaces
Introduction In the realm of high-speed digital communication, choosing the right impedance is a critical aspect of successful PCB design. Impedance matching ensures optimal signal integrity, minimizes reflections, and enhances the overall performance of interfaces such as USB, Ethernet, HDMI, and SD Card. In this blog post, we'll explore the importance of impedance, the factors influencing impedance selection, and best practices for ensuring reliable data transmission in these widely used interfaces.......
Understanding Impedance Formulas for Accurate PCB Design
Complex Impedance: Z = R + jX combines constant resistance with frequency-dependent reactance. Frequency Behavior: Inductive reactance rises with frequency while capacitive reactance falls. Circuit Rules: Impedances add directly in series, while parallel networks sum admittances (Y = 1/Z). Trace Impedance (Z0): Depends on cross-section and dielectric properties, not trace length. Stackup Verification: Always confirm calculated trace widths with your fabricator's stackup and solder mask data. An impeda......
A Beginners Guide to Impedance Control in PCBs
When a digital signal is transmitted from one point to another, it causes a change in the state of the signal line. This change can be understood as an electromagnetic wave moving through the circuit. Reflection occurs when this wave encounters a boundary between different mediums. At this boundary, some of the wave's energy continues as a signal, while the rest is reflected. This process repeats until the energy is either absorbed by the circuit or dissipated into the environment. For electrical engi......
Design Guide for USB-3.0 Differential Signaling
In the world of data transfer, USB 3.0 is the Usain Bolt to USB 2.0’s friendly jogger. USB 2.0 is called “High Speed” and limped along at 480 Mb/s, whereas USB 3.0 SuperSpeed rockets up to 5 Gb/s (over ten times faster). But this speed jump brings full‑duplex operation and new differential transmit (SSTX) and receive (SSRX) pairs on dedicated pins. USB 2.0 D+/D– lines handle enumeration and legacy data, while two new 5 Gb/s high‑speed differential pairs carry SuperSpeed data in each direction. While m......
Can PCB Simulation Prevent Costly Manufacturing Revisions?
Key Takeaways PCB simulation identifies electrical, thermal, and EMC issues before fabrication, helping reduce costly design revisions. Signal integrity, power integrity, thermal, and EMC analysis address different PCB performance risks. Accurate simulation depends on matching the model to the actual stackup, materials, and manufacturing limits. Combining simulation with DRC checks and prototype testing helps ensure reliable, manufacturable PCB designs. PCB simulation is the practice of predicting how......
EMC Design for PCB: EMI, EMS, Testing Standards & Compliance Guide
Key Takeaways EMC design means controlling both EMI (unwanted emissions) and EMS (immunity to external disturbances); a board that meets emission limits but resets during an ESD test has not achieved EMC. Every interference problem can be analyzed with the source–path–victim model, and solved by reducing the source, interrupting the path, or hardening the victim. Core PCB techniques include minimizing current-loop area, maintaining continuous reference planes, controlling impedance, decoupling power p......