What is Attenuation: How Signal Weaken Over Distance
7 min
- What is Attenuation? Meaning & Definition
- Different Types of Variable Attenuators:
- Causes of Signal or Cable Attenuation
- Preventing of Improving Attenuation Rate
- How to Calculate Signal Attenuation?
- Why does the Signal Attenuate When it Travels in Wire?
- What Causes Signal Attenuation in PCBs?
- Other Ways to Reduce Signal Attenuation?
- Design Tips for Better Signal Integrity:
- Conclusion:
As a signal travels from the source to the load through PCB conductors, the signal is attenuated due to trace resistance and dielectric losses, resulting in energy loss. Signal attenuation is the most common term used when high-speed signals travel across a circuit board. It is one of the major contributors to signal degradation that leads to signal integrity issues. Usually more attenuation can be seen at higher frequencies due to phenomena like skin effect.
The attenuation factor determines how far a signal can travel and still provide enough data bits or information. It quantifies different transmission media based on how the amplitude of the transmitted signal decreases with frequency. It is given by:
AF = P output/P input
The signal attenuation coefficient depends on:
- Transmission medium length
- Transmission media materials
- Physical conditions
What is Attenuation? Meaning & Definition
Attenuation is the reduction in the amplitude of a signal as it travels through a medium. Attenuation can be caused by transmission loss, reflection, or absorption. In an electrical system, attenuation is a decrease in voltage as it flows along a wire or other transmission line. Attenuated systems can also be referred to as degraded systems.
Attenuation is expressed in decibels (dB) and represents the ratio of output to input power or intensity. Attenuation values can range from zero decibels for an unobstructed or perfect transmission, to extremely large negative numbers. A perfect attenuator with 0 dB of attenuation has an infinite number of taps along the transmission line.
Different Types of Variable Attenuators:
Causes of Signal or Cable Attenuation
When we talk about signal or cable attenuation, we are talking about signal degradation between a transmitter and receiver. Signal loss can be caused by many variables that affect cable quality, such as:
- Poorly manufactured fiberoptics (bad connectors and poor splices)
- Excessive bending of the cable. This causes signal reflections.
- Operating at higher signal wavelengths.
- Long signal cable runs between transmitter and receiver (attenuation increases over signal cable length).
Preventing of Improving Attenuation Rate
There are several ways to prevent or improve attenuation. The most common ways are to:
1) Use a Physical Barrier: Prevents two conductors from touching and shorting out.
2) Use a Preamplifier: Boosts signal strength before it reaches its destination, reducing signal loss.
3) Use a Balun: Increases the distance between two conductors to prevent short circuits.
4) Increase Signal Strength: Helps prevent attenuation and ensures reliable transmission.
5) Multiple Methods for Signal Boosting: Various techniques can be used to maintain signal integrity.
How to Calculate Signal Attenuation?
Signal attenuation is estimated in decibels (dB) per unit length of the transmission medium. It can be calculated in terms of power and voltage.
To avoid the chance of fading, multiple signals are sent to ensure that at least one reaches the final destination, the receiver. But due to the need to send these extra signals, this approach slows down the overall network speed. The lower the attenuation, the more efficient the transmission medium is. Higher attenuation means more signal loss and reduced amplitude on the receiver side.
Why does the Signal Attenuate When it Travels in Wire?
The amplitude of the signal is distorted by trace resistance and the dissipation factor of the circuit board dielectric. This effect is more prominent at high frequencies since signals tend to propagate along the trace surface. Attenuation causes slower signal rise times and increases the likelihood of data errors.
Dielectric absorption: When high-frequency signals propagate across the surface of a circuit board, dielectric materials absorb the signal energy. It reduces signal strength which can only be controlled by choosing the perfect PCB material. Choose materials with low loss tangent to reduce dielectric absorption.
Skin Effect: Skin effect is a phenomenon where high frequency components start to propagate closer to the outside of a circuit board conductor rather than to the inside. High frequency signals have their own self-inductance value, which induces increasing inductive reactance as the frequency increases. It is responsible for reducing the conductive area of the PCB surface. Skin effect can be reduced by increasing trace width (surface area), but this is not always possible because changing trace geometry can cause impedance issues.
What Causes Signal Attenuation in PCBs?
As the signal range increases, so does the attenuation. Factors like low trace width
And crosstalk also plays a role in signal attenuation. Some factors listed below are responsible for signal attenuation:
Transmission frequency: The shorter the wavelength, the greater the attenuation of radio waves. Such signals are transmitted via 2.4GHz or 5GHz electromagnetic waves. Electromagnetic waves have high frequencies and short wavelengths. Therefore, radio signals have large attenuation and cannot be transmitted over long distances.
Resistive losses associated with conductor materials: The conductive materials used to manufacture transmission lines, such as copper, introduce resistive losses that cause attenuation of signals traveling on copper traces.
Losses Related to Dielectric Materials: Dielectric losses are introduced by losses in the dielectric material sandwiched between transmission lines. This dielectric loss creates a conductance in the substrate, also known as reverse resistance, and absorbs some of the propagated signal energy, causing signal attenuation.
Copper Surface Roughness: Copper surface roughness on a PCB also acts as a resistance to signal propagation. Rough copper traces increase resistance because the topography of the copper surface moves the signal up and down. Surface spikes also increase capacitance. Smooth copper is a solution to this problem, but is more expensive.
Other Ways to Reduce Signal Attenuation?
Signal attenuation can be mitigated using the following techniques:
Use a repeater: If the received signal is weak, use a repeater to regenerate the original signal by reducing attenuation. It also enhances the range of the signal, allowing it to transmit longer distances without failure.
Use an Amplifier: If the received signal is weak, an amplifier is used to increase its amplitude, unlike a repeater which regenerates the entire signal.
Proper material selection: Careful selection of low-loss dielectric materials and low-resistance traces can minimize signal attenuation.
Use programmable differential output voltage (VOD) settings: Programmable VOD ensures drive strength is synchronized with line impedance and trace length. Increasing VOD at the driver enhances the signal at the receiver.
Pre-emphasis: Using amplifiers to increase signal strength is not the only solution for attenuation control, as it also amplifies the associated signal noise and jitter. Pre-emphasis only enhances the high-frequency components of the signal by increasing the level of the first transmitted symbol. If subsequent symbol levels are transmitted at the same level, they will remain unchanged. For example, if a signal transmits a high level for three symbols, only the first symbol is emphasized. The next two symbols will be transmitted at the usual levels.
Design Tips for Better Signal Integrity:
- Place the antenna closer to the source.
- Improve conductivity by wiring together different materials.
- Make sure that there is nothing interfering with the signal.
- Place antennas far away from any metallic objects.
- Use a power amplifier for stronger signals if needed.
Conclusion:
Signal attenuation is a critical factor in high-speed PCB design, impacting signal integrity and overall system performance. As signals traverse transmission lines, they experience losses due to trace resistance, dielectric absorption, skin effect, and material properties. These losses become more significant at higher frequencies, leading to degraded signal quality and potential data errors.
By carefully designing PCB layouts with attenuation in mind, including proper grounding, impedance matching, and controlled trace geometry, engineers can enhance signal integrity and reduce performance degradation. As electronic systems continue to push the boundaries of speed and complexity, addressing signal attenuation remains a crucial aspect of maintaining efficient and reliable communication within circuits.
Popular Articles
Keep Learning
How Impedance Controlled Routing Delivers Reliable High-Speed PCB Performance
Key Takeaways Impedance Controlled Routing is essential for reliable high-speed PCB performance above 1 Gbps, eliminating reflections, ringing, and bit errors by precisely targeting interface-specific impedances (USB 90 Ω, PCIe 85 Ω, DDR4 40/80 Ω, HDMI 100 Ω) through field-solver calculations, symmetrical stackups with continuous reference planes, stable low-loss dielectrics, and strict single-ended/differential routing rules. Manufacturing precision in etching, copper profile, and lamination, verifie......
Understanding Impedance Matching for High-Speed PCB Designs
With the advancement of technology and the ever wider application of integrated circuits, the frequency and speed of electronic signal transmission have been increasing, making it essential for PCB conductors to provide high-performance transmission lines. These transmission lines are responsible for delivering signals from a source to the input of a receiver accurately and completely. This requirement emphasizes the need for impedance matching. Electrical impedance, commonly represented as Z and meas......
Keeping Your PCBs Cool : Practical Heatsink Strategies for Better Thermal Performance
The current PCBs are becoming insane, and hence the cooling of PCBs is absolutely necessary. Large power components such as CPUs, GPUs, SOCs, voltage regulators, and LED drivers all ooze heat as a side-effect of their operation. Therefore, as an example, it is common to have CPUs, GPUs, or SOCs with their own heatsink, or boards that are extremely dense or contain power items such as motors, power transistors, amplifiers, regulators, etc., can end up in hot spots. A small PCB may become hot whena lot ......
EMI Shielding for PCBs : Advanced Techniques and Materials for Superior Electromagnetic Compatibility in Professional Fabrication
In essence, EMI shielding is simply the act of enclosing any conductive or magnetic material to ensure the electrical and magnetic fields do not creep in or out of a particular zone on your PCB. Imagine that you had a Faraday cage around your delicate circuits, except that you have to shield not yourself, but your neighbor, against your noisy switching regulator (and the other way around). Modern electronics have become a massive nightmare due to EMI. With clock speeds in the GHz and switching regulat......
How to Determine a Circuit's Impedance: Key Facts & PCB Applications
Determining the impedance of a circuit is critical for analyzing behavior and optimizing performance in high-speed and RF designs. Impedance (unlike simple resistance) includes both resistance and reactance, making it essential in PCB design and PCBA manufacturing. In this article, we explore the impedance formula, impedance matching, microstrip calculations, and how JLCPCB's free impedance calculator helps designers achieve reliable results with ±10% tolerance. What is the difference between impedanc......
Differential Pairs on PCBs: Best Practices for Routing, Impedance Control, and Signal Integrity
High-speed digital designs increasingly rely on differential pairs to transmit data reliably at rates from several Gbps to tens of Gbps. These paired traces carry signals of equal magnitude but opposite polarity, allowing receivers to reject common-mode noise while preserving the differential signal. Engineers use differential pairs for interfaces like USB, HDMI, PCIe, and Ethernet because they provide superior noise immunity and reduced EMI compared to single-ended traces. Introduction: The Importanc......