What Is a Flexible Heater? A Complete Guide
8 min
- What Is a Flexible Heater?
- How Does a Flexible Heater Work?
- Types of Flexible Heaters
- Polyimide vs Silicone Rubber Heaters
- How to Choose the Right Flexible Heater
- Common Applications
- Specifications Needed for a Custom Heater
- How to Order a Custom Flexible Heater
- Frequently Asked Questions About Flexible Heaters
Flexible heaters provide customizable heating for applications where space, shape, or installation conditions make conventional rigid heaters difficult to use. But different materials offer different specifications, so selecting the right heater requires more than choosing a size and target temperature.
This guide explains what flexible heaters are, how they work, the main types available from JLCPCB, and the differences between polyimide and silicone rubber heaters. It also covers common applications, key customization specifications, and the steps for ordering a custom flexible heater.
What Is a Flexible Heater?
A flexible heater is a thin, bendable resistive heating element laminated between flexible insulation such as polyimide or silicone rubber. It provides precise temperature control in compact or complex spaces and can conform to flat, curved, or irregular surfaces.
When electric current flows through its etched-foil or wire element, resistance generates controlled heat across flat, curved, or irregular surfaces.
Polyimide heaters are best for thin, fast-response applications, while silicone rubber heaters suit harsher, wetter, and more mechanically demanding environments.
How Does a Flexible Heater Work?
A flexible heater converts electrical energy into heat through resistance heating. Electricity flows through a resistive element embedded within a flexible insulating substrate. As the current meets resistance, the element generates heat and distributes it across the heater surface.
A typical flexible heating element uses an etched metal foil laminated between insulating layers under high temperature and pressure. The resistive core is usually made from copper, stainless steel, or iron-chromium-aluminum alloy.
Types of Flexible Heaters
Flexible heaters can be classified by their insulating material. JLCPCB offers two primary options: polyimide flexible heaters and silicone rubber flexible heaters.
Polyimide Flexible Heaters
Polyimide (PI) provides heat resistance, electrical isolation, mechanical strength, and a thin profile. A polyimide heater, also commonly described as a PI heating film, is suitable for applications that require a thin and lightweight flexible heating element.
Silicone Rubber Flexible Heaters
Silicone rubber provides high-temperature resistance, moisture resistance, and electrical insulation. It maintains resilience and stability across electrical, thermal, mechanical, and environmental conditions.
For a more detailed material discussion, see choosing insulating materials for flexible heaters.
Common Features of Flexible Heaters
• Customizable and Flexible: A flexible heater can be customized in size, shape, wattage, and temperature and can conform to curved or irregular surfaces.
• Thin and Lightweight: Its low-profile construction allows it to fit into compact or limited spaces.
• Reliable and Consistent: With no moving parts, a flexible heater can provide stable heat output in demanding applications.
• Rapid and Uniform Heating: Flexible heaters can provide fast heat-up and uniform heat distribution across the surface.
• Simple Installation: Flexible construction and optional adhesive backing, such as 3M™, support mounting on flat or curved surfaces.
Polyimide vs Silicone Rubber Heaters
The main differences between polyimide and silicone rubber flexible heaters include substrate thickness, operating temperature, insulation resistance, power density, thermal conductivity, and mechanical compressive strength. The following specifications are based on the product data supplied for this article.
| Specification | PI Flexible Heaters | Silicone Flexible Heaters |
|---|---|---|
| Substrate Thickness | 0.09–0.27 mm | 1.0–2.0 mm (including silicone layer) |
| Light Transmittance | 60.2% (for 50 μm PI film) 70.6% (for 25 μm PI film) | 0% |
| Operating Temperature Range | -40°C to 260°C (recommended long-term use: below 150°C) | -40°C to 300°C (recommended long-term use: below 200°C) |
| Dielectric Strength | 1–380 VAC / 2000 VDC, 1-minute test leakage current ≤ 1 mA | 1–380 VAC / 2500 VDC, 1-minute test leakage current ≤ 1 mA |
| Insulation Resistance | ≥100 MΩ @ DC 1000 V | ≥500 MΩ @ DC 1500 V |
| Max. Power Density | 1.0 W/cm² | 2.0 W/cm² |
| Thermal Conductivity | 0.2–0.35 W/(m·K) | 1.0–1.5 W/(m·K) |
| Mechanical Compressive Strength | ≤50 kg/cm² | ≥200 kg/cm² (typically up to 350 kg/cm²) |
| Lead Wire Pull Strength | ≥100 N | ≥100 N |
| Service Life | Up to 5 years | Up to 5 years |
| Solder Joint Pull Strength | ≥40 N | ≥40 N |
How to Choose the Right Flexible Heater
Choose the flexible heater material according to the available installation space, required operating temperature, power density, mechanical conditions, and application environment. Use the verified specifications in the comparison table when evaluating a design.
| Application Requirement | Polyimide Flexible Heater | Silicone Rubber Flexible Heater |
|---|---|---|
| Thin, lightweight construction | Preferred option | Thicker construction |
| Compact or limited installation space | Suitable | Confirm available space |
| Moisture and demanding environmental conditions | Confirm application requirements | Suitable |
| Higher mechanical compressive strength | Refer to the verified specification | Refer to the verified specification |
| Higher maximum power density | Up to 1.0 W/cm² | Up to 2.0 W/cm² |
Before making a final selection, confirm the voltage, wattage or resistance, dimensions, target temperature, adhesive backing, lead wire, and installation conditions with the JLCPCB Flexible Heater team.
Common Applications
Flexible heating elements are used across aerospace, automotive, medical, consumer electronics, industrial equipment, energy, marine, and transportation applications.
Polyimide Flexible Heater Applications
• Aerospace: dashboards, avionics heating, fuel-line heating, sensor protection, optical systems, and de-icing systems
• Automotive: mirror defogging, battery-pack thermal control, and wiper-blade heating
• Medical devices: diagnostic instruments, laboratory equipment, sample trays, reagent bottles, IV tube warmers, blood warmers, incubators, medical imaging systems, and CPAP machines
• Consumer electronics: battery warming in cameras, phones, and laptops, heated beauty devices, and hand warmers
Silicone Rubber Flexible Heater Applications
• Industrial equipment: machinery-component temperature control, platen heating, process-tank warming, pump and valve freeze protection, and conveyor-belt de-icing
• Energy systems: solar-panel snow melting, wind-turbine blade de-icing, energy-storage thermal management, and fuel-cell heating
• Marine and boating: boat-hull de-icing, engine-block heating, bilge-pump freeze protection, and marine-electronics thermal management
• Transportation: pipe freeze protection, engine-component preheating, fluid-reservoir warming, and battery-pack thermal control
Specifications Needed for a Custom Heater
Prepare the following information when requesting a custom flexible heater design or quotation:
• Heater material and dimensions
• Voltage and power or resistance
• Required temperature
• Adhesive backing requirements
• Lead-wire requirements
JLCPCB recommends uploading Gerber files in ZIP or RAR format or CAD drawings in DXF or DWG format. The maximum file size is 100 MB. For additional parameter guidance, use the JLCPCB flexible heater design guide.
How to Order a Custom Flexible Heater
1. Visit the JLCPCB Flexible Heater Website
Go to the JLCPCB custom flexible heater platform, log in to your account, and start a new order.
2. Configure the Specifications
Select the material, dimensions, voltage, power or resistance, temperature, adhesive backing, and lead wire. Upload the recommended production files or CAD drawings.
3. Review and Place the Order
Confirm the selected parameters, proceed to checkout, and choose a shipping method based on the required timeline and budget.
Before production starts, JLCPCB engineers will reprocess and manually confirm the production files. The lead time will be recalculated after confirmation.
Why Choose JLCPCB Flexible Heaters?
• One-Stop Heating Customization: JLCPCB provides free circuit design support and heating-solution consultation to help customers design and validate prototypes.
• Competitive Price: Under the same area conditions, JLCPCB Flexible Heaters can reduce costs by more than 90% compared with typical custom-heater market quotations.
• Rapid Prototyping: There is no MOQ limit, and shipping can be as fast as three business days.
• Instant Online Quotes: Upload a design and select the required materials and specifications to receive an online quotation.
• Precision and Flexibility: Available specifications include 0.5–1.0 mm dimensional tolerance and ±5% resistance value tolerance.
• Inspection Options: JLCPCB offers visual inspection and individual resistance testing according to the options selected for the order.
Submit your files and specifications through the JLCPCB Flexible Heater website to request a quote or begin an order.
Frequently Asked Questions About Flexible Heaters
1. What is a flexible heater?
A flexible heater is a thin, bendable heating element that converts electrical energy into heat through resistance heating. It can conform to flat, curved, or irregular surfaces.
2. What are the main types of flexible heaters offered by JLCPCB?
JLCPCB offers polyimide flexible heaters and silicone rubber flexible heaters. They differ in thickness, temperature range, power density, thermal conductivity, insulation resistance, and mechanical compressive strength.
3. What is the difference between a polyimide heater and a silicone rubber heater?
Polyimide heaters have a thinner substrate and are suitable for compact, lightweight applications. Silicone rubber heaters provide greater moisture resistance and mechanical compressive strength. Use the verified comparison table above to evaluate the required specifications.
4. Can JLCPCB manufacture a custom flexible heater?
Yes. JLCPCB flexible heaters can be customized by material, dimensions, voltage, power or resistance, temperature, adhesive backing, and lead-wire requirements.
5. What files can I upload for a custom flexible heater?
JLCPCB recommends Gerber files in ZIP or RAR format or CAD drawings in DXF or DWG format. The maximum upload size is 100 MB.
Flexible heaters provide customizable heating for compact, curved, and irregular surfaces. Select polyimide or silicone rubber according to the verified product specifications and application requirements, then confirm the final design with the JLCPCB Flexible Heater team.
Keep Learning
JLCPCB Flexible Heater Manufacturing Process: A Comprehensive Guide
In various industries, resistive heating elements play a critical role in converting electrical energy into heat. As demand grows for more compact and customizable thermal solutions, flexible heater manufacturing has become essential to producing efficient and reliable heating components. Flexible heaters, particularly polyimide (PI) flexible heaters, are known for their thin, lightweight, and adaptable design, which is crucial for effective thermal management across a wide range of applications—from ......
The History and Evolution of Polyimide (PI) Film
Polyimide film has become a critical material in aerospace, electronics, flexible circuits, and other demanding applications. Its history is a progression from making a heat-resistant polymer into a usable film to adapting that film for increasingly specialized engineering needs. This article traces the history and evolution of polyimide (PI) film through Kapton's early commercialization, space applications, the expansion of electronics, and newer developments in optical and high-frequency materials. ......
What Is a Flexible Heater? A Complete Guide
Flexible heaters provide customizable heating for applications where space, shape, or installation conditions make conventional rigid heaters difficult to use. But different materials offer different specifications, so selecting the right heater requires more than choosing a size and target temperature. This guide explains what flexible heaters are, how they work, the main types available from JLCPCB, and the differences between polyimide and silicone rubber heaters. It also covers common applications......
The Complete Guide to Silicone Rubber: Properties, Applications, and Benefits
When we think of rubber, we often imagine car tires or elastic bands. However, there is a "super-material" in the elastomer family that operates where ordinary rubbers fail: Silicone Rubber. From the seal in your smartphone to life-saving medical implants and the turbocharger hoses in high-performance cars, silicone rubber is the silent hero of modern engineering. Consider this: the same material that makes your flexible phone case also keeps astronauts safe in space, helps premature babies breathe in......
What Are the Difference between Polyimide Flexible Heater and FPC?
Introduction While polyimide (PI) flexible heaters and flexible printed circuit boards (FPCs) may appear similar in structure, their materials, tolerances, and purposes are fundamentally different. PI flexible heaters are designed for heat generation and thermal management, whereas FPCs focus on signal transmission and electrical interconnection. This article explains their differences in features, structures, and functions, helping engineers choose the optimal solution for their applications. Feature......
The Evolution of Flexible Heaters: From Early Prototypes to Modern Applications
The history of engineering is often narrated through grand monuments that dominate the horizon—soaring cross-sea bridges, colossal skyscrapers, and the rhythmic thunder of steam engines. Yet, there is a narrative just as profound and compelling to be found in the subtle, thin, and often invisible components that form the hidden foundations of modern life. Among these, the trajectory of the Flexible Heating Film stands as a testament not only to breakthroughs in materials science but to the persistent ......