How to Use Solder Flux When Soldering Through-Hole Components: Best Practices
5 min
- Step-by-Step: How to Use Solder Flux for Through-Hole Soldering
- Solder Flux Tips for Through-Hole Soldering
- Conclusion
Through-hole soldering is often done with flux-core solder, but relying on the core alone is rarely enough for consistent, high-quality joints. Oxidized leads, thick copper barrels, and large ground planes all demand better flux control to ensure proper wetting and full barrel fill.
This guide explains how to use solder flux for through-hole soldering in real-world conditions—from choosing liquid flux pens to handling difficult ground connections.
Before walking through the step-by-step process, we’ll first answer the most common practical questions technicians ask when soldering THT components.
Q1: Do I Need Extra Flux If Using Flux-Core Solder?
Technically, no - but practically, yes. While the flux inside the solder wire core is sufficient for clean, new components, it often isn't enough for oxidized vintage parts or thick power planes. Adding external flux ensures wetting starts before the solder melts, guaranteeing a better bond.
Q2: Liquid Pen or Gel Flux: Which is Best for Through-Hole?
Liquid Flux Pens are superior for THT. The low viscosity allows the flux to wick rapidly down the plated hole (capillary action), coating the entire barrel walls. Gel flux tends to sit on top and may not penetrate deep enough before activation.
Q3: How Does Flux Help with "Barrel Fill"?
IPC standards require vertical fill (solder visible on the top side of the board). Flux reduces surface tension inside the barrel, allowing the solder to climb up against gravity. Without extra flux, the solder may stop halfway up, leading to a weak mechanical connection.
Q4: Can Flux Help When Desoldering Through-Hole Parts?
Yes. Old solder joints are often heavily oxidized and do not transfer heat efficiently, making desoldering difficult. Applying fresh liquid flux to an old joint acts as a heat-transfer medium, helping the iron melt the solder faster and protecting the pad from lifting due to excessive thermal stress.
Q5: What If My Through-Hole Components Are Old and Oxidized?
If you are working with "New Old Stock" (NOS) or salvaged parts, standard flux-core solder may fail to wet the leads. In this case, use a more active flux like Rosin Activated (RA) or gently abrade the leads with a fiberglass eraser before soldering to expose fresh metal.
Q6: Does Flux Help with Ground Planes?
Absolutely. Soldering a leg connected to a large ground plane requires significant heat. Flux prevents the joint from oxidizing during the extended heating time required to bring the copper plane up to temperature, ensuring a solid connection rather than a cold, dry joint.
Step-by-Step: How to Use Solder Flux for Through-Hole Soldering
1. Targeted Application: Use a flux pen or fine brush to apply a localized amount of flux to the annular ring (the copper pad surrounding the hole) and the component lead. You do not need to flood the area; a simple coat ensures that as the lead heats up, the flux activates immediately to clean the barrel walls.
2. Create a Heat Bridge: Use a flux pen or fine brush to apply a localized amount of flux to the annular ring (the copper pad surrounding the hole) and the component lead. You do not need to flood the area; a simple coat ensures that as the lead heats up, the flux activates immediately to clean the barrel walls.
3. Feeding for Capillary Action: Feed the solder wire into the joint, ideally on the side opposite to the soldering iron tip. Do not melt the solder on the tip itself. By feeding into the joint, you force the molten alloy to follow the activated flux down into the plated barrel (vertical fill), creating a robust mechanical rivet.

Figure: Showing how flux helps solder wick down the barrel of a through-hole component.
Solder Flux Tips for Through-Hole Soldering
1. Avoid Socket Contamination: When soldering sockets (DIP, ZIF), be extremely careful with liquid flux. Capillary action can wick the flux inside the spring contacts, insulating them and ruining the socket. Apply flux sparingly to the solder side only.
2. Fixing "Icicles" (Solder Flags): If you pull the iron away and leave a spike of solder (an icicle), it indicates the flux has burned off. Add a drop of fresh flux to the icicle and touch it with a clean iron. The flux will break the surface tension, causing the solder to snap back into a smooth cone.
3. Managing Ground Planes: Flux is essential for ground pins. Because ground planes act as massive heatsinks, you must hold the iron on the joint longer. Without extra flux, this extended heating time would oxidize the pad before the solder melts. A generous coat of flux protects the copper during this "pre-heat" phase.
Conclusion
Using solder flux correctly is one of the most effective ways to improve through-hole soldering quality. While flux-core solder works for clean, simple joints, additional external flux becomes essential when dealing with oxidized components, thick barrels, or heat-sinking ground planes. Proper flux application improves wetting, enables full vertical barrel fill, and reduces the risk of cold joints and lifted pads.
By applying flux precisely, feeding solder into the joint rather than the tip, and refreshing flux during extended heating, you can achieve mechanically strong, IPC-compliant through-hole joints with far greater consistency and reliability.
Popular Articles
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
IC Package Types Explained: A Practical Guide for PCB Designers
Walk into any electronics lab, and you'll hear the same debate: "Which IC package should I use here?" It sounds like a simple question until you realise the answer determines your PCB footprint, thermal headroom, assembly process, rework feasibility, and field reliability - all at once. This guide breaks down every major IC package type used in modern PCB design, helping you understand the differences between common IC package types in plain engineering language so you can make the right call from the......
Everything You Need to Know About Solder Wire
The Latin word solidare means "to make solid," this is where the term solder gets its start. For joining two metal parts, this alloy is used because of its low melting point. Solder is a substance that is used to attach items, basically we can say wires and leads components together. Soldering is considered a skill in electronics for assembly of components onto a bare board PCB. The solder wire used has a significant impact on how well a soldering project turns out. It consists of alloys, mostly based......
SMT vs Through Hole: Which PCB Assembly is Most Cost-Effective?
Performance and cost in the realm of electronics production depend on choosing the correct assembly method. Of the several approaches accessible, Surface Mount Technology (SMT) and Through-Hole Technology (THT) are the two most often used ones for PCB assembly. These two assemblies can be combined to create some products or used as individual technologies. Though seemingly little, this variance affects several aspects including board design, materials and techniques employed, heat dissipation, and rel......
PCB Soldering Basic Techniques and Overview
Soldering means joining metal components with a melted metal called solder, which has a low melting point compared to other metals. Soldering is crucial in the electronics industry and is the primary method of joining electrical components. There are different types of soldering materials based on quality and their melting points. The most common combination is a tin or lead metal alloy mixed with silver or brass. The soldering iron melts the metal so it can be used like glue to connect two pieces. On......
Lead-Free Solder vs Lead Solder : What is the Difference?
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties ......
How to Repair a Burnt Circuit Board (and When to Replace It)
Key Takeaways Find out why the board burnt before you repair anything. The part that charred is often a victim of a fault somewhere else. Charred FR-4 conducts. A repair only lasts if every trace of carbon is cut out and the area measures as an insulator again. Heat that went through the board, blistering, or a burn among vias or under a BGA usually means replacing the board. Rebuild a burnt trace heavier than the original, and keep conductive epoxy off power paths. Power the repaired board from a cur......