Design Guidelines for RF PCB Layout and Manufacturing
4 min
- 7 Key RF PCB Layout Considerations
- Conclusion:
RF PCBs work on some fundamental rules that involve prior knowledge of digital and analog design circuits. Comparing directly to analog and digital is not directly possible because here the frequency range is in the GHz range. The frequency range makes the PCB so different and we have look for almost everything:
- Impedance mismatches
- Trace lengths
- Grounding
- Shielding
If not done so, may cause the full failure of the system. Or if designed not considering all the requirements it will lead to performance degradation, signal loss, EMI (electromagnetic interference), and increased power consumption. We will see what type materials can be used, how the traces are routed in microwave RF PCB and most importantly the rules for signal integrity and impedance. Careful layout is required to prevent signal degradation and crosstalk between sections. Before starting an RF layout, consider the following parameters:
7 Key RF PCB Layout Considerations
1. Material Selection
RF PCBs require a stable substrate now. What do you mean by stable? It only means a stable Dielectric constant (Dk) and lower loss tangent (Df). Common materials which are used in RF are Rogers RO4000, RO3000, Taconic RF laminates and PTFE. Lower dielectric constant means there will be small propagation delay. On the other hand lower loss tangents minimize the energy loss.
2. Controlled Impedance
For the trace we can use microstrip, stripline, or coplanar waveguide structures which will be discussed below. Other than that we have to maintain consistent trace width and height from the reference ground plane. By implying that, characteristic impedance (typically 50Ω or 75Ω) can be set. If the line does not match to the network there will be reflections and losses. For more we can use curved corners traces instead of sharp 90° bends. After designing the circuit and PCB, simulation is very important. There are many online tools like impedance calculators & simulation tools to determine the appropriate trace dimensions and working. See our detailed article on impedance control.
3. Trace Design and Routing
Due to high frequency we need minimum parasitic and for that, Keep RF traces as short and direct as possible. Avoid sharp corners and use 45° bends or curved traces to prevent impedance discontinuities. Avoid via transitions in RF paths, use back-drilled or blind vias. Avoid running RF and non-RF traces in parallel to prevent coupling. Place test points outside the traces to preserve impedance continuity. Keep digital and RF sections isolated; maintain at least 20 mm separation, otherwise we have 20H rules, H is the distance from L1 to L2 of PCB, it can be prepreg between them if 4 layer PCB is considered.
4. Using RF Transmission Lines
1. Microstrip: A signal trace routed on an outer layer with a solid ground plane directly underneath.
2. Stripline: Signal traces routed on inner layers with ground planes above and below for balanced performance.
3. Coplanar Waveguide (Grounded): A center conductor flanked by ground traces with via fences for excellent isolation.
5. Grounding and Return Paths
A solid ground strategy is essential to prevent noise and EMI. Use a continuous ground plane directly beneath RF traces. Avoid ground plane interruptions that break return paths. The usual procedure is to route the RF on the top layer and ground just below it. Although vias are not recommended but where signal spreading is more we can stitch the PCB with vias which help to reduce parasitic capacitance. Ensure digital grounds are separated from RF grounds to reduce noise coupling. They should join only at one point in the circuit with some special considerations.
6. Power Supply Decoupling
Clean power is crucial for RF circuitry. Use multiple capacitors with varying values to filter a wide frequency range. Placing decoupling capacitors close to the power pins of RF ICs always helps to reduce noise. Route power traces separately and isolate them with filters if necessary. You can see a PMIC utilizing all these outside the chip.
7. Shielding and Isolation
EMI can degrade RF performance if not managed properly. Use grounded shielding cans to isolate RF sections. Separate RF, digital, and analog sections on the PCB. Implement guard traces (grounded) around sensitive RF traces to reduce coupling. Minimize crosstalk by spacing traces appropriately.
Conclusion:
RF PCB design starts with careful substrate selection as we do in step 1. Then the layer stack planning and controlled impedance routing is done. RF circuits are more susceptible to layout induced losses because of crosstalking and parasitic effects of the material. Following the given guidelines helps you build RF boards. Which are capable of handling high frequencies with minimal loss and interference. As frequencies increase into GHz ranges we can not just skip the simulation and testing.
Keep Learning
Understanding Multilayer PCB Stackup
Key Takeaways Layer Arrangement: Optimize signal, ground, and power layer placement for better performance. Material Selection: Choose suitable core, prepreg, and copper materials. Signal Integrity: Control impedance and minimize crosstalk and EMI. Stackup Design: Use symmetrical structures to reduce warpage risks. Manufacturability: Consider layer count, via structures, and manufacturing limits early in design. Performance & Cost: Balance electrical requirements, reliability, and production costs. In......
Designing Antennas on PCB: A Beginner to Advance Guide
In today’s world of widespread wireless connectivity, the demand for small, affordable, and reliable antennas is higher than ever. Antennas act as real-world implementations of electromagnetic wave principles. They enable the sending and receiving of signals for a variety of wireless uses. While there is a lot of theoretical and experimental research in this area, only a few designs become widely used in actual products. Among the different options, Printed Circuit Board (PCB) antennas have become a p......
PCB Antenna Design: Types, Principles, and Best Practices
In the world surrounded with wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. Antennas are the application of electromagnetic waves. There are many theories and practicals available on antennas, but only few of them get recognised. For wireless data transfer the one solution can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating t......
Effective Escape Routing Strategies for High-Density BGA Success
Key Takeaways Escape routing is essential for successfully fanning out high-density BGAs, especially at 0.5 mm pitch and below. Use dogbone fanout for ≥0.5 mm; switch to via-in-pad (filled & capped) for finer pitches. HDI microvias and stacked vias significantly improve routing density and reduce layer count. Maintain symmetry and short stubs for differential pairs to preserve signal integrity. Combine smart stackup, DFM checks, and capable fabrication for reliable, high-yield results. Ever put a 484-......
ESP32 BLE Guide: Choosing the Right Chip and Designing Your PCB
Key Takeaways ESP32 BLE support: Most ESP32 chips support Bluetooth Low Energy (BLE), except the ESP32-S2, which supports only Wi-Fi, and the ESP32-P4, which has no built-in wireless radio. The original ESP32 also supports Bluetooth Classic, while newer models offer Bluetooth 5 features. Wi-Fi and BLE coexistence: Wi-Fi and BLE share the same 2.4 GHz radio and take turns using it. Heavy Wi-Fi activity can reduce BLE throughput or interrupt scanning, so both functions need to be tested together. Power ......
How SMA Connectors Work in RF PCB Design
Key Takeaways Focus on the Launch: Signal loss happens where coax turns into a flat trace, not inside the SMA body. Clear Ground Under Pads: Cut ground planes under launch pads to control capacitance and keep 50 ohms. Place Ground Vias Close: Put ground vias next to connector legs to shorten return paths. Account for Tolerances: Trace etching and board thickness directly alter launch impedance. Handle with Care: Use a torque wrench on joints and switch to high-frequency boards above 6 GHz. An SMA conn......