Tutorial on Partially Flipped Panelization
2 min
- Partially Flipped Panelization Method
In the layout engineering phase of PCB design, panelization is frequently employed. Panelization, in essence, involves assembling individual boards into a larger one, leaving room for V-Cuts, process edges, fiducials, tooling holes, and other process clearances.
During PCB prototyping, it is often more efficient to assemble small boards into a larger one in Altium before fabrication and assembly.
Partially Flipped Panelization Method
Today, let's delve into the partially flipped panelization method, specifically for PCB prototyping. Essentially, it involves transforming the TOP layer of the drawn PCB into the BOTTOM layer and vice versa for panelization.
Here are the overall steps:
1. Create a new PCB file and copy the completed PCB design into the newly created PCB file.
2. Perform a special paste.
3. Copy the entire PCB board, select it, flip it, and then rotate it 180 degrees clockwise.
To execute these steps:
1. Select the entire file (Shortcut: S+A).
2. After copying the file, perform a "special paste." Ensure you select the two middle options, as shown in the following image. After selecting these options, refrain from reapplying copper fill.
3. After copying the file, it should be positioned appropriately. At this point, select the move command and drag it. During the drag, a dialog box will appear. Please choose "YES." After dragging, the file can be moved with your mouse. Press the "M" key on the keyboard. When the dialog box appears, select "Flip Selection." As shown in the right image below, the file will be flipped, and you may need to adjust its orientation. Select the file again and use the "Move Command" while pressing the spacebar to rotate it 180 degrees and place it in the desired position.
When handing the design to the PCB manufacturer for PCB prototyping, it's essential to add the process edges. Select the "keep-out" layer for drawing. Add "tooling holes" and "fiducial points" on the process edges. Finally, use any layer, such as the "Overlay" layer or the "keep-out" layer, to label the V-cuts. With this, the entire panelization process is complete, as shown in the image below.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
How to Determine the Right PCB Voltage Clearance for Safe and Reliable Designs
Key Takeaways Clearance is the air gap; Creepage is the surface path — both essential for high-voltage safety. Base spacing on peak voltage and follow IPC-2221 / IEC 60664-1 standards. Major factors: voltage, pollution degree, CTI, altitude, and conductor location. Use isolation slots, guard rings, and conformal coating to optimize spacing. Always run clearance calculations, DFM checks, and Hipot testing before production. Why do two copper traces that work fine at 5V suddenly arc over and burn at 400......
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......