Lead-Free Solder vs Lead Solder : What is the Difference?
6 min
- What is Lead Solder?
- What is Lead-Free Solder?
- Key Differences Between Lead and Lead-Free Solder:
- Comparing Costs of Lead-Free vs Leaded Solder:
- Melting Point Equations:
- Global Regulatory Requirements:
- Conclusion:
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties of solder are used in the electronics industry:
- Lead-based solder
- Lead-free solder
The classic ingredients for solder are tin and lead. The electronics industry has relied on this combination for a long time. There has been a dramatic transition away from lead-based solders. Which were formerly the norm, due to increased health and environmental concerns. In this article we will learn why lead-free solder has surpassed lead ones. We'll go over the composition differences, melting points and regulatory standards.
What is Lead Solder?
Lead solder is an alloy of solder that contains lead with tin. Lead solder is usually named as 63/37 which is the ratio of tin and lead. Means it will contain 63% tin and 37% lead. But why do we use LEAD based solders? And why are they so popular? The answer is because of their low melting point of about 185°C. There were a number of reasons why this solder was formerly the standard:
Cooling and Curing: Lead solder cools down more slowly than other metal options. This reduces the possibility of the joint cracking also there will be no issues like dry soldering.
Wetting the joints: Wetting the joints means making the two wires which are going to solder more effective. Means giving them an extra adhesiveness. Using this type of solder is effective in wetting joints.
We can not rely on lead based products, its poisonous. Lead has negative impacts on ecosystems and human health. It comes under the health issues linked to lead exposure according to the CDC in the US.
What is Lead-Free Solder?
The amount of metals in lead-free solder compositions might vary. Metals such as tin, copper, silver, nickel, and zinc can be used as components. For better performance and environmental safety lead-free solder substitutes are also available.Lead with alternative metals include bismuth (Bi) or antimony (Sb). Among lead-free mixes, tin-copper is the most popular due to its melting point of 217°C. When compared to conventional lead-tin solders the lead-free solders have unique characteristics. Because of these quirks the manufacturers have to make adjustments to their product designs and processes.
Common Lead-Free Solder Compositions:
- SAC305: 96.5% Tin, 3% Silver, 0.5% Copper and has a melting point: 217-221°C
- SnCu0.7: 99.3% Tin, 0.7% Copper and has a melting point: 227°C
Tin and copper make up the lead-free combination that sees the most action. A greater melting point is associated with lead-free solder than lead-based alternatives. When compared to lead soldering this technique also produces tougher and stronger junctions.
Key Differences Between Lead and Lead-Free Solder:
Comparing Costs of Lead-Free vs Leaded Solder:
Lead is not very expensive, this is the second reason it is used. On the other hand if we use other alternatives or if we use more tin it will be an expensive option. Manufacturers can save up to 10 times if they are using lead. Other alternatives like silver makes the deal more expensive but due to the conductivity can be used in high end systems.
Using lead-free solder could add to the overall cost, not to mention the initial investment. Because more resources and processing to make the lead-free solder is usually more expensive than leaded solder. Equipment wear and tear and energy expenses might both rise due to greater melting points.
Melting Point Equations:
To put a number on this impact, we may utilize a linear equation that describes the connection between alloy composition, melting point, and temperature (Tm):
The equation: T=Tm −kC
Where:
The alloy has a melting point denoted by T.
C is the element's concentration in the alloy.
Tm is the temperature at which a pure metal, like lead or tin, melts.
k remains constant.
Global Regulatory Requirements:
Lead is toxic and can accumulate in the body as a result of chronic exposure. Contaminating land and groundwater, it is a hazardous waste product. The EU Restriction of Hazardous Substances regulation came into effect in 2006. Lead solder is now restricted in EU devices thanks to this rule.
European Union (EU):
European Union (EU) restricts the incorporation of lead and other toxic materials into electrical devices . In homogenous materials, the content cannot be more than 0.1% by weight according to the new limitations regulation.
United States:
While there is no federal RoHS rule, several states have imposed their own regulations. The proven dependability of lead solder leads to its exemption.
Conclusion:
The controversy over lead-free vs lead solder goes beyond a simple technicality. Progress towards a cleaner electronics sector, compliance and sustainability are the key issues. Due to the pervasiveness of electronics in our daily lives it is crucial to steer clear of items containing lead. Electronics assembly is one area where lead-free solder excels. But it isn't a good fit for aeronautical or medical applications. There may not be enough surface tension in lead-free soldered junctions to withstand impact.
This is not a big problem for PCB uses because the majority of electronics are not subject to harsh conditions. Use of lead-free solder has several advantages. At JLCPCB, lead-free solder to meet global environmental standards while ensuring reliable performance. It is crucial for manufacturers, engineers and enthusiasts to understand the important distinctions in composition. In order to educate them to make a decision.
Popular Articles
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Wire Bonding vs Flip Chip: Key Differences in Semiconductor Packaging
In the rapidly evolving world of semiconductor packaging, the choice between Wire Bonding and Flip Chip technology is more than just a mechanical decision—it is a strategic pivot that dictates your product’s performance, thermal limits, and bottom line. Are you looking for the cost-effective reliability of traditional interconnects, or does your application demand the high I/O density and superior signal integrity of modern flip-chip architectures? In this comprehensive guide, we draw on years of high......
Chip Scale Package (CSP) Explained: Types, Benefits & More
Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action. By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds t......
How to Solder Wires to a Circuit Board Properly: Step-by-Step Guide
Learning how to solder wires to a circuit board is a fundamental skill for electronics repair, prototyping, and PCB assembly. Whether you are attaching power leads, signal wires, or test connections, a weak solder joint can cause intermittent failures, lifted pads, or long-term reliability issues. In this step-by-step guide, you'll learn the correct tools, preparation methods, and soldering techniques needed to create strong, clean, and reliable wire-to-PCB connections. From preparing the wire and PCB......
BGA Reballing Explained: Complete Process, Tools, Risks, and Best Practices
In modern electronics design, the Ball Grid Array (BGA) is the standard for high-performance silicon, enabling thousands of I/O connections in a tiny footprint. However, this density creates a "black box" scenario: connections are hidden, and defects like cold joints or thermal fatigue cracks are invisible to the naked eye. Unlike a QFP that can be fixed with a soldering iron, a failed BGA threatens the viability of the entire board. BGA reballing is the critical solution to this problem. It is the pr......
SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
Surface Mount Devices (SMDs) are essential components in modern electronic devices, including smartphones, tablets, and IoT systems. Unlike older through-hole methods, where components were inserted through drilled PCB holes, soldering SMD components manually can be challenging, especially for beginners. The extremely small sizes and tight spacing on modern PCBs require high precision, and achieving reliable solder joints often depends on using the best SMD soldering tools. Common issues arising from ......
IC Package Types Explained: A Practical Guide for PCB Designers
Walk into any electronics lab, and you'll hear the same debate: "Which IC package should I use here?" It sounds like a simple question until you realise the answer determines your PCB footprint, thermal headroom, assembly process, rework feasibility, and field reliability - all at once. This guide breaks down every major IC package type used in modern PCB design, helping you understand the differences between common IC package types in plain engineering language so you can make the right call from the......