Design Guidelines for Industry-Standard Solder Stencil
5 min
- What Are Industry-Standard Solder Stencils?
- Considerations for Solder Stencil Designing:
- 7 Key Design Guidelines for Standard SMT Stencils:
- Conclusion:
Solder paste printing is one of the most important processes in PCB assembly, and the design of a stencil directly affects the quality of solder paste application. In a previous article, we discussed stencils and their types in detail. JLCPCB’s advanced stencil options, including step-up/step-down and nano-coated stencils, help engineers achieve higher printing accuracy and assembly reliability. In electronics hardware design, following proper design rules is just as crucial as having the right tools. This essay examines key design principles for producing useful and production-ready content today.
What Are Industry-Standard Solder Stencils?
Solder paste stencil is applied using industry-standard stencils, which are commonly laser-cut stainless steel foils with precise perforations that line up with PCB pads. These foils are typically 100µm to 120µm thick. Usually utilized for SMT assembly lines, these stencils are made to integrate easily with pick-and-place machines and automated stencil printers.
They are designed to meet common SMT requirements without the need for specialized features like thickness stepping, and they adhere to standards set by organizations such as the IPC, SMTA, and IEC. Click here to view the whole standard IPC guidelines for PCB stencils.
Considerations for Solder Stencil Designing:
The key design features of an effective solder paste stencil are as follows:-
- Stencil thickness
- Aperture design
- Stencil material and mounting
- Stencil alignment
- PCB design specific
7 Key Design Guidelines for Standard SMT Stencils:
1. Stencil Thickness Selection
The amount of solder paste put down depends on the thickness of the pattern. Give most of your attention to the board's smallest pitch component. In a thick stencil due to a phenomenon named surface tension, solder paste may stick to the inner walls of the aperture. According to a general guideline, the smallest aperture should preferably have at least five solder particles.At JLCPCB, stencil thickness can be customized to meet your board requirements, with standard options from 0.10 mm to 0.20 mm and special options from 0.03 mm to 0.5 mm, ensuring precise and consistent solder paste deposition even for fine-pitch components.
2. Aperture Design Guidelines
To prevent solder flaws like bridging and solder beads, this is crucial. For accurate deposition the apertures are made to be a bit smaller than the pads. However, for certain parts, an aperture with a specific design is required to deposit less paste on the inner edge of the part, which helps to prevent the formation of "mid-chip" solder balls. Here are a few instances:
3. Aperture Reduction (Pad-to-Aperture Ratio)
Apertures are frequently made slightly smaller than the actual pad dimensions in order to prevent bridging and extra solder.
- For most components, the typical reduction is between 5 and 7%.
- For dependable printability, IPC-7525 suggests a stencil-to-pad area ratio >0.66.
Formula: Area Ratio = (Aperture Area) / (Aperture Wall Height × Aperture Perimeter)
Keep this ratio above 0.66 to ensure clean paste release.
4. Fiducial Marks
When printing solder paste onto pads, it is very important that the pattern is lined up correctly with the PCB. This is accomplished by applying fiducial marks, which are registration marks, to the PCB and stencil. As you can see from our most recent comprehensive piece on fiducial marks, adding them to the stencil will guarantee proper alignment.
5. Stencil Frame and Border
Stencils can be frameless (for rapid prototyping or manual printing) or framed (glued into aluminum frames).
- Typical frame dimensions are 23 x 23 inches.
- Keep the distance between the aperture area and the frame edge at least 10 mm.
- Mark the stencil's position, thickness, and part number clearly.
6. Stencil Material
The stencil's capacity to remove solder paste from the apertures will depend on the kind of material it is made of. Although stainless steel is usually used, nickel, which is about 50% more expensive than stainless steel, can be used for PCB designs that include fine pitch components.
Chemical etching was used to create the initial generation of stencils, which worked well for larger apertures but became more difficult to remove solder from as component sizes shrank. This led to the development of laser-cut stencils, which created a much finer, trapezoidal-shaped opening that improved paste release. The possibility of electropolishing the aperture walls and, more subsequently, the technique of electro-forming the stencil were developed as component sizes decreased.
7. Window Effect design:
There are instances where the PCB design features big copper pads underneath the component. Devices that use power electronics typically experience this. In this case, a window effect is present to ensure a good electrical link and to let the device's heat escape. The device may lift and the outer leads may not solder if solder paste is placed over the entire pad. A "window effect" in the design can be used to decrease the solder volume, which is shared in the image above.
Conclusion:
For the majority of PCB assemblies, these fundamental design guidelines will yield good print results. At JLCPCB, it is critical that PCB manufacturers and assembly engineers understand the design recommendations provided for their stencils.I think it's critical that the PCB manufacturer comprehends the design guidelines provided by their stencil supplier. An essential step in the assembly process is printing. There will be "knock on" repercussions throughout the procedure if mistakes are made at this point. It is crucial to utilize a stencil that has been designed with all the necessary considerations in order to provide good, repeatable printing results. Before experimenting with more complex methods like step stencils, electroformed versions, or nano-coated foils, PCB designers and assembly engineers can establish a strong foundation by becoming proficient in these standard processes.
Keep Learning
DFN Package Guide: Footprint, Soldering & Stencil Tips
Key Takeaways What a DFN is: A DFN (Dual Flat No-Lead) package is a leadless chip-scale IC package with connection pads on two opposing sides of its underside, usually plus a central exposed thermal pad. Assembly requirements: DFN joints sit hidden under the body, so it needs reflow soldering with a stencil and X-ray or AOI inspection, not hand soldering. Design essentials: Follow IPC-7351 land patterns and IPC-7525 aperture rules, use a thinner stencil foil around 0.1-0.12 mm, and segment the thermal......
Paste Mask vs. Solder Mask: What Each Layer Does (and Why It Matters)
Key Takeaways Two layers, opposite jobs: The solder mask is the physical polymer coating that insulates copper and keeps pads solderable, while the paste mask is data-only manufacturing information that never appears on the finished board. Opposite pad adjustments: A mask opening is drawn slightly larger than the pad (mask expansion) while a paste aperture is drawn equal to or smaller than the pad (paste reduction), and these mirror-image rules cause most of the confusion. The paste mask is the stenci......
BGA Stencil Design: Apertures, Thickness & Tips
On a ball grid array, every solder joint hides underneath the package where you cannot see it, touch it, or easily rework it. That is exactly why BGA stencil design decides whether the board works: the paste you print is the paste you get, and a print that is slightly too heavy or too light turns into hidden bridges, voids, or starved balls that only an X-ray will reveal. Get the stencil right and the joints reflow clean the first time. Get it wrong and you are chasing intermittent faults after assemb......
Stencil Aperture Design: Geometry, Area Ratio & Tips
Key Takeaways Stencil aperture design controls paste volume, deposit shape, and print registration — it's the key controllable variable in SMT print quality. As per IPC-7525B, two math rules are non-negotiable: stencil area ratio ≥ 0.66 and stencil aspect ratio ≥ 1.5. Aperture geometry is component-dependent: 1:1 with pad for BGA, window-pane splits for QFN/BGA thermal pads, home-plate shapes for 0201/01005 chips, and modest reductions for fine-pitch QFP. Aperture reductions intentionally decrease the......
Red Glue Stencil: Types, Thickness & Ordering Guide
Key Takeaways A red glue stencil deposits adhesive dots under component bodies, not solder paste on electrical pads. Its main use is holding bottom-side SMD parts during wave soldering of through-hole leads. SMT red glue is commonly dyed red so operators can confirm each deposit during inspection. Printable adhesive families include epoxy, acrylic, and UV- or dual-cure materials. Glue stencils are commonly thicker than paste stencils because the dot must reach the component underside. A custom o......
A Beginners Guide to Step-Up and Step-Down Stencils
As everyone knows, companies are moving down to 2nm, and electronics are at their peak right now. The component sizes of a PCB likewise drastically shrink during a ten-year period. From 1206, BGAs have shrunk to 0402, 0201, and even smaller. Due to the small size of the components and the requirement for high throughput, defects such as tombstoning, bridging, or poor connections may occur during the soldering process. To address these challenges, specialized stencil technologies such as step-up and st......