Common problems and solutions in PCB design
4 min
- Unreasonable circuit layout
- Power supply noise interference
- Signal integrity issues
- Thermal management issues
- EMI/EMC Issues
- Component selection issues
- PCB size limitations
- Selecting a Package
- Manufacturing and assembly issues
- Conclusion :
PCB (Printed Circuit Board) design is a crucial aspect of electronic product development. During the design process, we often encounter challenging issues, which may include circuit design and wiring regulations. Understanding these common problems and their solutions can help engineers enhance the quality and efficiency of the design.
Unreasonable circuit layout
Circuit layout is crucial for maintaining signal integrity and electromagnetic compatibility. Unreasonable layout can lead to issues such as signal crosstalk and electromagnetic interference.
Solution:
1. Reasonably plan the hierarchy of the circuit board and separate high-speed signals from low-speed signals to minimize signal interference.
2. Divide the ground plane to prevent the formation of large-area ground plane loops and reduce electromagnetic interference.
3. Shorten the signal line as much as possible to minimize transmission delay and signal attenuation.
Power supply noise interference
Power supply noise may degrade circuit performance or even cause malfunction.
Solution:
1. Implement filter capacitors to eliminate power supply noise.
2. Add decoupling capacitors to the power supply to ensure stable power for each device.
3. Optimize the layout of the ground wire to ensure a solid ground wire reference plane and minimize noise resulting from the return flow of the ground wire.
Signal integrity issues
In high-speed signal transmission, maintaining signal integrity is a common challenge.
Solution:
1. Use the appropriate signal line width and spacing to ensure impedance matching and signal integrity.
2. Strengthen the ground reference plane of the signal layer to minimize the signal return path.
3. Implement terminal resistors and signal attenuators to minimize signal reflection and crosstalk.
Thermal management issues
High-power devices can lead to thermal issues, such as overheating and temperature unevenness.
Solution:
1. It is important to strategically design heat dissipation components, such as heat sinks and heat dissipation holes, to enhance heat dissipation efficiency.
2. Enhance heat dissipation by increasing the heat dissipation area to improve its ability.
3. Utilize a cooling pad to enhance the thermal contact between the device and the heat sink.
EMI/EMC Issues
Electromagnetic interference and electromagnetic compatibility issues can lead to degradation in system performance.
Solution:
1. Reasonably lay out the ground wire to minimize the return path and loop area.
2. Utilize a shielding cover to minimize electromagnetic radiation and electromagnetic interference from sensitive devices.
3. Apply a filter to eliminate high-frequency noise and interference.
Component selection issues
Using incorrect components may lead to unstable or unreliable circuit performance.
Solution:
1. Select the appropriate components and evaluate them based on design requirements and performance indicators.
2. Consider the temperature characteristics of the components to ensure that they operate normally within the specified temperature range.
3. Consider the reliability of components and select reliable brands and models.
PCB size limitations
Limitations on PCB size can result in layout challenges or signal integrity issues.
Solution:
1. Plan the layout reasonably, taking into account size restrictions when planning the device layout and signal line direction.
2. Use multi-layer boards to incorporate additional wiring layers and ground planes in order to enhance signal integrity and electromagnetic compatibility.
3. Optimize the signal line direction, minimize the length of the signal line, and reduce delay and interference as much as possible.
Selecting a Package
In PCB design, choosing the appropriate package is crucial as it directly impacts the layout, connection method, and reliability of components.
Solution:
1. Understand the functions and usage environment of the components, and choose the appropriate packaging type based on the design requirements, such as SMD, THT, BGA, etc.
2. Refer to the component data sheet or the supplier's recommended packaging to ensure that the selection meets the electrical and mechanical specifications.
3. Customized Packaging: If there is no standard package that meets the requirements, you can consider creating a custom package. This requires accurate dimensions and pin layout, as well as appropriate materials and processing techniques.
4. Utilize 3D modeling tools to validate the packaging, identify potential collisions between the package and other components, and guarantee the precision and assembly of the package.
Manufacturing and assembly issues
Issues that may arise during the manufacturing and assembly process include inadequate welding, component misalignment, and so on.
Solution:
1. Select the appropriate manufacturer to guarantee manufacturing quality and process reliability.
2. Conduct thorough prototype testing to verify the manufacturability and ease of assembly of the design.
3. Optimize the reflow process by using the appropriate reflow temperature and flux to enhance welding quality.
Conclusion :
During the PCB design process, it is inevitable to encounter various challenges. By employing hierarchical planning, rational layout, appropriate power and signal processing techniques, and effective thermal management, engineers can effectively address these issues and enhance the quality and performance of PCB designs.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......