This website requires JavaScript.
Coupons
Ship to
Blog

The True Cost of Custom PCBs: Understanding the Factors that Affect the Bottom Line

Published Jul 28, 2023, updated Sep 09, 2026

13 min

Table of Contents
  • What Factors Affect the Cost of Your Printed Circuit Board?
  • The cost of different types of PCB materials:
  • Component Selection and Sourcing:
  • Design Specifications and Requirements:
  • Hidden Costs of Custom PCBs:
  • How can we reduce the cost of custom PCBs?
  • Key DFM Optimization Rules for JLCPCB Cost Reduction:
  • FAQ about Custom PCB Costs
  • Conclusion:
pcb prototype assembly banner 2

Key Takeaways

  • Optimize Layout & Size: Simplify circuit design and keep board size within 100mm x 100mm for basic promo rates.
  • Stick to Standard Specs: Use 1.6mm board thickness and 1 oz copper weight to avoid material surcharges.
  • Respect DFM Limits: Maintain trace width/spacing ≥ 5/5 mil and via drills ≥ 0.3mm to prevent fine-feature fees.
  • Select Low-Cost Finishes: Choose HASL over ENIG for prototypes unless fine-pitch BGAs are required.

Printed circuit boards (PCBs) are integral to modern technology, used in everything from smartphones to aircraft systems. PCBs provide the mechanical support and electrical connections necessary for electronic components to function properly. However, the design and production of PCBs can be a complex and costly process, requiring careful consideration of several factors.

When designing a PCB, it is important to understand the factors that can affect the cost and bottom line. The complexity of the circuit, number of layers required, size and shape of the PCB, materials used, component selection and sourcing, and design specifications and requirements all play a role in determining the final cost of a custom PCB.

In addition to these factors, there are also hidden costs associated with the design and production of PCBs. These costs can include prototyping and testing, tooling and manufacturing, assembly and testing, quality control and certification, and shipping and logistics.

To minimize the cost of custom PCBs, it is important to consider all factors when designing and producing them. By simplifying the circuit design, reducing the number of layers, using standard components, optimizing the size and shape of the PCB, and applying design for manufacturability (DFM) principles, it is possible to reduce costs without sacrificing quality or reliability.

In this article, we will explore the various factors that affect the cost of PCB manufacturing and the hidden costs associated with their design and production.

What Factors Affect the Cost of Your Printed Circuit Board?

When designing a PCB, it is important to consider the various factors that can affect the cost. These factors can include:

1. The Complexity of the Circuit:

The complexity of the circuit is one of the main factors that can affect the cost of a PCB. A more complex circuit will require more components, which can lead to increased costs for sourcing and assembly. Additionally, a more complex circuit may require a larger PCB with more layers, which can further increase the cost.

2. Number of Layers Required:

The number of layers required for a PCB is another important factor that can affect the cost. A PCB with more layers will generally be more expensive to produce than one with fewer layers. This is because additional layers require more materials and additional processing steps during manufacturing.

3. PCB Size and Shape:

The size and shape of the PCB can also affect the cost. A larger PCB will require more materials and will take longer to manufacture, which can increase the cost. Similarly, a PCB with an unusual shape may require special tooling or processing steps, which can also increase the cost.

4. Materials Used:

The materials used to manufacture a PCB can also affect the cost. High-quality materials may be more expensive, but they can also provide better performance and reliability. Additionally, specialized materials, such as those required for high-temperature or high-frequency applications, may also increase the cost.

The cost of different types of PCB materials:

FR-4:

FR-4 is the most common material used in PCB production, made from woven glass-reinforced epoxy laminate. It is popular due to its high mechanical strength, excellent electrical properties, and cost-effectiveness. On JLCPCB, standard FR-4 (TG130–TG150) offers the most budget-friendly option (e.g., prototyping starting at $2 for 1–2 layer boards up to 100x100mm). High-TG FR-4 (TG170) is also supported for high-thermal durability at a slight engineering premium.

Rogers:

Rogers is a high-performance substrate commonly used in high-frequency applications (such as RF antennas, 5G, and radar systems). Made from ceramic-filled PTFE, it provides low dielectric loss (Dk = 3.48 @10GHz) and excellent signal integrity. Due to specialized raw material sourcing and tight impedance tolerances, Rogers substrates on JLCPCB carry a higher cost than standard FR-4.

Aluminum:

Aluminum PCB (Metal Core PCB / MCPCB) features a metal base with a dielectric layer and copper foil. It is widely used in high-power LEDs and power supplies due to its superior thermal conductivity (1.0–2.0 W/m·K on standard Aluminum). Its material and processing costs are slightly higher than standard FR-4.

Polyimide:

Polyimide is a flexible PCB (FPC) material used where boards need to bend or fit compact spaces (e.g., wearables, foldable devices). Formed from thin polyimide film (25µm/50µm), FPC materials require specialized laser profiling, making them higher in cost compared to rigid FR-4.

Ceramic:

Ceramic substrates offer extreme high-temperature and high-power performance, but are highly specialized and not part of standard online quick-turn prototyping. For high-thermal or high-frequency designs on JLCPCB, High-TG FR-4, Aluminum/Copper Core, or Rogers RO4350B serve as the standard cost-effective alternatives.

JLCPCB PCB Material Capabilities and Cost Comparison:

Material TypeKey Technical Parameters / TG / Dk​Typical ApplicationsJLCPCB Relative Cost Level
Standard FR-4TG130–TG150Consumer electronics, IoT, general circuitsStandard Low (Prototypes from $2)
High-TG FR-4TG170Industrial control, automotive, high-temp environmentsModerate (+Small engineering fee)
Aluminum Substrate1.0–2.0 W/m·K Thermal ConductivityLED lighting, power converters, automotive driversLow to Moderate
Polyimide (Flex/FPC)Ultra-thin (0.12–0.2mm), High FlexibilityWearables, compact interconnects, medical devicesModerate
Rogers (RO4350B)Dk = 3.48, Low Loss (Df < 0.0037)5G RF antennas, satellite comms, high-speed radarHigh

Component Selection and Sourcing:

The selection and sourcing of components can also have a significant impact on the cost of a custom PCB. Higher-end components will generally be more expensive, but they may offer better performance and reliability. Additionally, sourcing components from multiple suppliers can increase the cost due to shipping and handling fees.

Design Specifications and Requirements:

The design specifications and requirements for a PCB can also affect the cost. For example, if a PCB requires specific tolerances or testing procedures, this can increase the cost of production. Similarly, if a custom PCB requires specialized testing or certification, this can also increase the cost.

Therefore, by carefully considering these factors and making informed decisions during the design and production process, it is possible to reduce costs without sacrificing quality or reliability.

Hidden Costs of Custom PCBs:

While the factors discussed in the previous section can have a significant impact on the cost of custom PCBs, there are also several hidden costs that are often overlooked.

1. Prototyping and Testing Costs:

Before a PCB can be manufactured, it must be prototyped and tested to ensure that it meets the design specifications and requirements. This process can be time-consuming and expensive, as it may require multiple iterations to achieve the desired results. The cost of prototyping and testing can vary greatly depending on the complexity of the design and the number of iterations required.

2. Tooling and Manufacturing Costs:

Once the PCB design has been finalized and prototyped, it must be manufactured. This process requires specialized tooling and equipment, which can be expensive to set up and maintain. Additionally, the cost of manufacturing custom PCBs can be higher than that of standard PCBs due to the complexity of the design and the need for specialized processes.

3. Assembly and Testing Costs:

After the PCB has been manufactured, it must be assembled and tested to ensure that it functions properly. This process can be time-consuming and expensive, especially if the PCB requires specialized assembly techniques or testing procedures.

4. Quality Control and Certification Costs:

To ensure that the PCB meets the required quality standards, it may need to undergo additional testing and certification processes. This can include environmental testing, electrical testing, and safety certifications. The cost of these processes can add up quickly, especially if the PCB requires multiple certifications.

5. Shipping and Logistics Costs:

There are also shipping and logistics costs associated with PCBs. These costs can include shipping the PCB materials to the manufacturing facility, shipping the finished PCBs to the customer, and any additional handling or storage fees.

How can we reduce the cost of custom PCBs?

Designing and manufacturing custom PCBs can be a complex and costly process. However, there are several strategies that can be employed to help reduce the cost of custom PCBs while maintaining quality and reliability.

1. Simplify the Circuit Design:

One of the most effective ways to reduce the cost of a custom PCB is to simplify the circuit design. A simpler circuit design will require fewer components, which can reduce the cost of sourcing and assembly. Additionally, a simpler design may require fewer layers, which can reduce the materials and processing costs.

2. Reduce the Number of Layers:

As discussed earlier, the number of layers required for a custom PCB can have a significant impact on the cost. By reducing the number of layers required, it is possible to reduce the amount of materials and processing required, which can help to lower the overall cost.

3. Use Standard Components:

Using standard components can also help to reduce the cost of a custom PCB. Standard components are readily available and can be sourced at a lower cost than specialized components. Additionally, using standard components can help to simplify the design and reduce the number of layers required.

4. Optimize the Size and Shape of the PCB:

Optimizing the size and shape of the PCB can also help to reduce costs. A smaller PCB will require less material and processing, which can help to lower the overall cost. Additionally, a PCB with a simpler shape may require fewer processing steps, which can further reduce costs.

5. Apply Design for Manufacturability (DFM) Principles:

Design for manufacturability (DFM) is a set of principles that are used to optimize a product design for efficient and cost-effective manufacturing. By applying DFM principles to the PCB design, it is possible to reduce the cost of manufacturing and improve the quality and reliability of the final product.

Key DFM Optimization Rules for JLCPCB Cost Reduction:

To maximize cost efficiency when ordering from JLCPCB, engineers should design specifically within JLCPCB’s standard manufacturing capabilities:

1.Trace Width and Clearance: Keeping trace width/spacing ≥5/5mil for 2-layer boards (or ≥ 3.5/3.5mil for 6+ layer boards) avoids special fine-trace surcharge fees.

2.Via Drill Sizes: Standardize minimum via drill sizes to 0.3mm (outer diameter 0.6mm) for 2-layer boards and 0.2mm for multilayer boards. Micro-vias or non-standard drill diameters increase mechanical wear and machining cost.

3.Board Dimensions & Panelization: Keep individual board sizes within 100 mm × 100 mm to qualify for standard promotional prototyping pricing. For PCBA orders, panel dimensions should ideally be maintained within 250 mm × 250mm to prevent PCB warping and SMT placement alignment issues.

4.Standard Thickness & Copper Weight: Stick to 1.6mm board thickness with 1 oz (35μm) outer copper weight. Thicker copper (2oz) or non-standard board thickness (<0.8mm or >2.0mm) requires extra plating cycles and raw material surcharges.

Manufacturing ParameterJLCPCB Standard (Lowest Cost)Advanced Capability (Higher Cost / Precision)Cost Reduction Tip
Min Trace / Space5 mil / 5 mil (1-2L), 4 mil (4L)3.5 mil / 3.5 mil (6L+)Avoid using ultra-fine traces unless routing density demands it.
Min Via Drill / Pad0.3mm / 0.6mm (2L), 0.2mm / 0.45mm (4L+)0.15mm laser drillStandardize drill sizes to reduce tool-change cycles.
Board Thickness1.6mm0.4mm, 0.6mm, 2.0mm, 2.4mmStandard 1.6mm balance strength and cost.
Outer Copper Weight1 oz (35 µm)2 oz (70 µm)Use 1 oz unless carrying heavy current.
Surface FinishHASL (Leaded) / Lead-free HASLENIG (Electroless Nickel Immersion Gold)Choose HASL for low-cost prototypes; use ENIG for fine-pitch BGA/QFN.
PCBA Minimum Package0402 component size0201 component size0402 and standard pitch ICs allow Economic PCBA assembly.
Ready to Bring Your PCB Ideas to Life?

Turn designs into working hardware with expert fabrication, assembly, and component services from a trusted industry leader. Upload your files, choose your options, and get boards that are ready to test, ready to ship, and ready to scale.

Get Quote Now >

FAQ about Custom PCB Costs

Q: What is the most cost-effective PCB thickness and copper weight for JLCPCB orders?

The standard 1.6mm board thickness paired with 1 oz (35μm) outer copper weight offers the lowest cost. Choosing other thicknesses or 2 oz copper will incur extra raw material and processing surcharges.

Q: How can I avoid extra trace width surcharges during layout?

Keep your trace width and spacing at or above 5/5 mil for 1 or 2-layer boards, and at least 4/4 mil for 4-layer boards. Designing finer traces triggers precision manufacturing fees.

Q: What minimum via size should I use to keep costs low?

Use a minimum via drill size of 0.3mm with a 0.6mm outer diameter pad for 2-layer boards. For 4-layer or higher boards, 0.2mm drill size is supported without premium micro-via fees.

Q: How does board size affect JLCPCB promotional pricing?

Keeping individual PCB dimensions within 100mm x 100mm qualifies your order for standard low-cost prototyping rates. Exceeding 100mm increases both raw material and processing costs.

Q: Which surface finish should I select for prototype PCBs?

HASL (Leaded) or Lead-free HASL is the most economical choice for general prototypes. You only need ENIG (Immersion Gold) if your board uses fine-pitch BGA or QFN packages.

Conclusion:

Reducing custom PCB costs is not about compromising on product quality—it is about making smart engineering choices early in the design phase. By streamlining your circuit layout, standardizing components, and aligning directly with JLCPCB standard DFM rules for trace spacing, via sizes, and board dimensions, you can eliminate unnecessary process surcharges and drastically cut production costs.

Ready to turn your design into hardware? Upload your Gerber files to the JLCPCB instant quote engine today to test your layout against their DFM capabilities and unlock industry-leading prototyping rates!

Keep Learning