Gerber Files: The Essential Tool for PCB Manufacturing - JLCPCB
4 min
- Generating Gerber Files Properly
- Importance of a Gerber Viewer
- Conclusion
When it comes to PCB manufacturing, Gerber files are an essential tool for ensuring that your PCB design is accurately translated into a physical product. Gerber files are a set of instructions that communicate the design specifications to the manufacturer.
As a leading PCB manufacturer in the industry, JLCPCB utilized a Gerber real-time analysis system for providing instant online quotes and a Free Gerber Viewer for free inspecting if Gerber files are 100% accurate for manufacturing file standards.
Save your time for back-and-forth manual checking. Experience JLCPCB Gerber analysis system.
A correct Gerber file is the first step to starting your excellent electronic project. In this article, we will discuss the importance of generating GERBER files properly and the role of a GERBER viewer in PCB manufacturing.
Generating Gerber Files Properly
To generate Gerber files in a proper way, you need to use software that can create the needed file format. This can be done using a variety of software, including CAD programs like KiCAD, Altium, Diptrace, EasyEDA or dedicated PCB design software. When creating Gerber files, it's important to ensure that they contain all of the design-related necessary information, such as the layers, drill holes, and board outline.
It's also important to double-check the files to ensure that they are error-free. Any mistakes or errors in the Gerber files can result in significant issues during the manufacturing process, leading to delays and additional costs. As such, it's essential to have an accurate and detailed Gerber file before submitting it for manufacturing. At JLCPCB, the CAM engineers will prepare the Data For Manufacturing based on the submitted Gerber files, but they will not touch or fix any design mistakes, instead, the engineers will inform the customer in some cases when the design does not match the manufacturing capabilities.
Importance of a Gerber Viewer
A Gerber viewer is a software tool that allows you to view the Gerber files before submitting them for manufacturing. This is an essential step in the PCB manufacturing process as it ensures that the files are error-free and contain all the necessary information.
As a PCB manufacturer, JLCPCB provides an online Gerber viewer as a reference for customers to check the uploaded Gerber files before proceeding to order the related PCB, but it remains a reference tool and the final produced PCB will be identical to the designed board and this is why we JLCPCB recommend using external powerful Gerber viewers for file checking.
The Gerber viewer allows you to zoom in on specific areas of the design, ensuring that there are no errors in the placement of components or drill holes.
It also provides a visual representation of the layers, helping you to identify any issues with the layer stackup.
Additionally, a Gerber viewer can also be used to check the manufacturer's output files, ensuring that the final product matches the original design specifications. By using a Gerber viewer, you can ensure that your PCB design is accurate and ready for manufacturing, saving you time and money in the long run.
Conclusion
Gerber files are an essential tool for PCB manufacturing, providing a set of instructions for the manufacturer to follow. To ensure that your Gerber files are generated correctly, it's important to use the right software and double-check the files for errors. A Gerber viewer is an essential tool for checking the files before submitting them for manufacturing, ensuring that your design is accurate and ready for production. By following these steps, you can ensure that your PCB design is manufactured correctly, accurately, and efficiently.
Here get quality PCBs for your awesome electronics projects. Up to $54 coupons for new users! Upload Gerber files and experience JLCPCB Gerber analysis system.
Keep Learning
Achieving Clean PCB Separation: The Benefits of Professional Depaneling
Note Clean depaneling is a critical final step: a poor split can cause microcracks, trace/solder-joint damage, delamination, and rough edges. Choose the method early based on outline, material/thickness, component edge clearance, volume, and required edge quality—V-scoring for fast straight cuts, routing for complex shapes, and laser for fragile or edge-constrained designs—with IPC criteria guiding controls and inspection. Have you ever broken a PCB off a panel and found rough edges, small cracks alon......
Via Filling Explained: Key Techniques, Benefits, and Solutions for High-Performance PCBs
Note Via filling completely fills plated through-holes and microvias with epoxy or conductive copper paste, followed by planarization and copper capping (POFV). It eliminates voids, solder wicking, and thermal/mechanical issues while enabling reliable via-in-pad designs. Benefits include superior heat dissipation (up to 8 W/m·K), better signal integrity, higher mechanical strength, and improved assembly yields. JLCPCB provides free non-conductive filling + POFV on 6+ layer boards. Ideal for HDI, high-......
How to Choose the Right Prepreg Material for Reliable Multilayer PCB
Have you ever wondered what makes all those copper layers stick to a cross-section of a multilayer PCB? Prepreg material is the answer, and it is of much more importance than most engineers think it is. Choose the prepreg selection wrong, and you are predetermined to delamination, impedance drift, and long-term reliability problems. Prepreg is not only glue. It is a designed composite that determines your dielectric separation, dictates your impedance, affects signal loss, and determines your board be......
PCB Basic 3: Understanding PCB Manufacturing Processes
Welcome to the third installment of our PCB Basics series. In this article, we will unravel the step-by-step process of PCB manufacturing, guiding you through each stage with clarity and precision. Join us as we embark on this educational journey and discover how JLCPCB's advanced manufacturing capabilities and technology together with unparalleled commitment to quality assurance can elevate your PCB designs to the next level. Substrate Selection: Laying the Foundation One of the critical steps in PCB......
Laser Engraving vs. Professional PCB Fabrication : Understanding DIY Limitations and Industrial Advantages
In the conventional approach, we first apply a mask pattern and then remove metals using chemicals. In hobby electronics, using a laser engraver to make circuit boards is an exciting idea. The basic concept is to generate a laser to pattern a copper-clad board. Typically, a bare PCB is first coated with a dark resist layer that protects the copper. Then a laser cutter follows your circuit design to burn away the resist where copper traces should remain. After laser etching, the exposed copper is chemi......
Understanding SMT PCB Boards Technology: An Essential Component of Modern Electronics
Surface Mount Technology (SMT) has changed manufacturing of modern electronics. It has made designs and assembly methods more efficient. Many modern electronics depend on SMT PCB boards, which make it possible for circuit designs to be small and efficient. This is what today's technology needs. This article discuss about many types of SMT PCB boards, their uses, and the best methods for designing and assembling them. 1. What is an SMT PCB Board? Printed circuit boards called SMT PCB boards, use surfac......