Simplified yet Intricate: Single-Sided PCB Design
3 min
- Structure of Single-Sided PCB
- Soldering of Single-Sided PCBs
- Designing Engineering Files
- Characteristics of Factory Production
- Special Note
- Conclusion
Printed Circuit Boards (PCBs) are crucial electronic components. They act as the support structure for electronic devices and serve as the carrier for electrical connections among electronic components. Since its inception in 1925, the evolution of printed circuit boards has led to increasingly intricate layouts, more layers, and greater complexity. However, even amidst these advancements, the most basic form known as the single-sided PCB is still widely employed in various industrial products like radios, washing machines, and remote controls.
Structure of Single-Sided PCB
Traditional FR4 single-sided PCBs accommodate one side of copper, one side of solder mask, and two sides of silkscreen (depending on customer design). Due to the absence of the electroplating step in the production of single-sided boards, the hole walls of these PCBs lack copper (note: board thicknesses of 0.4 mm, 0.6 mm, 0.8 mm, and 2.0 mm are produced by default as double-sided to maximize utilization of board material. For boards of these thicknesses, through-holes will be plated).
Soldering of Single-Sided PCBs
Given the structure of single-sided PCBs, where only one side contains circuitry, soldering is limited to the exposed pads on that particular side. Depending on the component's structure, this results in two distinct soldering methods:
1. Same-Side Soldering
For components where the main body is on the same side as the circuit, often used for SMT-type component soldering.
2. Opposite-Side Soldering
For components where the main body is on a different side from the circuit, commonly used for through-hole component soldering.
Designing Engineering Files
In practical design, a complete PCB is designed layer by layer.
Taking double-sided boards as an example, patterns designed on the top layer are seen directly (e.g., top layer text appears correctly). Conversely, patterns designed on the bottom layer have a mirroring effect; if text is designed on the bottom layer and it appears upright in the design software, due to the mirroring effect, the text on the actual board will appear reversed (since the physical board is viewed from the opposite side).
The same principle applies to the circuit layer. For single-sided boards, when designing circuitry on the bottom layer, because of the mirroring effect, the actual board needs to be viewed from the front with a backlight to match the bottom layer's circuit design (as shown in the figure below).
Characteristics of Factory Production
In actual production, to avoid burrs and peaks, the mirrored image of the bottom layer's wiring is used for the top layer (mirrored production does not affect the customer's original design structure). This approach ensures that the drill bit first penetrates the copper layer on top. Since the substrate provides support underneath, the copper can be drilled very cleanly. Drilling holes with the copper side facing down would result in numerous burrs and peaks.
Special Note
1. Single-sided aluminum-based boards have a conductive aluminum base layer, making them unsuitable for component soldering (soldering could lead to short circuits).
2. Single-sided aluminum-based boards generally have silkscreen printed on one side, applied to the copper-covered side. Printing Silkscreen on the aluminum-based side is not recommended as it may be difficult to read.
Conclusion
In summary, single-sided PCBs have a straightforward design, but careful attention must be paid to the layer where the circuit is located and where soldering occurs to avoid an unintentionally mirrored design.
Popular Articles
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Capacitor Voltage Rating Explained with Examples
Capacitors are small components widely used not only for power delivery but also for signal conditioning in electronic circuits. In this article, we focus on the capacitor voltage rating across different types of capacitors. At first glance, capacitors look simple—small cans, discs, or chips on a PCB. However, their markings carry essential design information, including capacitance and voltage rating. These are not arbitrary values but directly affect circuit reliability. Ignoring the voltage rating w......
From Prototype to Product with a Better Development Board
Note Prototype Fast: Development boards integrate power, clock, and programming circuits to validate firmware in hours. Pick the Right Platform: Use ESP32 for Wi-Fi/BLE, Arduino UNO for 5 V sensors, Raspberry Pi Pico for tight I/O timing, and Raspberry Pi 5 for Linux. Scale to Custom PCB: Reuse your prototype's certified module, firmware, and support circuits, but remove unused headers to cut unit cost. Build for Production: Use a 4-layer ground-plane stackup for wireless boards, verify BOM stock earl......
4 Layer vs 6 Layer vs 8 Layer PCB: How to Choose the Right Stackup
Random selection of layers in electronics may lead to serious signal integrity issues. That's why we always design our stackup before designing the PCB. Stackup decides the type of PCB and how it gonna perform under high-frequency conditions. There are a lot of things that directly affect the stackup of the PCB, related to impedance matching, routing density, signal and power integrity, electromagnetic compatibility (EMC), and cost. Knowing the requirements before design and the most critical componen......
Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
Key Takeaways Choosing the best PCB solder mask color involves balancing aesthetics, visibility, and functionality. Green remains the top choice for superior contrast and inspection, while black offers premium appeal, white excels in LED applications, and other colors like purple and red provide unique design options. The ideal color depends on your priorities in inspection ease, thermal performance, and brand image, with minimal impact on electrical performance when using proper silkscreen contrast. ......
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......