This website requires JavaScript.
Coupons
Ship to
Blog

Navigating the Impedance Landscape: Selecting the Right Impedance for USB, Ethernet, HDMI, and SD Card Interfaces

Published Sep 09, 2026, updated Nov 21, 2026

3 min

Table of Contents
  • Introduction
  • Understanding Impedance in Digital Interfaces
  • USB (Universal Serial Bus)
  • Ethernet
  • HDMI (High-Definition Multimedia Interface)
  • SD Card
  • Factors Influencing Impedance Selection
  • Best Practices for Impedance Matching
  • Conclusion
hdi pcb coupons

Introduction

In the realm of high-speed digital communication, choosing the right impedance is a critical aspect of successful PCB design. Impedance matching ensures optimal signal integrity, minimizes reflections, and enhances the overall performance of interfaces such as USB, Ethernet, HDMI, and SD Card. In this blog post, we'll explore the importance of impedance, the factors influencing impedance selection, and best practices for ensuring reliable data transmission in these widely used interfaces.

Impedance

Understanding Impedance in Digital Interfaces

Impedance, measured in ohms, is a key parameter that characterizes the opposition a circuit presents to the flow of alternating current (AC). In the context of high-speed digital interfaces, maintaining the correct impedance is crucial for preventing signal reflections, minimizing crosstalk, and ensuring the integrity of transmitted data.

USB (Universal Serial Bus)

A- USB 2.0:

Standard Impedance: 90 ohms

Best Practice: Use a controlled impedance trace for USB 2.0 data lines to prevent signal distortion and ensure reliable communication.

B- USB 3.x:

Differential Impedance: 90 ohms

Single-Ended Impedance: 45 ohms

Best Practice: Maintain a consistent impedance profile across the entire USB 3.x signal path, including connectors and cables, to support high-speed data rates.

USB 3.x

Ethernet

10/100/1000BASE-T (Ethernet):

Differential Impedance: 100 ohms

Best Practice: Ensure consistent impedance along the entire length of the transmission line to avoid signal degradation and maintain signal integrity.

10/100/1000BASE-T (Ethernet)

HDMI (High-Definition Multimedia Interface)

HDMI 1.4/2.0:

Differential Impedance: 100 ohms

Best Practice: Use controlled impedance traces and maintain signal integrity for high-speed HDMI data transmission. Consider signal repeaters for longer cable runs.

HDMI (High-Definition Multimedia Interface)

SD Card

SD (Secure Digital) Card:

Differential Impedance: 50 ohms

Single-Ended Impedance: 25 ohms

Best Practice: Design PCB traces with the specified impedance values to prevent signalreflections and ensure reliable communication with SD card interfaces.

Factors Influencing Impedance Selection

A- Data Rate:

Higher data rates demand more precise impedance control to prevent signal degradation and ensure reliable communication.

B- Cable Length:

Longer cable lengths may introduce signal losses. Impedance matching becomes crucial to maintain signal integrity across extended transmission paths.

Connector Specifications:

C- Connectors:

including USB, Ethernet, HDMI, and SD card slots, come with specified impedance requirements. Adhering to these specifications is essential for seamless data transmission.

D- PCB Material:

The dielectric properties of the PCB material influence the characteristic impedance. Different materials have different impedance values, so it's important to choose a material that aligns with the target impedance.

Best Practices for Impedance Matching

A- Consistency Across Design:

Maintain consistent impedance values throughout the entire signal path, including traces, connectors, and cables.

B- Use of Controlled Impedance Traces:

Utilize controlled impedance traces for high-speed signals to minimize reflections and signal distortions.

C- Simulation and Testing:

Conduct impedance simulations and measurements during the design phase to validate the chosen values and identify potential issues.

D- Consult Specifications:

Refer to the datasheets and specifications provided by the interface standards for precise impedance requirements.

jlcpcb pcb assembly service banner 1

Conclusion

Selecting the right impedance for USB, Ethernet, HDMI, and SD Card interfaces is a critical aspect of PCB design, influencing the reliability and performance of high-speed digital communication. By understanding the specific impedance requirements of each interface, considering factors such as data rate and cable length, and adhering to best practices, engineers can ensure that their designs meet the stringent demands of modern electronic systems. As technology continues to evolve, maintaining optimal impedance matching will remain a cornerstone of successful high-speed digital communication.

Keep Learning