How Pick-and-Place Machines in SMT Assembly Works
7 min
- 1. Key Components of a Pick-and-Place Machine
- 2. Step-by-Step Pick-and-Place Process
- 3. Types of Pick-and-Place Machines
- 4. Comparison of Pick-and-Place Machine Types
- 5. Important Parameters & Design Considerations
- 6. Common Challenges & Solutions
- Conclusion
In the early days of electronics, everything on the IC was either DIP or through-hole, but with the invention of SMD, everything changed. The size of the components is reduced by more than 80%, thus the PCB cost and area are reduced, and small form factor PCBs with HDI interconnects are out there. With this miniaturisation of sizing, what comes is heat and power issues, but on the other hand, it also gives rise to the automated 'pick-and-place' machines. These are critical to the functionality of any Surface Mount Technology (SMT) line. These devices are capable of remarkably fast and precise placement of individual components, which are fetched from feeders and affixed to boards that have previously had solder paste applied to them. Students and engineers wishing to design dependable circuits with optimized production are required to understand the practical implementation of these machines and their vital parts.
JLCPCB offers affordable PCB fabrication and professional SMT assembly services with industry-grade pick-and-place lines. From prototype to small-batch production, you can order PCBs online in minutes and even preview real SMT assembly capabilities on their website.
1. Key Components of a Pick-and-Place Machine
A pick-and-place machine utilizes mechanical, optical, and software systems. Its core components enable high-speed, accurate placement:
1. Feeder Systems
Feeder systems organize and supply components to a pick-and-place machine in a dependable manner. Components are often provided in tapes and reels, trays, or tubes. Tape and reel feeders are widely used for miniature resistors, capacitors, and integrated circuits. Trays are used for larger, more fragile components such as connectors and oddly shaped components. Tube or bulk feeders are utilized for inexpensive, mass-packaged components. Feeder systems are configured to maximize accurate component indexing, improving nozzle's component pickup, throughput, and error reduction.
2. Pick-and-Place Head / Nozzles
The pick-and-place head moves items from the feeder to the PCB. Nozzle heads that generate vacuum suction and pick up parts with the nozzles. In the interest of speed, current models almost always have several heads working simultaneously. Various nozzles are available for almost all models, and some can even rotate and tip for better accuracy. To ensure that the speed and quality of placement are kept at a high level, routine cleaning is necessary to avoid mis-picks.
3. Vision & Alignment Systems
Vision systems enhance accuracy by inspecting components and precisely locating the PCB. Pre-pick cameras verify component orientation and detect defects, while pre-place cameras locate fiducial marks to calculate board position and rotation. Post-place cameras confirm placement and trigger corrections if necessary. Vision systems compensate for tolerances and thermal expansion, enabling high-precision placements.
4. Conveyor / PCB Handling
SMT lines transport PCBs using conveyors, which ensure board stability. Board movements are controlled by clamping the PCB to the holder, and conveyors are adjustable to various sizes.
5. Software / Control System
The software coordinates all machine operations, managing coordinates, rotations, nozzle assignments, feeder maps, and placement sequencing. This reduces the time that the heads are traveling, organizes placement order, records placement errors, and provides interfaces for operators to configure and maintain the system.
2. Step-by-Step Pick-and-Place Process
Understanding the process helps in designing boards for smooth assembly:
PCB Preparation & Solder Paste Printing: Solder paste is applied to PCB pads using a stencil printer. The key is proper deposit and stencil alignment for reliable results.
Feeder Setup & Component Loading: Operators load reels, trays, or tubes into specified feeders and map them in the machine software. Accurate mapping ensures correct part placement.
Board Loading & Fiducial Detection: The PCB is clamped on the conveyor. Cameras detect fiducial marks to calculate board offset and rotation.
Pick Operation: The nozzle moves to the feeder, picks a component via vacuum, and lifts it. Pre-pick vision checks verify correct pickup.
Transfer & Correction: During movement to the placement site, the component can be inspected. Software adjusts for small offsets in angle or XY position before placement.
Placement: The nozzle places the component onto the solder paste pad with controlled speed and force. For some parts, light tapping ensures flush seating.
Post-Place Inspection: Cameras verify position, rotation, and presence. If misplacement is detected, the machine either corrects it immediately or flags it for rework.
Repeat: The cycle continues until all components are placed. Boards then move to reflow soldering to permanently attach components.
3. Types of Pick-and-Place Machines
Machines are optimized around speed, flexibility, or precision:
High-speed ‘chip-shooters’: These are used to place large volumes of small passives quickly, with limited flexibility for large parts.
Precision Placers: These machines can achieve micron-level accuracy for fine-pitch ICs, QFNs, and BGAs.
Hybrid / Multi-Head Systems: These machines combine fast heads for passives and precision heads for ICs.
Benchtop / Prototyping Machines: Smaller machines that are lower in throughput for R&D or small runs. Machine selection depends on component mix and production volume.
4. Comparison of Pick-and-Place Machine Types
| Machine Type | Strengths | Limitations | Typical Use Cases |
|---|---|---|---|
| High-speed “chip-shooter” | Extremely fast for small passives | Limited flexibility for large/odd parts | Mass production of consumer electronics |
| Precision placer | Micron-level accuracy | Slower than chip-shooters | High-speed ICs, BGAs, and advanced modules |
| Hybrid / multi-head | Combines speed and precision | More complex, higher cost | Mixed designs with varied components |
| Benchtop/prototyping | Compact, affordable, good for R&D | Low throughput, not for mass production | Labs, prototyping, small-volume runs |
5. Important Parameters & Design Considerations
Key factors for evaluating or designing for pick-and-place:
Placement Accuracy: Expressed in microns; critical for fine-pitch ICs and BGAs. The better the accuracy of the machine, the better the resolution with which it places components onto the PCB.
Throughput: Measured in terms of components per hour (CPH). Higher speed may often reduce the variety of components each head can handle.
Component Size Range: Ensure nozzles and feeders accommodate all components. Because SMD covers a range from 01005 to 1206 and even bigger, nozzles will change accordingly.
Setup Time / Changeover: Component feeding and changing take time, which affects productivity. It is done as per the BOM of the specific PCB.
6. Common Challenges & Solutions
With the machines, the issues are also there; in these auto pick-and-place machines, everything is too fast. Because of the high speed and friction in the machines, problems like feeder jams, solder paste inconsistencies, contaminated nozzles, incorrect or absent component orientation will also be present.
Conclusion
In modern SMT assembly, pick-and-place machines are the key component, integrating mechanical motion, machine vision, and sophisticated software capabilities to position thousands of components very quickly and very accurately.
With the machines, the issues are also there; in these auto-pick and place machines, everything is too fast. Because of the high speed and friction in the machines, problems like feeder jams, solder paste inconsistencies, contaminated nozzles, and incorrect or absent component orientation will also be present. In addition to improved PCB design, fulfilling the needs of students and engineers begins with following well-established PCB design procedures. Proper machine preparation also contributes to reliable component placement.
Popular Articles
• Power Supply Symbols Chart: A Complete Guide to AC, DC, Ground, Battery, and Source Symbols
• How to Design and Assemble a Reliable ESP32 Module PCB on a 2-Layer Board
• How to Identify SMD LED Polarity: Markings, Testing, and PCB Tips
• Logic Gate Symbols: The Complete Chart, Truth Tables [2026]
• The Ultimate Guide to Relay Symbol: Coil, Contacts, Diagrams, and Circuit Applications
Keep Learning
What Is Tombstoning? A Practical Guide to Causes, Reflow Risks, Prevention, and Rework
Key Takeaways Definition: Tombstoning occurs when a small two-terminal component lifts off one pad during reflow and stands upright, leaving one end without a proper solder connection. Root Cause: Unequal solder wetting forces act on the two terminals, often due to differences in pad temperature, solder-paste volume, pad geometry, or thermal mass. Highest Risk: Small passive components, such as 0201 and 0402 resistors and capacitors, are especially susceptible because their low mass and small terminat......
12 Professional Soldering Tips and Tricks Every Beginner Should Know
Soldering is not merely "gluing" metal; it is a metallurgical process that creates an intermetallic compound (IMC). This molecular bond ensures the electrical and mechanical integrity of your device. A poor joint might pass a quick visual check but will inevitably fail under vibration or thermal stress, leading to "ghost" bugs and hardware failures. These soldering tips and tricks focus on practical, repeatable techniques used in professional electronics soldering—from correct heat transfer and flux u......
How to Solder SMD Components Like a Pro [2026 Updated]
Soldering is a core skill to know, and when it comes to SMD, things become more complex and smaller. Soldering is similar to welding, but instead of welding two iron/steel pieces, we are now welding small components. To develop a circuit, the best way to join two components is by soldering. There are two main types of components in electronics: one is a through hole with long legs covered with tin, which can be easily inserted onto a PCB and then soldered, and the other is SMDs (surface mount devices)......
The Ultimate Guide to Wafer Level Packaging (WLP): Process, Types, Benefits, and Applications
Modern electronics are hitting a hard limit: you can’t keep shrinking devices without rethinking how chips are packaged. As PCB space tightens and signal speeds increase, traditional packaging methods introduce too much size, parasitic loss, and inefficiency. Wafer-level packaging (WLP) addresses this by forming interconnects directly on the wafer before singulation, eliminating substrates and shortening signal paths. The result is a chip-scale package with higher integration density, lower parasitics......
Reading Motor Symbols: Common Types, IEC/ANSI Conventions & Typical Circuit Examples
Key Takeaways ⬇ Download the Free Motor Symbols Cheat Sheet (PDF) First find the basic designator: a circle marked M is a motor, a circle marked G is a generator, and the leads coming out of the circle are the connection terminals. Two drafting standards exist: IEC and ANSI/IEEE schematics differ slightly in appearance but represent the same class of motor, with windings and terminals marked in the same way. Read the auxiliary marks: use annotations such as AC/DC, ~, and 3~ to judge AC/DC type and pha......
Diode Type Guide: How to Choose the Right Diode for PCB and Product Design
Modern electronics rely on highly specialized diode types for power conversion, ESD protection, signal detection, and high-frequency switching. Choosing the wrong diode doesn't just reduce efficiency; it also generates excess heat, introduces switching losses, and can even damage sensitive circuits during voltage transients. Choosing the right component ensures a reliable board, whether you are wiring a prototype or scaling to low-volume PCB assembly. In this guide, you'll learn: How do different diod......