A Beginners Guide to Impedance Control in PCBs
5 min
- Impedance of a Circuit
- What is Impedance Matching?
- Commonly used Impedance Lines in PCB Design
- Impedance Matching PCB Design Considerations
- Impedance Calculation and Measurement of a PCB Track
- Conclusion
When a digital signal is transmitted from one point to another, it causes a change in the state of the signal line. This change can be understood as an electromagnetic wave moving through the circuit. Reflection occurs when this wave encounters a boundary between different mediums. At this boundary, some of the wave's energy continues as a signal, while the rest is reflected. This process repeats until the energy is either absorbed by the circuit or dissipated into the environment.
For electrical engineers, this boundary is typically defined by a change in electrical impedance. In PCB design, reflections happen when a signal encounters an impedance mismatch along a trace. This mismatch causes part of the signal to reflect back towards its source, leading to signal integrity issues such as distortion, noise, and data errors, especially in high-speed digital or RF circuits.
Impedance of a Circuit
In circuits with resistors, inductors, and capacitors, the total equivalent resistance that hinders the flow of current in the circuit is called impedance. Impedance is composed of resistive and reactive elements. Resistors dissipate a circuit’s energy as heat. The recoverable energy in a circuit exists in the electromagnetic fields that permeate and surround conductors, inductors, and capacitors.
Impedance is commonly represented by the symbol "Z" measured in ohms (Ω) and is a complex number, with the real part known as resistance and the imaginary part known as reactance. Impedance is the combined effect of resistance, inductance, and capacitance in AC circuits. The impedance of a specific circuit is not constant; its value is determined jointly by AC frequency, resistance (R), inductance (L), and capacitance (C), and therefore varies with changes in frequency.
What is Impedance Matching?
Impedance matching is a way to ensure compatibility between a signal source or transmission line and its load. It can be classified into low-frequency and high-frequency matching. In low-frequency circuits, where the wavelength is relatively long compared to the transmission line, reflections can be disregarded. However, in high-frequency circuits, with shorter wavelengths comparable to the length of the transmission line, reflected signals superimposed on the original signal can alter its shape and affect signal quality.
Signal Reflections:
The behaviour of circuits at high frequencies change due to parasitic effects like fringe capacitance and inductance. PCB signal traces also behave like transmission lines, and every point along the signal trace has impedance.
As a result, the original signal becomes distorted, and what was intended to be transmitted from the transmitting end may change by the time it reaches the receiving end. Therefore, to achieve distortion-free signal transmission, PCB signal traces must maintain consistent impedance.
Commonly used Impedance Lines in PCB Design
Impedance matching effectively reduces or eliminates high-frequency signal reflections. Commonly used impedance lines can be classified into the following four types:
1. Single Ended Impedance Line:
The single-ended impedance line refers to the impedance of a single trace on a PCB and is typically categorized into two main types: Microstrip and Stripline.
- Microstrip Line: A signal trace on the outer layer of a PCB, with a ground plane directly below it on an inner layer. The impedance is controlled by the width of the trace, the thickness of the dielectric (insulating material) between the trace and the ground plane, and the dielectric constant of the material.
- Stripline: A signal trace sandwiched between two ground planes, typically on inner layers of the PCB. The impedance is controlled by the trace width, the dielectric thickness above and below the trace, and the dielectric constant.
2. Differential Pair Impedance Line:
Two parallel traces carrying equal and opposite signals, typically used for high-speed data transmission. The impedance is controlled by the trace width, spacing between the traces, and the dielectric properties of the material. It has a normalized impedance of 90–110 ohms.
3. Coplanar Single Ended/Differential Pair Impedance Line:
A signal trace on an outer layer with ground planes on either side of the trace, typically on the same layer. The impedance is determined by the trace width, the spacing between the trace and the adjacent ground planes, the thickness of the dielectric below the trace, and the dielectric constant. It has normalized impedance of 50 ohms (single-ended), 90–100 ohms (differential pair).
Impedance Matching PCB Design Considerations
Impedance Calculation and Measurement of a PCB Track
For orders requiring impedance control, it is essential to provide your impedance requirements in the form of a table or diagram, along with the compressed PCB files. The general value of impedance of tracks are listed in the figure below with trace width, gap and layer information.
Using JLCPCB Impedance Calculator:
Open JLCPCB's "Impedance Calculator" and input the impedance values while selecting the corresponding layer stack-up and other relevant parameters like board thickness. Design the corresponding line width and spacing in your engineering data.
Important Manufacturer's Note: For orders with "Impedance Control" selected as "Yes", our factory will control the impedance within a tolerance of ±10%. If you choose "No", we will not control the impedance, but we will ensure that the line width and spacing are within a tolerance of +/-20%. Impedance control is not yet available for double-sided boards.
Conclusion
Impedance matching is a critical aspect of high-speed PCB design, ensuring optimal signal transmission and preserving signal integrity. By carefully considering impedance values, line widths, spacing, dielectric properties, and reference layers, designers can effectively minimize signal reflections and distortion. Implementing impedance-controlled lines and utilizing tools like JLCPCB's Impedance Calculator can streamline the design process and help achieve the desired impedance values. With proper impedance matching techniques, designers can enhance the performance and reliability of high-speed PCBs, enabling seamless transmission of electronic signals in modern electronic systems.
Popular Articles
Keep Learning
Building Effective ESD Protection Into PCB Design
Key Takeaways Layout Rules: ESD spikes rise in nanoseconds; routing layout matters more than part specs alone. Clamp First: Place TVS diodes right at the connector using direct, flow-through traces. Low-Inductance Ground: Use short, wide traces with immediate ground vias to prevent voltage shifts. Capacitance Limits: Use low-capacitance clamps (< 0.5 pF) on high-speed lines like USB 3.x. DFM-Ready: Account for standard via and trace tolerances to ensure reliable board fabrication. ESD protection on a ......
Managing Skin Effect Loss in High-Frequency PCB Design
Key Takeaways Skin Depth Shrinks: High frequencies force current to the trace surface, shrinking depth to 0.66 µm at 10 GHz. Roughness Adds Loss: Copper foil roughness lengthens current paths, sharply increasing high-speed resistance. Plating Affects Signals: Low-conductive finishes like ENIG nickel increase attenuation on exposed lines. Wider Traces Help: Wider traces and thicker dielectrics lower conductor loss by expanding current surface area. Use Smooth Foils: Pairing low-profile copper foils (VL......
How Impedance Controlled Routing Delivers Reliable High-Speed PCB Performance
Key Takeaways Impedance Controlled Routing is essential for reliable high-speed PCB performance above 1 Gbps, eliminating reflections, ringing, and bit errors by precisely targeting interface-specific impedances (USB 90 Ω, PCIe 85 Ω, DDR4 40/80 Ω, HDMI 100 Ω) through field-solver calculations, symmetrical stackups with continuous reference planes, stable low-loss dielectrics, and strict single-ended/differential routing rules. Manufacturing precision in etching, copper profile, and lamination, verifie......
Getting PCB Characteristic Impedance Right for Reliable Signals
Key Takeaways Impedance Defined: Characteristic impedance is set by trace geometry and the reference plane, not by copper DC resistance. Core Factors: Trace width, copper thickness, dielectric height, and dielectric constant determine the impedance value. Reference Plane: High speed traces need a continuous reference plane to prevent signal reflection. Factory Verification: Fabricators adjust trace width and check impedance using time domain reflectometry on test coupons. Design Approach: Select a sta......
Stop PCB Crosstalk Before It Becomes a Signal Integrity Problem
Key Takeaways NEXT vs FEXT: NEXT saturates with trace length, while FEXT grows linearly with distance. Spacing & Stackup: Apply the 3W rule and keep traces close to reference planes. Edge Rates: Fast rise times drive crosstalk more than clock frequency. Fab Margins: Etching variations reduce gaps, requiring extra layout clearance. Verification: Use DFM checks and TDR coupons instead of basic continuity tests. PCB crosstalk is the noise one trace pushes into its neighbor, even though the two nets are e......
Navigating the Impedance Landscape: Selecting the Right Impedance for USB, Ethernet, HDMI, and SD Card Interfaces
Introduction In the realm of high-speed digital communication, choosing the right impedance is a critical aspect of successful PCB design. Impedance matching ensures optimal signal integrity, minimizes reflections, and enhances the overall performance of interfaces such as USB, Ethernet, HDMI, and SD Card. In this blog post, we'll explore the importance of impedance, the factors influencing impedance selection, and best practices for ensuring reliable data transmission in these widely used interfaces.......