What are S-Parameters in High Frequency Design
4 min
- 1. Why Do We Need S-Parameters?
- 2. The Physical Meaning of S-Parameters
- 3. Understanding S11 to S22 (and Beyond)
- 4. The S-Parameter Design Approach
- Conclusion
S parameters are one of the main tools in high frequency design which are used to evaluate the circuits. In RF and microwaves the signal frequency becomes too high that a copper wire is not capable of carrying the signal and the probability of losing information much increased. We can not measure a signal by voltage or current but there are certain parameters, we can note the system behavior and then we can apply Scattering Parameter, or S-Parameter calculations. S-parameters might look like intimidating complex numbers, but they are simply a way to describe how RF signals behave at the ports of a network. It is just based on a two port network that determines how much power is reflected, transmitted, or absorbed.
1. Why Do We Need S-Parameters?
At low frequencies, we can use Ohm’s law and Kirchhoff’s laws easily because voltages and currents are well-defined. And to define the property of a system there we use parameters like Z, Y, H and G. But at high frequencies (above a few hundred MHz):
Wires act like transmission lines with distributed inductance and capacitance. Voltages and currents vary along that transmission line. Parasitics and radiation effects increase a lot and only matters. Measuring currents directly is difficult without disturbing the circuit. Instead of voltages and currents, S-parameters use traveling waves (incident and reflected) to describe the network’s behavior.
2. The Physical Meaning of S-Parameters
Imagine you have a component (e.g., amplifier, filter or antenna) with ports, input and output. Now to check the behaviour what we do is apply some input excitation and record the response. And in S parameter specially we are looking for signal reflection:
Through this we can note how the signal is reflected back (due to impedance mismatch). What part of the signal is transmitted to other ports? And the part of the signal lost as radiation or heat. The S-parameter is simply a ratio of these incident and reflected waves:
Where:
⦁ i = output port number
⦁ j = input port number
Now because there are two ports and 4 terminals, there are a total of 4 combinations. We will see these in the next section. And Sij parameter contains magnitude and phase information, which is used to predict the wave behaviour:
⦁ Magnitude (|Sij|) tells you how much of the signal is transmitted or reflected.
⦁ Phase (∠Sij) tells you the phase shift between input and output.
3. Understanding S11 to S22 (and Beyond)
For a 2-port network (common in RF), we have four S-parameters:
S11 (Input Match):
Input reflection coefficient at port 1, it tells how much signal is reflected back from port 1. Related to input return loss and VSWR. If S11 = 0, perfect match, no reflection and If |S11| is large, poor match, high reflection. In decibels the return loss is represented as:
S21(Forward Gain or Loss):
Forward transmission from port 1 to port 2, it tells how much signal passes from input to output. Related to gain (or loss). Positive dB means amplification and negative dB means attenuation.
S12(Reverse Isolation):
Reverse transmission from port 2 to port 1, measures reverse isolation. In amplifiers, we want S12 to be as low as possible to avoid feedback and oscillations.
S22(Output Match):
Output reflection coefficient at port 2, it tells how much signal is reflected back from port 2. Related to output return loss and load matching. It is very similar to S11, but at the output. And used to measure maximum power transfer to the load.
4. The S-Parameter Design Approach
First we have to measure or simulate S-parameters of the device. It is done through Vector Network Analyzers (VNAs) for measurement. Then we use S11 and S22 to design impedance matching networks. In this step we have to minimize reflections and maximize power transfer.
We have to determine maximum available gain (MAG) or maximum stable gain (MSG). To measure, we have to convert S-parameters to other network parameters (ABCD, Y, Z) when cascading devices. By adjusting component values to meet target S21 (gain), S11/S22 (matching), and S12 (isolation) specs.
Conclusion
S-parameters are the language of high-frequency design. An example to 4 parameters are:
⦁ S11 = -15 dB → good input match (VSWR ≈ 1.43)
⦁ S21 = 10 dB → amplifier provides ~10× voltage gain
⦁ S12 = -40 dB → excellent reverse isolation
⦁ S22 = -12 dB → decent output match
If you work in RF/microwave design measuring, and designing with S-parameters is essential. From antennas to filters to high-speed digital interconnects, they are the bridge between theory and real-world performance.
Popular Articles
• PCB Board Design: A Step-by-Step Guide for Beginners
• Design Guidelines for PCB Using FR4 Substrates
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
Keep Learning
PCB Board Design: A Step-by-Step Guide for Beginners
Key Takeaways 10-Step Beginner Guide: Covers EasyEDA schematic capture, DRC checks, and Gerber export for a 3A IP2312 charger. 3A High-Current Routing: Upgrades the 1A TP4056 design with 1.3–1.8 mm traces (1 oz copper) and stitched ground planes. Thermal & DFM Ready: Applies ESOP-8 thermal vias and JLCPCB 2-layer standard rules for reliable prototyping. Printed Circuit Boards (PCBs) form the backbone of most modern electronic devices, providing a platform to connect electronic components. For beginner......
Design Guidelines for PCB Using FR4 Substrates
Material substrate concerns are necessary while designing electrical circuit boards. This is due to the fact that printed circuit boards cannot be manufactured without the appropriate PCB materials. When developing and producing circuit boards, the substrate material must be taken into account just as much as the copper layers, silkscreen, and surface polish. Generally speaking, non-conductive materials like porcelain, Marlon, FR4, and the like must be used for PCB substrates. Depending on its intende......
Master PCB Board Circuit Diagrams: From Zero to Reading & Drawing Like a Pro
When designing a circuit for real applications, it is better to use PCBs. PCBs are the formal electrical representation of an electronic system. If you don't want the wires to be hanging with components and messy systems, it's better to turn it into a circuit board. To design a PCB board, there are 2 steps: first, the schematic design. The schematic shows how components such as ICs, capacitors, resistors and other components are interconnected. The schematic is the blueprint through which we can gener......
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Capacitor Voltage Rating Explained with Examples
Capacitors are small components widely used not only for power delivery but also for signal conditioning in electronic circuits. In this article, we focus on the capacitor voltage rating across different types of capacitors. At first glance, capacitors look simple—small cans, discs, or chips on a PCB. However, their markings carry essential design information, including capacitance and voltage rating. These are not arbitrary values but directly affect circuit reliability. Ignoring the voltage rating w......
From Prototype to Product with a Better Development Board
Note Prototype Fast: Development boards integrate power, clock, and programming circuits to validate firmware in hours. Pick the Right Platform: Use ESP32 for Wi-Fi/BLE, Arduino UNO for 5 V sensors, Raspberry Pi Pico for tight I/O timing, and Raspberry Pi 5 for Linux. Scale to Custom PCB: Reuse your prototype's certified module, firmware, and support circuits, but remove unused headers to cut unit cost. Build for Production: Use a 4-layer ground-plane stackup for wireless boards, verify BOM stock earl......