This website requires JavaScript.
Coupons
Ship to
Blog

Single-Sided PCB Design: Combining Simplicity with Sophistication

Published Sep 24, 2024, updated Nov 14, 2026

10 min

Table of Contents
  • Structure of a Single-Sided PCB
  • Soldering on a Single-Sided PCB
  • Engineering Design File of Single-Sided PCBs
  • Single-Sided PCB Design Considerations
  • Manufacturing Characteristics in Factories
  • Special Considerations for Single-Sided Aluminum PCBs
  • FAQs about Single-Sided PCB Design
  • Conclusion

Key Takeaways

  • Single-sided PCBs offer a simple, cost-effective solution for many electronic applications.
  • SMT and THT components require different mounting and soldering arrangements.
  • Proper layer orientation, Gerber files, and design rules help ensure manufacturability.
  • Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement.

A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections required for a circuit to function. Among the different PCB configurations, a single-sided PCB features a relatively simple structure with conductive copper traces on only one side of the insulating substrate.

Despite the increasing use of multilayer PCBs in advanced electronic devices, single-sided PCBs remain a practical solution for applications with relatively simple circuit layouts and cost-sensitive requirements, including remote controls, household appliances, basic control circuits, and other consumer electronics.

Understanding the structure, component placement, soldering methods, design file orientation, and manufacturing considerations of a single-sided PCB is essential for avoiding design errors and ensuring manufacturability. This guide explores these aspects and explains the key considerations when designing single-sided PCBs.

Structure of a Single-Sided PCB

A traditional FR-4 single-sided PCB consists of an insulating substrate and a conductive copper layer on one side. The copper layer forms the circuit traces and component pads, while the opposite side generally remains free of circuitry. Depending on the design and manufacturing requirements, solder mask is applied to the circuit side, and silkscreen markings can be added to the required side or sides.

Unlike conventional double-sided PCBs, standard single-sided PCBs do not require copper electroplating inside their through-holes. As a result, their hole walls are generally non-plated. This distinction is important when selecting components and designing through-hole connections, as electrical connections cannot be established between the two sides through an unplated hole.

JLCPCB Manufacturing Note: Certain FR-4 board thickness options, including 0.4 mm, 0.6 mm, 0.8 mm, and 2.0 mm, are handled by default under JLCPCB's double-sided PCB numbering rules. Consequently, the finished boards will have copper-plated through-holes. Always check the available layer-count and thickness options when placing an order.

comparison itemsSingle-Sided PCBDouble-Sided PCB
Conductive Copper Layers12
Circuit RoutingOne sideBoth sides
Plated Through-HolesGenerally not requiredCommonly used
Electrical Connection Between SidesNo plated-hole connectionPossible through plated holes
Circuit ComplexityRelatively simpleMore flexible
Typical ApplicationsBasic control circuits, consumer electronicsMore complex electronic circuits

Structure of a Single-Sided PCB

Soldering on a Single-Sided PCB

Since a single-sided PCB has conductive copper on only one side, component placement and soldering must be arranged according to the location of the copper layer and exposed pads. Depending on the component package and mounting method, two common approaches are used:

1.Same-Side Soldering

For surface-mount technology (SMT), components are mounted directly onto the exposed pads on the copper side of the PCB. Both the component body and its solder joints are located on the same side. This approach is suitable for compact layouts and components designed for surface mounting.

Same-Side Soldering

2.Opposite-Side Soldering

For through-hole technology (THT), the component body is typically placed on the side opposite the copper layer, while its leads pass through the drilled holes and are soldered to the pads on the copper side. Since standard single-sided PCBs generally have non-plated through-holes, the electrical connection is formed by soldering the component leads directly to the copper pads rather than relying on plated hole walls.

When designing a single-sided PCB with through-hole components, ensure that the hole locations, pad sizes, component orientation, and soldering access are properly arranged to support reliable assembly.

Opposite-Side Soldering

Engineering Design File of Single-Sided PCBs

PCB design software organizes circuit layouts into separate layers, such as the top copper layer, bottom copper layer, solder mask layers, and silkscreen layers. Understanding how these layers are displayed and exported is essential for preparing accurate manufacturing files.

In a double-sided PCB design, the top and bottom copper layers represent different physical sides of the board. When viewed from their respective sides, the two layers have different viewing orientations. This is why text or patterns on the bottom side may appear mirrored when viewed from the top side of the PCB.

Engineering Design File of Single-Sided PCBs

The same layer-orientation principle applies to single-sided PCBs. Depending on the selected copper layer, the circuit may be assigned to either the top or bottom layer in the design software. However, the displayed orientation in the CAD interface should not be confused with the final manufacturing orientation.

When preparing Gerber files, designers should export the correct copper, solder mask, silkscreen, drill, and board outline layers according to the PCB design. Do not manually mirror the copper layout unless the design software or manufacturer specifically requires it. Always review the exported Gerber files to verify that the circuit orientation and text placement are correct before submitting the design for fabrication.

Single-Sided PCB Design Considerations

When designing a single-sided PCB, several factors should be considered to ensure that the circuit layout is compatible with the manufacturing process:

  • Trace Width and Spacing: Since all circuit connections must be routed on a single copper layer, sufficient spacing and appropriate trace widths are essential to prevent short circuits and maintain electrical performance.
  • Component Placement: Components should be arranged to minimize unnecessary trace crossings and keep connections as short and direct as practical.
  • Hole and Pad Design: Through-hole component pads must provide sufficient annular ring area for reliable soldering, especially when using non-plated holes.
  • Copper Clearance: Maintain adequate clearance between copper features and board edges, slots, or other mechanical features to avoid manufacturing issues.
  • Manufacturing File Verification: Check the copper layer, drill data, solder mask, silkscreen, and board outline before exporting the final Gerber files.
Manufacturing ParameterJLCPCB Specification
Minimum Trace Width (1 oz, 1–2 Layers)0.10 mm
Minimum Trace Spacing (1 oz, 1–2 Layers)0.10 mm
Standard FR-4 Thickness Options0.4–2.0 mm
Standard Outer Copper Weight1 oz / 2 oz
Minimum Non-Plated Slot1.0 mm
Minimum Plated Slot0.5 mm

Manufacturing Characteristics in Factories

During PCB fabrication, the manufacturer may adjust the orientation of the production data to match the requirements of the manufacturing equipment and process. In the single-sided PCB production process described by JLCPCB, the bottom-layer circuit image is mirrored onto the top-side production orientation. This is a manufacturing data adjustment and does not change the original circuit layout or electrical connections designed by the customer.

Drilling quality is another important consideration in single-sided PCB manufacturing. The drill entry surface, backing material, and drilling parameters all affect hole quality and the formation of burrs. In JLCPCB's described production setup, the copper surface is positioned so that the drill bit enters through the copper side, with the base material providing support underneath. This helps achieve cleaner drilling results.

It is important to distinguish between the manufacturer's production-side adjustments and the customer's original PCB design. Designers should prepare and export the correct design files rather than attempting to reproduce factory-specific mirroring or drilling operations manually.

Manufacturing Characteristics in Factories

Special Considerations for Single-Sided Aluminum PCBs

Special Notes

Aluminum Base Layer:

A single-sided aluminum PCB typically consists of three layers: a copper circuit layer, a dielectric insulation layer, and an aluminum base. The dielectric layer electrically isolates the copper circuitry from the conductive aluminum substrate while allowing heat to transfer toward the metal base.

When designing single-sided aluminum PCBs, SMT components are generally recommended. Through-hole components should be avoided because their leads may extend through the board and come into contact with the conductive aluminum base, potentially causing short circuits.

JLCPCB recommends SMT components for its single-sided aluminum PCBs rather than conventional through-hole assembly. Designers should therefore consider component packages and mounting methods before choosing an aluminum substrate.

Silkscreen Printing:

For single-sided aluminum PCBs, silkscreen markings are generally recommended on the copper circuit side, where the solder mask provides a suitable surface for printing.

Printing directly on the bare aluminum surface is not recommended because the ink may have poor adhesion and can easily peel off. In addition, white markings may have insufficient contrast against the grayish-white aluminum surface, making them difficult to read.

If silkscreen printing on the bare aluminum side is necessary, the requirement should be clearly specified in the order remarks so that the manufacturer can review the feasibility.

JLCPCB Single-Sided Aluminum PCB Capabilities

When selecting a single-sided aluminum PCB, it is important to consider the available material thickness, copper weight, minimum drilling diameter, and routing requirements. JLCPCB provides the following specifications for its aluminum substrate service:

Manufacturing ParameterJLCPCB Specification
PCB Layer1 Layer
Board Thickness0.8 / 1.0 / 1.2 / 1.6 mm
Copper Thickness1 oz
Minimum Drilling Diameter0.65 mm
Minimum Trace Width / Spacing0.10 / 0.10 mm
Minimum PCB Size5 × 5 mm
Maximum PCB Size602 × 506 mm
Solder Mask ColorsWhite / Black
Silkscreen ColorsBlack / White
Minimum Routing Slot Width1.6 mm
Simplify Your PCB Production with JLCPCB

Your one-stop supplier for PCB fabrication, assembly, and components. From instant quoting to fast delivery, streamline your workflow, cut back-and-forth, and keep every build moving smoothly—prototype to production.

Get Instant Quote >

FAQs about Single-Sided PCB Design

Q: What is a single-sided PCB?

A single-sided PCB has a conductive copper layer on only one side of the substrate. It is commonly used in simple electronic devices due to its straightforward structure and cost-effective manufacturing.

Q: Can SMT and THT components be used on a single-sided PCB?

Yes. SMT components are mounted on the copper side, while THT components are inserted from the opposite side, with their leads soldered to pads on the copper side.

Q: Do single-sided PCBs have plated through-holes?

Conventional single-sided PCBs generally use non-plated through-holes because they do not require copper plating on hole walls. However, specific board options may differ depending on the manufacturer's process.

Q: What should be considered when designing a single-sided PCB?

Key considerations include trace width and spacing, component placement, pad and hole design, copper clearance, and proper layer orientation to ensure manufacturability.

Q: Can single-sided aluminum PCBs be used with through-hole components?

Special care is required. Since the aluminum base is conductive, through-hole component leads may contact it and cause short circuits. Proper electrical insulation and component mounting design are essential.

Conclusion

Single-sided PCBs offer a straightforward and cost-effective solution for electronic applications with relatively simple circuit requirements. However, their limited copper routing area makes proper component placement, soldering access, hole design, and layer orientation particularly important.

Understanding the differences between SMT and through-hole mounting, preparing accurate Gerber files, and accounting for manufacturing requirements can help prevent common design and fabrication issues. For specialized applications such as aluminum-based PCBs, material structure, electrical insulation, and assembly compatibility also need careful consideration.

By combining sound design practices with appropriate manufacturing processes, designers can make the most of single-sided PCBs in a wide range of electronic applications.

Keep Learning