Gerber Files: The Essential Tool for PCB Manufacturing - JLCPCB
4 min
- Generating Gerber Files Properly
- Importance of a Gerber Viewer
- Conclusion
When it comes to PCB manufacturing, Gerber files are an essential tool for ensuring that your PCB design is accurately translated into a physical product. Gerber files are a set of instructions that communicate the design specifications to the manufacturer.
As a leading PCB manufacturer in the industry, JLCPCB utilized a Gerber real-time analysis system for providing instant online quotes and a Free Gerber Viewer for free inspecting if Gerber files are 100% accurate for manufacturing file standards.
Save your time for back-and-forth manual checking. Experience JLCPCB Gerber analysis system.
A correct Gerber file is the first step to starting your excellent electronic project. In this article, we will discuss the importance of generating GERBER files properly and the role of a GERBER viewer in PCB manufacturing.
Generating Gerber Files Properly
To generate Gerber files in a proper way, you need to use software that can create the needed file format. This can be done using a variety of software, including CAD programs like KiCAD, Altium, Diptrace, EasyEDA or dedicated PCB design software. When creating Gerber files, it's important to ensure that they contain all of the design-related necessary information, such as the layers, drill holes, and board outline.
It's also important to double-check the files to ensure that they are error-free. Any mistakes or errors in the Gerber files can result in significant issues during the manufacturing process, leading to delays and additional costs. As such, it's essential to have an accurate and detailed Gerber file before submitting it for manufacturing. At JLCPCB, the CAM engineers will prepare the Data For Manufacturing based on the submitted Gerber files, but they will not touch or fix any design mistakes, instead, the engineers will inform the customer in some cases when the design does not match the manufacturing capabilities.
Importance of a Gerber Viewer
A Gerber viewer is a software tool that allows you to view the Gerber files before submitting them for manufacturing. This is an essential step in the PCB manufacturing process as it ensures that the files are error-free and contain all the necessary information.
As a PCB manufacturer, JLCPCB provides an online Gerber viewer as a reference for customers to check the uploaded Gerber files before proceeding to order the related PCB, but it remains a reference tool and the final produced PCB will be identical to the designed board and this is why we JLCPCB recommend using external powerful Gerber viewers for file checking.
The Gerber viewer allows you to zoom in on specific areas of the design, ensuring that there are no errors in the placement of components or drill holes.
It also provides a visual representation of the layers, helping you to identify any issues with the layer stackup.
Additionally, a Gerber viewer can also be used to check the manufacturer's output files, ensuring that the final product matches the original design specifications. By using a Gerber viewer, you can ensure that your PCB design is accurate and ready for manufacturing, saving you time and money in the long run.
Conclusion
Gerber files are an essential tool for PCB manufacturing, providing a set of instructions for the manufacturer to follow. To ensure that your Gerber files are generated correctly, it's important to use the right software and double-check the files for errors. A Gerber viewer is an essential tool for checking the files before submitting them for manufacturing, ensuring that your design is accurate and ready for production. By following these steps, you can ensure that your PCB design is manufactured correctly, accurately, and efficiently.
Here get quality PCBs for your awesome electronics projects. Up to $54 coupons for new users! Upload Gerber files and experience JLCPCB Gerber analysis system.
Keep Learning
How Laser-Made PCBs Are Used in Rapid Prototyping
Key Takeaways Speed & Precision: Digital lasers enable 24-hour quick-turn HDI and FPC prototyping without mechanical tooling. LDI Patterning: Replaces physical photo-films to deliver precise circuit traces down to 2/2 mil. HDI Microvias: UV/CO2 lasers drill 0.075–0.15 mm blind vias (1:1 aspect ratio) for 1+N+1 to 3+N+3 stackups. Laser Profiling & Stencils: Achieves ±0.05 mm FPC cut accuracy and ±0.003 mm LPKF stencil aperture precision. Laser DFM: Maintain ≥ 0.30 mm copper clearance on FPCs and ≥ 0.07......
A Beginners Guide to Tented vs Untented Vias
Via’s are important, If working at high speed design and HDI boards then they become super important. Choosing a type of via during PCB manufacturing matters. Via’s are basically joining two or more layer traces together. Shape, size and track length guidelines became more interesting at high frequency and high speed signals. Today in this article we will explore a fabrication side, the decision to use tented or untented vias. This beginner-friendly guide explains what tented vias are, the differences......
Understanding SMT PCB Boards Technology: An Essential Component of Modern Electronics
Surface Mount Technology (SMT) has changed manufacturing of modern electronics. It has made designs and assembly methods more efficient. Many modern electronics depend on SMT PCB boards, which make it possible for circuit designs to be small and efficient. This is what today's technology needs. This article discuss about many types of SMT PCB boards, their uses, and the best methods for designing and assembling them. 1. What is an SMT PCB Board? Printed circuit boards called SMT PCB boards, use surfac......
How to Choose the Right Prepreg Material for Reliable Multilayer PCB
Have you ever wondered what makes all those copper layers stick to a cross-section of a multilayer PCB? Prepreg material is the answer, and it is of much more importance than most engineers think it is. Choose the prepreg selection wrong, and you are predetermined to delamination, impedance drift, and long-term reliability problems. Prepreg is not only glue. It is a designed composite that determines your dielectric separation, dictates your impedance, affects signal loss, and determines your board be......
Via Filling Explained: Key Techniques, Benefits, and Solutions for High-Performance PCBs
Key Takeaways Via filling completely fills plated through-holes and microvias with epoxy or conductive copper paste, followed by planarization and copper capping (POFV). It eliminates voids, solder wicking, and thermal/mechanical issues while enabling reliable via-in-pad designs. Benefits include superior heat dissipation (up to 8 W/m·K), better signal integrity, higher mechanical strength, and improved assembly yields. JLCPCB provides free non-conductive filling + POFV on 6+ layer boards. Ideal for H......
How Fiducial Markers Guarantee Perfect Alignment in Professional PCB Fabrication
Today, the most sophisticated pick-and-place machine can place a 0.5 mm pitch QFP on its footprint, board after board, thousands of times, and never miss. It is not only a matter of expensive cameras or high-quality servos, but it begins with a little, very small copper dot, simply hanging there in the corner of your PCB. That dot represents a fiducial marker, and without it, even the smoothest SMT line would be laying components in the dark. The unrecognized heroes of automated assembly are the fiduc......