FR4 vs Rogers: Which PCB Material Should You Choose?
6 min
- What is FR4
- What is Rogers
- Types of Rogers PCB Material
- 7 Main Difference Between FR-4 and Rogers Material
- Conclusion
Traditionally, manufacturers have been making PCBs or printed circuit boards of materials that offer resistance to heat and are, therefore, less expensive to produce. As the electronics industry is increasing in terms of high frequency application, only FR4 is not enough. Some equipment, while not being subject to extreme temperatures, may have to work at RF or radio frequencies. According to the extreme performance conditions demanded by RF, specialized materials such as Rogers are necessary to deliver the best functionality from PCBs. See our recent article on different types of via's in pcb design. Rogers extensive PCB material portfolio enables its use in diverse applications, including:
- 5G NR mmWave antennas
- Satellite communications
- Radar systems
- Automotive sensors
- Aerospace Avionics
- High-speed datacom
- Test instrumentation
Let's explore what makes Rogers PCB materials such superior solutions for these cutting-edge electronics domains.
What is FR4
FR4 is a thermoset glass fabric reinforced epoxy resin composite. It is the traditional material that is the basis for most PCBs and is an acronym for Flame Retardant Level 4. Being a composite material made of epoxy and glass fiber, manufacturers shape it in the form of sheets and laminate it with copper foil on one or both sides.
Key properties and characteristics of FR4:
Low cost - FR4 is one of the most economical PCB substrate materials
Moderate dielectric constant - Around 4.5 at 1 MHz
Moderate loss tangent - Around 0.02 at 1 MHz
However, FR4 suffers from performance limitations at higher frequencies due to dielectric losses, making it unsuitable for many RF applications. The relatively high and inconsistent dielectric constant and loss tangent also make FR4 a poor choice for precision analog and high-speed digital circuits.
What is Rogers
Unlike FR-4, the Rogers substrate materials offer different compositions. Some of them use a ceramic base rather than glass. Various compositions are available, such as woven glass reinforced with hydrocarbons, and they offer electrical performance very close to that of PTFE.
Some key properties of Rogers materials:
Stable dielectric constant - Tightly controlled, varies by material in the 2.9 - 10.2 range
Low loss tangent - Around 0.0009 - 0.002 at 10 GHz
Excellent high frequency performance - Low signal loss up to mmWave frequencies
Low thermal expansion - Matching the coefficient of copper for reliability
The precise dielectric properties, close matching to copper, and low losses make Rogers an ideal choice for performance-driven microwave, telecom, aerospace and high-reliability applications. However, the exotic material compositions result in Rogers costing 5-10x more compared to FR4 on a per area basis.
Types of Rogers PCB Material
Rogers makes various types of PCB material for different applications. These include:
7 Main Difference Between FR-4 and Rogers Material
1. Frequency of Operations
The major difference between regular boards made of FR-4 and those with Rogers material is in their application. PCBs made of FR-4 can operate properly only when the frequency of operations is within a certain range. On the other hand, PCBs made of the Rogers material can perform over a much larger range of frequencies. For instance, while FR-4 PCBs can hardly reach 10 MHz, Rogers PCBs can operate very well in applications extending well beyond 500 MHz.
2. Material Hardness
There is a substantial difference in material hardness between FR-4 and Rogers material. FR-4 is mainly epoxy resin and quite hard. On the other hand, Roger’s material, being hydrocarbon, is comparatively softer.
3. Processing Technology
Although Rogers materials are meant for high-frequency operation, they are different from PTFE microwave PCB materials. Roger’s series of materials does not require any special treatment, such as special treatment for through-hole processing, and no extra technological processes are necessary.
The FR-4 material is epoxy glass cloth laminate, which offers stable electrical insulation, a smooth surface, good flatness, and no pitting. It is suitable for products requiring good electrical insulation. This material is also suitable for use as backing boards for PCB drilling, FPC stiffeners, planetary gears, test plates, motor insulators, and many more.
4. Cost
Cost is an important factor for electronic equipment. Customers look for manufacturers offering PCBs with the best and most economical performance. Although making boards with FR-4 can save costs, this material is suitable for products operating at low frequencies and moderate temperature settings. On the other hand, for applications requiring high-speed operation or high temperatures, using Rogers material would be more suitable, even if it is more expensive.
5. Impedance Stability
The maximum dielectric constant of FR-4 material is 4.5. In comparison, Roger’s material has a dielectric constant of about 2.2-12.85. The higher dielectric constant of Rogers material contributes to high impedance stability.
6. Thermal Capability
For applications operating at high speeds, the PCB must also have better thermal capacity to prevent it from overheating and causing operational problems. Rogers PCBs, with their higher thermal capabilities, perform better than FR-4 at high temperatures and for high-speed applications.
7. Signal Integrity
Rogers PCB material has a dissipation factor of 0.004%. In comparison, the dissipation factor for FR-4 material is 0.02%. The significantly lower dissipation factor of the Rogers PCB material contributes to a substantially lower signal loss, thereby improving the signal integrity.
Conclusion
We have presented a comprehensive comparison between regular FR-4 and Rogers PCB materials, and how to select the most optimum material for an application. The Rogers PCB materials have the advantage of not requiring any special process for fabricating PCBs. In suitable cases, designers can offset the higher cost of Rogers material by using it only for layers that handle high frequencies and using FR-4 for others.
For printed circuit board fabrication involving radio and microwave frequencies, mobile networking, and space technology, Rogers PCB materials offer uncompromising performance compared to any other types of PCB materials, including FR4. While being more expensive in comparison to other materials, Rogers PCB materials are worth the extra cost when printed circuit boards must work in unfavorable environmental conditions, at high frequencies, and with very high reliability.
Popular Articles
• The Hardware Development Process: From Concept to a Finished Electronic Product
• Understanding the Basics of Electronic Devices and Circuits
• Understanding Digital Circuit Timing: Setup Time, Hold Time, Contamination Delay & Clock Skew
• PCBs Explained: A Simple Guide to Printed Circuit Boards
• Guide to the Top 10 Commonly Used Electronic Components
Keep Learning
PCB Layers Explained : Building Better Boards Through Smart Stackup, Standards, and Design Practices
A PCB is a sandwich of copper and insulating sheets that are stacked together to form a circuit board. Each PCB layer has a specific purpose; for example, some carry signals (traces connecting components), while others serve as solid planes for power or ground. Think of PCB layers like the floors in a building, where each floor can have a different role. Think of it as offices (signals) on one floor and storage (ground/power) on another. The number of layers varies by design complexity, from just one ......
Understanding Industrial PCB Production:Materials, Manufacturing Processes, and JLCPCB Capabilities
Key Takeaways Layer Capabilities: Supports up to 32-layer Rigid and 24-layer HDI PCBs (Rigid-Flex unsupported). Industrial Materials: High-Tg FR-4 (Tg 170°C), Aluminum cores, and Rogers RF laminates. Free POFV Technology: Free resin-filled via-in-pad provided for 6–32 layer designs. Turnkey Assembly: Integrated online DFM checks and automated SMT assembly. Nearly all electronic devices rely on Printed Circuit Boards (PCBs) as their foundational backbone, supporting and interconnecting active and passi......
Types of PCB Boards: Ultimate Reference with Specs & Use Cases
A printed circuit board (PCB) consists of laminated insulating and conductive materials that connect multiple electrical devices. A PCB can be thought of as a layered composite of fibreglass and epoxy with copper patterns etched onto it. These serve as electrical conductors and pathways for signals and power. A PCB can be Simple (one layer of conductive material), Double-Sided (two conductive layers), or Complex (three or more conductive layers) to allow numerous circuit paths on a small piece of hard......
Series vs Parallel Circuits: Key Differences, Advantages, and Applications
Series and parallel circuits are fundamental to understanding electronics and designing efficient electrical systems. These configurations define how components like resistors, capacitors, and diodes are connected in a circuit, influencing the overall behavior of the system. Usually a circuit schematics contains a lot series and parallel combined elements embedded with each other in order to perform certain functions. Circuits consisting of just one battery and one load resistance are very simple to a......
Master PCB Warpage Control with Proven Causes, Prevention Techniques & Professional Manufacturing Solutions
PCB warpage remains one of the most persistent challenges in modern electronics manufacturing. Even minor deviations in flatness can disrupt automated assembly lines, cause solder joint failures, and compromise long-term reliability in high-density designs. Effective PCB Warpage Control starts with understanding the root mechanisms and applying proven engineering practices from design through fabrication. Leading manufacturers achieve consistent results by combining symmetric layouts, thermally stable......
Importance of Printed Wiring Boards (PWB) in Modern Electronics
Printed wiring boards, or PWBs is very crucial for modern electronics. Almost every electronic device is built on these components. PWBs are an important part of putting together and connecting electronic parts because they provide the mechanical and electrical links that the parts need to work well. All modern technologies center on PWBs, from heavy tools to cellphones. This article will discuss the significance of printed wire boards (PWBs) in electronics, highlighting their construction, types, fun......