What are the Principles and Techniques for PCB Layout?
4 min
- Principles of PCB Layout:
- Techniques for PCB Layout:
- Conclusion:
Printed Circuit Boards (PCBs) are an indispensable part of electronic devices, with their performance and reliability directly impacting the operation of the entire system. PCB, short for Printed Circuit Board, is also known as a printed wiring board. It is a critical electronic component, serving as the support structure for electronic components and the medium for their electrical interconnections. It's called a "printed" circuit board because it's made using electronic printing techniques.
Routing is a critical step in PCB design, as it determines the performance and stability of the circuit board. This article will explore the principles and practical techniques for PCB layout to help engineers achieve better results in their designs.
Principles of PCB Layout:
- Follow the Circuit Schematic: Routing should strictly adhere to the circuit schematic to ensure correct connections and prevent short circuits or open circuits. Each component in the circuit should be labeled during routing for future maintenance and troubleshooting.
- Consider Signal Flow: When routing, consider the path of signals and aim to make signal traces as short as possible to minimize signal attenuation and noise. For high-frequency signals, pay attention to impedance matching to avoid signal reflection and distortion.
- Layered Routing: In multilayer PCBs, routing should be organized into layers based on circuit functionality. For instance, power and ground planes should be routed separately to reduce noise. Different signal layers should also be isolated to prevent interference.
- Avoid 90-Degree Bends: Signal traces should avoid sharp 90-degree bends during transmission, as they can increase signal reflections and noise, degrading signal quality. If necessary, use 45-degree bends or curved routing transitions.
- Ground Plane Design: Proper ground plane design is crucial for PCB reliability. Ensure that ground planes are as wide as possible to reduce impedance and enhance stability. Avoid 90-degree bends in ground traces to maintain continuity.
Techniques for PCB Layout:
- Use Automated Routing Tools: Modern circuit design software often provides automated routing features that can greatly simplify the routing process. These tools allocate routes and optimize paths based on the circuit schematic. Manual adjustments can be made as needed to achieve optimal results.
- Post-Layout Verification: After routing is complete, conduct a series of checks to ensure the correctness and reliability of the layout. Check for trace continuity, conductivity, impedance matching of signal lines, and stability of power and ground connections. Additionally, utilize simulation tools to validate circuit performance and reliability before actual fabrication.
- Utilize Filling and Copper Pour: In the layout process, you can use filling and copper pour techniques to improve PCB performance and stability. Filling can be used to fill gaps on the PCB, enhancing mechanical strength and thermal stability. Copper pour can serve as ground planes or power traces, increasing circuit reliability and stability. However, keep in mind that filling and copper pour can affect the PCB's thermal expansion, so careful consideration is required in specific designs.
- Layout Optimization: During routing, optimize trace widths and spacing, ground plane layouts, and power trace paths to minimize signal reflection, noise, and crosstalk issues. Consider using differential pair routing techniques to enhance signal integrity and reliability.
- Accumulate Experience and Techniques: Routing is a task that requires experience and skill, which can be gained through practice. Engineers should stay updated on the latest routing technologies and tools, learn from the experiences and methods of other designers, and continually improve their routing skills and design capabilities. Utilizing simulation tools for virtual testing can also help validate design feasibility and reliability before actual production.
Conclusion:
In summary, PCB layout is a task that relies on fundamental principles and the application of techniques. Engineers need to understand circuit schematics, plan routing paths logically, optimize routing techniques, and focus on accumulating experience and using tools effectively to enhance circuit performance and stability in their designs.
Keep Learning
The Ultimate Guide to PCB Layout Design
Key Takeaways PCB Layout Fundamentals: Component placement and routing are essential to achieving optimal PCB performance, reliability, and manufacturability. Follow a Structured Design Process: Start with schematic transfer and board dimension definition, followed by stackup planning, component placement, routing, and design file generation. Optimize Placement and Signal Integrity: Proper component placement, signal integrity, and thermal management are key to creating a reliable PCB layout. Consider......
CAN Bus PCB Layout Guidelines for Reliable Networks
Key Takeaways Route CANH and CANL as a 120 Ω differential pair, and solve trace width and spacing from your actual stackup. Follow the signal-path placement order: bus connectors, 120 Ω termination, transceiver, CAN controller. Reserve footprints for TVS/ESD diodes and a common-mode choke if the environment is noisy. Terminate only the two physical end nodes, and switch the 120 Ω resistor in or out with a jumper so one board works at the end or in the middle of the bus. Keep on-board stubs effectively......
What are the Principles and Techniques for PCB Layout?
Printed Circuit Boards (PCBs) are an indispensable part of electronic devices, with their performance and reliability directly impacting the operation of the entire system. PCB, short for Printed Circuit Board, is also known as a printed wiring board. It is a critical electronic component, serving as the support structure for electronic components and the medium for their electrical interconnections. It's called a "printed" circuit board because it's made using electronic printing techniques. Routing ......
PCB Layout Guidelines for USB Type-C
Key Takeaways Follow the Correct Component Order at the Interface: Working outward from the connector, place the ESD device first, then the common-mode inductor, then the capacitor, and keep the voltage regulator as close to the connector as possible. Put the TX coupling capacitors near the interface and the RX capacitors at the device end. Control Impedance Before Anything Else: Route the SuperSpeed pairs as 90 Ω ±10% transmission lines with a continuous, unsegmented ground reference plane, and keep ......
PCB Design Rules and Guidelines: A Complete Best Practices Guide
Key Takeaways Avoid Respins: Run early Schematic ERCs to stop design errors before layout begins. Protect SI/PI: Follow the 3W rule and never route high-speed traces over split ground planes. Match JLCPCB DFM: Set your DRC to JLCPCB capabilities (e.g., ≥ 3.5 mil trace/space, ≥ 0.15 mm vias). Use Free POFV: Utilize Via-in-Pad for dense boards—free on JLCPCB 6 to 20-layer stackups. Pre-Verify Designs: Use JLCPCB’s free online DFM and impedance tools to ensure first-time production success. Introduction ......
BGA PCB Design Complete Guide: Layout and Routing Guidelines
Key Takeaways Define pad type first: Always confirm SMD or NSMD pad strategy before routing BGA fanout. NSMD is generally preferred for better solder joint formation, while SMD suits very small pads or tight mask registration. Match the process to the pitch: 0.8 mm BGAs work with dog-bone fanout and standard vias; 0.5 mm BGAs typically need via-in-pad or HDI routing. Picking the right via strategy early saves layers and cost. Place decoupling capacitors on the bottom side: Mount MLCCs directly under t......