How to Select the Right Surface Mount Capacitor
7 min
- What Is a Surface Mount Capacitor?
- How Surface Mount Capacitors Work
- Common Package Sizes of Surface Mount Capacitors
- Types of Surface Mount Capacitors
- Applications of Surface Mount Capacitors
- Advantages of Surface Mount Capacitors
- Limitations of Surface Mount Capacitors
- How to Select the Right Surface Mount Capacitor
- Surface Mount Capacitors vs. Through-Hole Capacitors
- Conclusion
Capacitors are basically similar to small batteries. These units store energy in the form of an electrostatic field and deliver it to the load whenever required. Usually, they are big and used in circuit design as decoupling, energy storage, signal conditioning, and much more, depending on the use case scenario. Because it is the basic building block of an electronic circuit, we should have knowledge about the types of capacitors, where to use them, and what specific type is required. SMT (Surface Mount) capacitors do not use drilled holes due to their small size, stability, and almost zero failure rate. Let’s dive deeper into the concept and see the types of capacitors in some of the next sections.
What Is a Surface Mount Capacitor?
A surface-mount capacitor with the flat metal leads soldered to a printed circuit board (PCB). In contrast, through-hole capacitors require wire leads soldered or inserted into drilled holes; surface-mount capacitors can be attached directly to a metal pad or onto the PCB and are ideal for highly automated placement.
They serve the same basic purposes: storing and releasing charge, filtering signals, and stabilizing voltage, but they do it in a far smaller footprint. They have gained popularity with the advancement of electronics miniaturization and are now considered essential in mobile phones, laptops, vehicle equipment, and IoT applications.
How Surface Mount Capacitors Work
A surface mount capacitor performs the same function as any other capacitor: it stores and releases energy between two conductive surfaces separated by an insulating material. When connected in a circuit:
- In DC circuits, capacitors act as energy storage devices that charge and discharge as needed.
- In AC circuits, AC-coupling capacitors pass alternating current and block direct current, but are used to couple one circuit to another while blocking the DC component on a given line.
The most recognizable application of SMD Capacitors in digital electronics is decoupling. They are placed near the IC of an integrated circuit to filter and eliminate noise, providing a stable power supply to sensitive ICs.
Common Package Sizes of Surface Mount Capacitors
SMD capacitors are standardized in package sizes defined by the EIA code, which specifies the length and width in hundredths of an inch. Some of the most common sizes are:
| EIA Code | Metric Size (mm) | Typical Use |
| 0201 | 0.6 × 0.3 mm | Ultra-compact devices, smartphones |
| 0402 | 1.0 × 0.5 mm | High-density PCBs, RF circuits |
| 0603 | 1.6 × 0.8 mm | Consumer electronics |
| 0805 | 2.0 × 1.25 mm | General-purpose designs |
| 1206 | 3.2 × 1.6 mm | Power supply decoupling |
| 1210 | 3.2 × 2.5 mm | Higher voltage applications |
Miniaturization is a key result of accommodation packages such as 0201 and 01005 for advanced electronics. However, for the third blade section molded structure, larger packages are still required if higher capacitances or voltage ratings are to be achieved.
Types of Surface Mount Capacitors
Multilayer Ceramic Capacitors (MLCCs)
A multilayer ceramic capacitor is surface-mountable, and in which the ceramic multicore forms its layers. Alternating layers are used for the dielectric and as an electrode, with one common layer designated to connect them. These capacitors cover a wide capacitance range (picofarads to hundreds of microfarads), have low ESR, and perform well at high frequencies.
Tantalum Capacitors
Tantalum capacitors provide high capacitance density in a tiny size. They are polar; they must be properly oriented when fitted. They are mass-produced and used in power supplies for electronic equipment. In comparison to other capacitors, they provide stable capacitance over time and are valued for their mini size compared to electrolytic capacitors.
Aluminum Electrolytic Capacitors
These are also known as high-capacitance aluminum electrolytic capacitors. They are occasionally sold in surface-mount cylindrical packages. They are necessary for low-frequency filtering, bulk energy storage, and power supply smoothing applications. They’re a good option for power circuits that require high capacitance.
Film Capacitors
SMD film capacitors are not as well-known, but they can be used in specific applications such as audio circuits, where low dielectric losses with high stability are preferred, and precision timing circuits.
Applications of Surface Mount Capacitors
Surface-mount capacitors are widely used in electronic devices because of the variety of available mounting options. They can usually be found near an IC's power pins (for decoupling or bypassing) to assist in suppressing noise at high frequencies. They are also employed in RF circuits and power supply filters, hoping to control interference, voltage level, etc. They can also serve as a medium of signal coupling in many circuits, facilitating AC while blocking the unwanted DC. The time to lose or the set oscillator frequency of a circuit (oscillator, resonator) is also tuned by surface-mount capacitors. They are also small secondary storage devices, providing short-term buffering during power management systems.
Advantages of Surface Mount Capacitors
- Small form: PCB space-saving, facilitating miniaturization.
- Machine use: Can be used by a machine.
- Very reliable: No mechanical stress on flat connections.
- High-frequency performance: This is especially for MLCCs.
- Economical: Because they are mass-produced, they are quite affordable.
Limitations of Surface Mount Capacitors
Since the size was reduced too much, there are some limitations to this. Capacitance is like a storage of charges; if we need to store more, then a bigger one is required. The size also depends on the voltage rating. When scaling down to the SMT ones, capacitors lose their ability to store high charge and their operating voltage range. Smaller ones are mechanically fragile due to their small size and can crack if handled roughly. In cases where they aren't suitable for high-energy storage applications, you will want electrolytic or film capacitors instead. But these capacitors took very less space on the SMT PCB.
How to Select the Right Surface Mount Capacitor
Consider Electrical Requirements
- Capacitance value: Match to application requirement (decoupling vs. filtering).
- Voltage rating: You select the voltage rating of the capacitor to be 20–30% higher than the operating voltage for reliability.
- Tolerance and ESR: Important for RF and precision applications.
Consider Mechanical & Size Constraints
- The package size must be relevant to the PCB layout.
- Thinner packages are essential in smartphones and compact IoT devices.
Consider Application Environment
- Automotive systems demand capacitors with high temperature stability.
- Consumer electronics prioritize miniaturization.
- Industrial systems need a long lifetime and durability.
Consider Cost and Availability
The least costly capacitors are typically MLCCs, as they are also the most prevalent and best suited for higher production quantities. Higher-performance (expensive) variants, such as tantalum or film capacitors, have performance advantages in some applications.
Surface Mount Capacitors vs. Through-Hole Capacitors
| Feature | Surface Mount Capacitor | Through-Hole Capacitor |
| Size | Very small, compact | Larger, bulkier |
| Assembly | Automated SMT | Manual or wave soldering |
| Reliability | High, low inductance | Robust but higher parasitics |
| Applications | Consumer, automotive, RF | Power supplies, audio, legacy designs |
However, through-hole capacitors are still used for power and high-energy applications; they've been largely replaced by SMD capacitors in most modern PCB designs due to their space-saving benefits.
Conclusion
Surface-mount capacitors are another key innovation in contemporary electronic design. Starting from MLCCs for smartphones to tantalum capacitors in power circuits, they deliver dependable performance in a small space. In terms of the small size, high-frequency performance, and automation compatibility, this constitutes a trio that any PCB designer is hard-pressed to ignore. Although we made a difference guide also for SMT and TH components.
Designers should carefully evaluate electrical requirements, mechanical limitations, and environmental conditions when choosing an SMD capacitor. With a good selection of packages and types, an engineer can achieve the best performance while increasing cost-effectiveness in their design.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......