Understanding Impedance Matching for High-Speed PCB Designs
5 min
- What is Impedance Matching?
- Impedance Design Considerations
- Impedance-Control Ordering Instructions
- Conclusion
With the advancement of technology and the ever wider application of integrated circuits, the frequency and speed of electronic signal transmission have been increasing, making it essential for PCB conductors to provide high-performance transmission lines. These transmission lines are responsible for delivering signals from a source to the input of a receiver accurately and completely. This requirement emphasizes the need for impedance matching.
Electrical impedance, commonly represented as Z and measured in ohms (Ω), refers to the combined effect of resistance, inductance, and capacitance in AC circuits. The impedance of a specific circuit is not constant; its value is determined jointly by AC frequency, resistance (R), inductance (L), and capacitance (C), and therefore varies with changes in frequency.
What is Impedance Matching?
Impedance matching is a way to ensure compatibility between a signal source or transmission line and its load. It can be classified into low-frequency and high-frequency matching. In low-frequency circuits, where the wavelength is relatively long compared to the transmission line, reflections can be disregarded. However, in high-frequency circuits, with shorter wavelengths comparable to the length of the transmission line, reflected signals superimposed on the original signal can alter its shape and affect signal quality.
As shown in the diagram above, a signal is transmitted from the source A, passes through the intermediate transmission line, and enters the receiving end B. During this transmission process, parasitic resistances, capacitances, and inductances in the circuit hinder high-speed signal transmission. When the signal propagates between these elements and encounters inconsistent impedance, it may lead to signal reflection, resulting in signal distortion.
Impedance matching effectively reduces or eliminates high-frequency signal reflections. Commonly used impedance lines can be classified into the following four types:
Impedance Design Considerations
(1) Impedance-controlled lines can be designed on the outer layer (all four types mentioned above are outer layer impedances) or the inner layer.
(2) The magnitude of impedance values depends on the product design and chip type. In general, component manufacturers have preset impedance values for signal sources and receivers (e.g., SDIO: single-ended 50 ohms, USB: differential 90 ohms).
(3) Impedance-controlled lines must have a reference layer, typically using adjacent ground or power layers as reference (e.g., for top layer impedance, the reference layer is usually the second layer).
(4) The purpose of the reference layer is to provide a return path for the signal and act as electromagnetic shielding. Thus, the reference layer must be poured with solid copper.
(5) Factors influencing line impedance
Line width: Impedance is inversely proportional to line width; the narrower the line, the higher the impedance.
Dielectric constant: Impedance is inversely proportional to the dielectric constant; the lower the dielectric constant, the higher the impedance.
Solder mask thickness: Impedance is inversely proportional to the solder mask thickness; the thicker the solder mask, the lower the impedance.
Copper thickness: Impedance is inversely proportional to the copper thickness on the surface; the thinner the copper, the higher the impedance.
Line spacing: Impedance is directly proportional to the distance between impedance lines; the greater the spacing, the higher the impedance.
Dielectric layer thickness: Impedance is directly proportional to the dielectric layer thickness; the thicker the dielectric layer, the higher the impedance.
(6) Calculation method for impedance lines: It is recommended to use JLCPCB's "Impedance Calculator" (click here for direct access). Alternatively, you can download impedance calculation software (e.g., SI9000) and combine it with our lamination parameters for calculations.
(7) A quick note on "line width and spacing": Line width refers to the horizontal width of the line, the distance from one edge of the line to the other edge. Line spacing refers to the distance from the edge of one line (or the surrounding copper plane) to the edge of a different line.
Impedance-Control Ordering Instructions
For orders requiring impedance control, it is essential to provide your impedance requirements in the form of a table or diagram, along with the compressed PCB files.
Open JLCPCB's "Impedance Calculator" and input the impedance values while selecting the corresponding layer stack-up and other relevant parameters like board thickness. Design the corresponding line width and spacing in your engineering data.
Important reminder: Currently we can only ensure that the traces width and spacing are within a tolerance of +/-20%.
Conclusion
Impedance matching is a critical aspect of high-speed PCB design, ensuring optimal signal transmission and preserving signal integrity. By carefully considering impedance values, line widths, spacing, dielectric properties, and reference layers, designers can effectively minimize signal reflections and distortion. Implementing impedance-controlled lines and utilizing tools like JLCPCB's Impedance Calculator can streamline the design process and help achieve the desired impedance values. With proper impedance matching techniques, designers can enhance the performance and reliability of high-speed PCBs, enabling seamless transmission of electronic signals in modern electronic systems.
Popular Articles
Keep Learning
A Beginners Guide to Impedance Control in PCBs
When a digital signal is transmitted from one point to another, it causes a change in the state of the signal line. This change can be understood as an electromagnetic wave moving through the circuit. Reflection occurs when this wave encounters a boundary between different mediums. At this boundary, some of the wave's energy continues as a signal, while the rest is reflected. This process repeats until the energy is either absorbed by the circuit or dissipated into the environment. For electrical engi......
Design Guide for USB-3.0 Differential Signaling
In the world of data transfer, USB 3.0 is the Usain Bolt to USB 2.0’s friendly jogger. USB 2.0 is called “High Speed” and limped along at 480 Mb/s, whereas USB 3.0 SuperSpeed rockets up to 5 Gb/s (over ten times faster). But this speed jump brings full‑duplex operation and new differential transmit (SSTX) and receive (SSRX) pairs on dedicated pins. USB 2.0 D+/D– lines handle enumeration and legacy data, while two new 5 Gb/s high‑speed differential pairs carry SuperSpeed data in each direction. While m......
Can PCB Simulation Prevent Costly Manufacturing Revisions?
Key Takeaways PCB simulation identifies electrical, thermal, and EMC issues before fabrication, helping reduce costly design revisions. Signal integrity, power integrity, thermal, and EMC analysis address different PCB performance risks. Accurate simulation depends on matching the model to the actual stackup, materials, and manufacturing limits. Combining simulation with DRC checks and prototype testing helps ensure reliable, manufacturable PCB designs. PCB simulation is the practice of predicting how......
EMC Design for PCB: EMI, EMS, Testing Standards & Compliance Guide
Key Takeaways EMC design means controlling both EMI (unwanted emissions) and EMS (immunity to external disturbances); a board that meets emission limits but resets during an ESD test has not achieved EMC. Every interference problem can be analyzed with the source–path–victim model, and solved by reducing the source, interrupting the path, or hardening the victim. Core PCB techniques include minimizing current-loop area, maintaining continuous reference planes, controlling impedance, decoupling power p......
How to Choose and Place Decoupling Capacitors for PCB Design
Every digital PCB depends on decoupling capacitors, yet a surprising number of boards still suffer from voltage dips, glitches, and electromagnetic interference (EMI) issues caused by one simple mistake: incorrect placement or selection. This guide walks through what decoupling capacitors do, how to choose the right value, where to place them, and which layout mistakes to avoid, so your next board runs clean on the first try. Key Takeaways Place one decoupling capacitor near each IC's power pin. Use 1......
Effective Solutions to Reduce PCB Ground Loop Noise
Key Takeaways Cause: Multiple ground paths with voltage differences cause hum, ADC errors, and EMI. Strategy: Use star grounding for <1 MHz; use solid ground planes for >10 MHz. Routing: Never route fast traces across split planes to avoid large return loops. Mitigation: Use isolation, differential pairs, and place GND vias/caps close to IC pins. Stackup: Use thinner prepreg to lower return loop inductance. A ground loop occurs when multiple grounds form a closed conductive path, allowing unwanted ele......