PCB - JLC3DP Q&A
Are component pads PTH by default on fabrication? I have a two sided board and have many unconnected pads on top layer. Si......
is it possible to get a PCB manufactured that is 3.6mm thick?
Hi there! We need conformal coating on our next PCB, but we need to mask out buttons, connectors and a diagonally placed b......
Hello, For a project I need an FR4 PCB with a hexagonal pattern of large holes(~20mm) closely packed together like in this......
I already have a panel made of 8 round pcb. Now I would like to make a production of 50 panel. I have BOM data for the sin......
Hi JLCPCB, Would it be possible to merge two different accounts? For instance, if I had an old account that I used in the ......
For flex PCB i was wondering if it was possible to have multiple stiffeners under a PCB, a FR4 stiffener and a 3M Tape sti......
Are footprints for 0.35mm pin pitch parts (pad size 0.8x0.2mm with 0.15mm spacing or 0.875x0.15mm with 0.2mm spacing) supp......
Hello when i chose the stackup JLC08081H-1080B , it doesnt show the dielectric paramerters(Dk , Loss tangent...) , and tha......
Hi all, where can I found the dimension of vias / annular ring that I can use in a 3oz PCB? BR, Dario
I have read some articles about FPC additional fee charging cases, and I saw that multiple designs on one board require ad......
Hello , My PCB has two seperated circuits in the same panel. How much will cost for a v-cut to seperate them? I only menti......
I have been using the epoxy cap and filled option on my boards, which applies to all the vias on the board. How do we spec......
I want to change the username of my account. How can I do it?
I'd like to know if and how I can either combine multiple seperate PCBs in EasyEda into a single Gerber or how I can uploa......
Hi, what is the minimum gap between two slots in pcb that you recommend?
I have a IC with a large contact pad underneath it. The IC will consume a lot of power during operation, so it's highly de......
- 1
- 2
- 3
- 4
- 5
- 6
- 17