PCB - JLC3DP Q&A
Can I order a PCB, SMT stencil and parts to solder it by myself? So not only parts (which is not possible) but in combinat......
My 8-layer PCB vias after review set to 0.2mm and the cost increased, while in my designed PCB file all vias is 0.3 mm. Do......
Seems that you cannot open excellon files. I put .XLN to my excellon files expecting to make them readable with no success
What is the minimum annular ring for a via? I do not see any information about this in your capabilities page.
For a keyboard PCB, I'm using "standard" keyswitch footprints in Kicad, but I'm concerned that holes may be too closely sp......
Is it correct that the copper layer is not exposed in the area where the solder mask layer is removed from the attached pi......
I am inquiring about the possibility of producing a PCB without any solder mask application. For our project, it is essent......
Hello, For simulation purpose I need to specify exact parameters of the PCB. In this case it's about 1.52mm 2 layer PTFE T......
What would be recommended minimum PTH and NPTH hole/drill distance from PCB edge (milled edge, not a v-cut) to avoid manuf......
hello, i see on the capabilities page to mill a slot inside the PCB area say a half circle the std mill size is 1mm ? can ......
Hello For singe layer copper core boards, what is the minimum trace width and the minimum distance between traces ? Thanks
Where can i find a detailed stackup for a 0.4mm 2 layer board? I need it for impedance considerations
Hi! I'd like to add thermal relief vias to a QFN thermal pad, but since epoxy/copper filling is expensive, I want to ask i......
Hello, I have a PCB design that requires very small tht pads (through hole) what is the smallest hole and diameter I can g......
Hello, Do you have the ability to produce 2-layer flex PCB that is 203mm in width and 934mm in height? Thanks, Elaine
Hi! For importing goods to EU in the IOSS mode, the local authorities of Czech Republic require end customers to pair pack......
Hello Can I share collaborate a design with another Hardware Engineer who has another account? Thanks Suresh
The solder mask layer was removed from the Kicad to cover the copper pad part that constitutes the capacitive sensor with ......
Hi! How do I instruct the router to process the board? (Created with Kicad) Can you process it if the instructions are on ......
Hi, I have already given you detail please share quotation with me
- 1
- 8
- 9
- 10
- 11
- 12
- 17