PCB - JLC3DP Q&A
The JLCPCB capabilities page says a NPTH (non-plated through hole) must have a diameter > 0.5mm. However, the drill sizes ......
Hello. I want to produce panel combining routing(milling) and V-scoring. I have used a *.gm1 file for milling and a *.gko ......
Hello. I am currently designing a 4-layer pcb, and I want to calculate trace width and gap for high speed signal, I need J......
my PCB 1-BGA pad 0.26mm dia 2- BGA pad to pad distance 0.14mm 3-via in pad 0.15/0.25mm is this you can easily produce or i......
Hello, I’m working on a project using the ADXL382 from Analog Devices. I used their evaluation board for some tests, but I......
What are the minimum dimensions for a flex pcb design?
Good afternoon - Where can I find information about the temperature handling capability of your FR4 and solder mask materi......
I'd like to have NPTH countersunk holes on my PCB. Is it possible to make a PCB with countersunk holes? If possible, how c......
When milling a slot, what are the available knife sizes? 0.8mm possible, but discouraged 1.0mm possible 1.6mm good yield 2......
We are interested in having cards manufactured by your company. Could you kindly provide detailed information regarding yo......
Hello, I want to order 10 PCBs, but do we have problems with customs with a basket amount of $47.25? I need to provide thi......
Rather than the 'Instant Quote', is it possible to generate a downloadable quote document for a given PCB design?
Hi. I hope you are well. Do the photo`s specifications, thicknesses and Dk coefficients comply with the JLC04161H-7628 sta......
Hey, I'm trying to identify and source the exact board-to-board connector shown in the attached images. The connector is m......
Hello! I see that I am unable to route out a BGA 0.5mm pitch device using the default DRC rules in EasyEDA. Is there anyth......
HI, I see nothing about back drilling. Can you do this. This effectively removes the stub on a thru via
I would like to know if header pins could be installed onto my pcb board after print? If yes, how do I go about that pleas......
When is JLCONE app available for download at mobile and windows? is there any specific time frame for it? SIncerely, Pyry
Can i cancel the payment if i accidentally submit an order?
Is it possible to make a multi layer PCB which has some pads with plated through holes, and some pads with non-plated thro......
- 1
- 2
- 3
- 4
- 5
- 6
- 17