This website requires JavaScript.
Coupons
Ship to

PCB - JLC3DP Q&A

Mu board design is irregular in shape. How much extra does that cost?

My board, approx 33x20mm is shaped as a rectangle with a triangular section missing. Is there a cost per liner mm of cut, ......

1 Reply Asked by 91*******9A
Clearance Between PCB Traces and Pins – Minimum Safe Distance

Hello, I have designed a PCB where the clearance between traces and pins is 0.2mm (200µm). I would like to confirm if this......

1 Reply Asked by 90*******6A
About outline layers when using Protel99SE

I am writing an outline in KeepOutLayer, but the preview in the Gerber viewer does not seem to reflect this. I have also p......

1 Reply Asked by 96*******5A
Pads Enig and HASL surface finish

is it possible have the pads with Enig surface finish on th bottom and HASL on the Top, on the same PCB?

1 Reply Asked by 93*******6A
Flex PCB for directly soldering to another board

Hello, is it possible manufacture golden fingers on flexible pcb for directly soldering to another board? Sample in pictur......

1 Reply Asked by 26*******9A
Face detector

Want a face detector pcb with components

1 Reply Asked by 95*******4A
Graving a burnt PCB

Good evening, Can you tell me if it's possible to send you a PCB with burnt but still visible traces (sending a single-lay......

1 Reply Asked by 25*******2A
1.8mm thickness

I would like to make the thickness of the PCB 1.8mm.

1 Reply Asked by 69*******7A
What is the breakdown voltage of the dielectric in a JLCPCB aluminum PCB?

We are planning to use a 1mm thick aluminium PCB as a thermal spacer between Mosfets and heatsink in a mains powered inver......

1 Reply Asked by 61*******2A
1 Reply Asked by 30*******9A
0.5mm pitch BGA - how to setup for manufacturing in KiCad

Hello, in our application we use 0.5mm pitch BGA package. I read this article https://jlcpcb.com/help/article/BGA-Design-G......

1 Reply Asked by 72*******9A
minimum distance between hole of a via to round pad

For my project I'm using a component the T8F81C2 which has which is a 81-FPGA (5 x 5), here they recommend using pad sizes......

1 Reply Asked by 33*******2A
untented vias and HASL

Hi! What happens to untented vias (0.3mm drill, 1mm-thick 2-sided board) or open vias in pads when the board goes through ......

1 Reply Asked by 80*******7A
What is Your IPC Grade Standard for Rigid Circuit Boards?

Hello, On your blog, you have a page specifying that you adhere to IPC-6013 Class 2 for Flexible Circuit Boards: https://a......

1 Reply Asked by 25*******0A
PCB Oblong hole error

Hi Sir I was received the ordered 2 kind of sample PCBs. Thanks greatly for fast delivery and cheap price. But, there are ......

1 Reply Asked by 94*******9A
Press Fit Holes and File Upload

Hello, I saw you can do a press fit hole with 0.05mm tolerance. I will need that done for the next board I am doing. Where......

1 Reply Asked by 43*******3A
Flex Gold fingers with notches

Hello, Amphenol 59453 (SFVL) series require locking notches like these. Can you manufacture these?

1 Reply Asked by 26*******6A
Minimum spacing between electrical conduction tracts and heatsink pads on copper core PCBs

The minimum spacing for traces is 0.1mm. How much space must there be between a heatsink pad on copper core PCBs and a “no......

1 Reply Asked by 84*******0A
3D Barcode from batch to batch

If I want a repeat order, how do I amend the unique number inside the 3D barcode?

1 Reply Asked by 22*******0A
PCB outline bit size

Hi - I'd like to put some fine details on my board outline. What is the router bit size used to cut the board outline for ......

1 Reply Asked by 26*******2A
  • 1
  • 5
  • 6
  • 7
  • 8
  • 9
  • 17