PCB - JLC3DP Q&A
Hello, This is Junki Kim, an intern at the Korea Institute of Science and Technology (KIST). I would like to ask about the......
Dear all, How can I define a V-cut in a Kicad 9 project? Best regards and thank you for your attention, Manuel Ferreira
I have a X1002WVS-03L-HF-LPSN on my board. What is the mating connector? Even better is if there is a mating connector and......
Hello, I am looking for the 94V-0 fire rating certificate
My project has hidden and blind transitions between layers, can you make such a board? Or do you only make through holes i......
A PCB Gerber was submitted recently and I noticed that there was an upcharge because the board was larger than normal. Wha......
I am designing a board that will be attached to a metal backplate using M2.5 bolts through PTHs (2.7 mm to 3.0 mm in diame......
Hello I need ENEPIG gold plating on the Rogers board. Can you make it?
Is the JLC04161H-2116D 4-layer stack-up option no longer available?
Do you have a detailled stack-up of a standard 4-Layer FR4 1.6mm PCB? I could not find it on your website.
https://www.youtube.com/watch?v=5V7dXCTpLK0 HOW CAN I MAKE THE RADIO PCB GERBER IN THIS VIDEO
Hii. Can i pay in chinese yuan for prototype pcb ? If yes, how can i do that ?
Hello, I am about to send a manufacturing request for a PCB I designed in Altium which includes internal power planes. Pla......
I understand that JLCPCB only offers 1-layer aluminum PCB's, however, I am curious to know if you can apply 1mm vias from ......
Are your boards Conflict Mineral Compliant? If so, are there documents to prove this? Thank you.
Hello, I use KiCAD to design my PCB boards, and in parts of my design, the silkscreen overlaps with the copper pads. But K......
I wish to stack 2 x C3001542 using your footprint RJ45-TH_HYCW61-RJ45-152B How close can I physically have them together s......
I purchased $23 worth of boards and until recently, had much cheaper shipping options. After temporary tariff changes in a......
- 1
- 4
- 5
- 6
- 7
- 8
- 17