PCB - JLC3DP Q&A
Is it possible to create a company account that more than one person can login to? We have multiple engineers who use JLC,......
We need to manufacture 4 layer Rigid PCB with 2mm thickness and Inner and Outer layer copper thickness is 2 Oz. Can i keep......
I intend to order a PCB to use as front panel. I would need 8mm holes for potentiometer shafts. In your capabilities page ......
Hello. i have a pcb that I would like to clone. Could you make the pcb just by having the front and back photo of the pcb?
Hello! I'm designing an 8-layer PCB with impedance control. I'd like to know the 8-layer stackup you offer, since in the w......
If we can't do blind vias, only PTH in four-layer boards. How can the mid layers of the board be connected?
Hi, What type of shipment should I choose for shipment to EU with duty paid? Regards Henrik
How do I replace wrong gerber datas in running process? I received a mail, that there is a lost of solder mask. Order hsit......
For a multi-layer board, can I specify the thickness of inner layers?
Dear support team, con you make the PCB (4-6 layers) with BGA footprint as follows: Pitch 0.4 mm Pad diameter 0.25mm Via/H......
Hi, can ODB++ files be used to order PCBs or Gerber only? We have a customer who only exports their manifacturing data as ......
Hi, I want to make a PCB with 2.0mm thickness, that contains a lot of cutouts (refer to the image). Q1: what is the minimu......
It would be our intention to make an aluminum pcb so that all plated vias have a complete electrical connection with the a......
To the person in charge Could you show me how to generate gerber data in "CR-8000 Design Force" ?
If a buyer purchases several PCB prototypes from you, and one of them is ready for shipment before the others, how is ship......
When making a PCB using Aluminum base, what is the typical thickness of the thermal insulation layer between the copper an......
In a 2 layer flex pcb, is the stiffener internal to the two PCB layers?
Does JLCPCB have a solution to add a sequencing serial number to PCB production?
- 1
- 12
- 13
- 14
- 15
- 16
- 17