This website requires JavaScript.
Coupons
Ship to

PCB - JLC3DP Q&A

Minimising delamination risk on flex PCBs with a copper plane layer

Can one of the layers on a flex PCB be made as a completely solid copper plane without risking delaminiation problems due ......

1 Reply Asked by 28*******1A
How do I specify a counterbore hole in a PCB?

Hello, how do I specify a counterbore hole in the gerber files of a PCB? Counterbore hole, as described in: https://jlcpcb......

1 Reply Asked by 28*******4A
Mistakes in impedance controlled stackup data

I have noticed some errors in your impedance controlled stackup data. JLC04201H-1080 has exclamation points instead of num......

1 Reply Asked by 28*******1A
Surface roughness profile for multi-layer PCBs

What is the surface roughness of the copper laminate used in impedance controlled NP-155F (Tg155) multi-layer PCBs? I woul......

1 Reply Asked by 28*******1A
1 Reply Asked by 90*******4A
UL Certification on Plastic Material

Hi, My company is trying to pass certification with our product and it requires UL certification on plastic material used ......

1 Reply Asked by 63*******4A
Platinenbestellung

There is a circuit board in the shopping cart, but the summary still says zero euros. When I go to Secure Payment, this me......

1 Reply Asked by 49*******4A
Inquiry About Minimum Order Quantity for Metal PCB

Dear JLCPCB, I am planning to order metal PCBs with a thickness of 1.6T. The details of my order are as follows: Size: 475......

1 Reply Asked by 39*******6A
1 Reply Asked by 90*******8A
Stiffner layer in Eagle

When designing the PCB in Eagle, which layer represents the stiffener ? I picked the layer 103 - Stiffener, but it did not......

1 Reply Asked by 81*******6A
Warpage board - IPC

Which IPC standard do you use to determine the maximum allowable warpage board without surface mount components?

1 Reply Asked by 23*******8A
In Eagle, why do drill holes scale up 10x?

Why do the drill holes scale up using the Eagle CAM processor? I read the following advisory note: "Start from Eagle 7.2 t......

1 Reply Asked by 64*******0A
CADSTAR .spl

CADSTAR .spl files can be used as input ?

1 Reply Asked by 28*******5A
Vias for use under a big module such as ESP32

When using a bigger module like the ESP32 on a two layer board the ground cannot be easily connected directly because the ......

1 Reply Asked by 89*******1A
Is PCB for WLP or WLCSP package ICs can be fabricated at JLCPCB?

Hi, Is PCB for WLP/WLCSP package ICs, such as STM32F051T8Y6TR, can be fabricated? I know 0.28mm pad is acceptable but have......

1 Reply Asked by 55*******3A
Board cutout

Hello, which layer should be used for board cutouts? Thank you, Thomas

1 Reply Asked by 63*******3A
pre-design cercit

can you provide a pre disine dsp sine wave ips cercit

1 Reply Asked by 30*******6A
FPC design file

I want to make a single layer FPC with different direction contact. (Reverse direction FPC) If I use single copper layer a......

1 Reply Asked by 33*******0A
1 Reply Asked by 75*******5A
Sharing my PCB design so others can order?

Can I share my PCB design so that someone else can order it from their account?

2 Replies Asked by 83*******6A
  • 1
  • 7
  • 8
  • 9
  • 10
  • 11
  • 17