This website requires JavaScript.
Coupons
Ship to

Large Board Surcharge - What are the maximum dimensions

Large Board Surcharge - What are the maximum dimensions
Large Board Surcharge - What are the maximum dimensions

26*******0A

2025-04-30 04:27 AM

A PCB Gerber was submitted recently and I noticed that there was an upcharge because the board was larger than normal.

What is the maximum dimension of the board at which point a 'Large Board Surcharge' is added?

The PCB was a typical 1.6mm thick, 4-layer, 1oz ENIG and I never saw this charge before.


Tony