How Operational Amplifiers Work: Four Essential Op-Amp Circuits Explained
6 min
- 1. What Makes Op-Amps Good at Math?
- 2. Op-Amp as an Adder (Summing Amplifier)
- 3. Op-Amp as a Subtractor (Differential Amplifier)
- 4. Op-Amp as an Integrator
- 5. Op-Amp as a Differentiator
- 6. Comparison Table of the Four Configurations
- 7. Factors to Consider in PCB Design
- Conclusion:
As we discussed in the first article of the series, Operational amplifiers (op-amps) aren’t just about amplifying signals; they’re called operational amplifiers for a reason. Back in the early days of analog computers, op-amps were literally used to perform mathematical operations like addition, subtraction, integration, and differentiation. Fast forward to today, we don’t solve calculus homework with op-amps anymore (thankfully), but these same principles power audio mixers, filters, and signal processing circuits. Digital circuits have some limitations related to operating frequency and all. But analog systems are real-time and fast; people nowadays want to go back to analog computing because digital electronics have almost reached their peak. In this article, we’ll explore four classic op-amp applications:
● Adder (Summing Amplifier)
● Subtractor (Differential Amplifier)
● Integrator
● Differentiator
1. What Makes Op-Amps Good at Math?
The secret is negative feedback. When used with resistors (and sometimes capacitors), op-amps manipulate input signals into predictable output expressions. We have full control over the output because we have full control over the variables.
● Adder/Subtractor: A weighted resistor network can be made to combine two signals to add or subtract them.
● Integrator: A capacitor in the feedback path makes the output proportional to the integral of the input.
● Differentiator: A capacitor at the input makes the output proportional to the derivative of the input.
But in the digital world, the task becomes complicated because a large number of bits are involved, and we need ADC and DAC to convert the signal back into the original format. This does nothing but increases the overall complexity of the block.
2. Op-Amp as an Adder (Summing Amplifier)
The summing amplifier combines multiple input signals into one output. Its essentially an inverting amplifier with multiple inputs. At the circuit level, what we do is:
Connect each input voltage (V1, V2, V3…) through a resistor (R1, R2, R3…) to the inverting input. The non-inverting input of the operational amplifier is grounded. A feedback resistor (Rf) sets the scaling of the overall signal. And we will get the overall equation as:
If all input resistors are equal (R1 = R2 = R3), the output is simply the negative sum of inputs. And all this finds applications in circuits like:
● Audio mixing consoles (adding multiple signals).
● Digital-to-analog converters (weighted sum).
3. Op-Amp as a Subtractor (Differential Amplifier)
A subtractor outputs the difference between two input voltages. This is the basis for differential amplifiers. Both inputs are used, one at the inverting terminal, one at the non-inverting. Resistor ratios are used to control the gain.
The operational amplifier itself is a differential amplifier, but it can only produce a differential output if connected in the open loop, as we know from the first article of this series - OPAMP: 101. By the way, using this type of configuration, we can easily subtract two signals. Some of the applications can be found in:
● Instrumentation amplifiers (when cascaded).
● Data acquisition systems (ADC front-ends).
4. Op-Amp as an Integrator
The integrator produces an output proportional to the time integral of the input, effectively summing the input over time. Input goes to the inverting terminal through a resistor (R). A capacitor (C) is placed in the feedback path, and the non-inverting input is grounded. The circuit is something similar to a low-pass filter, which is quite popular. But there is a condition when the circuit works as an integrator: “A Low-Pass Filter (LPF) behaves like an integrator when the input signal frequency is much higher than the filter's cutoff frequency.” Otherwise, we have the same LPF-type action. Some applications of this type of circuit are in:
● Waveform generation (turning square waves into triangular).
● Analog computing and signal processing.
Pure integrators can drift due to DC offsets. Designers often add a resistor in parallel with the capacitor for stability.
5. Op-Amp as a Differentiator
The differentiator outputs the time derivative of the input signal, highlighting how fast it changes. The input signal passes through a capacitor (C) to the inverting input. And a resistor (Rf) is used in the feedback path. It is the application circuit of a high-pass filter. Just keep the input signal frequency much lower than the cutoff frequency to keep the circuit working as a differentiator. Some of the applications include:
● Edge detection (digital signal transitions).
● Control systems (rate-of-change detectors).
Differentiators amplify noise at high frequencies. To fix this, engineers often add small resistors and capacitors for stability and noise reduction.
6. Comparison Table of the Four Configurations
7. Factors to Consider in PCB Design
Because these options are not available directly inside a system like the digital one, we need a board (PCB) to create the system, and at the system level, due to parasitics and non-linear effects, we may get some errors that we should take care of:
● Component Tolerances: Resistors and capacitors are essential for accurate math operations.
● Power Supply: Most of them require dual-rail power we should take care of both supplies when connecting the power.
● Stability: Add small compensation capacitors to avoid oscillations; this is often necessary for integrator and differentiators to ensure stability.
● Noise Considerations: Keep traces short, use ground planes, and decouple power rails with capacitors.
● Bandwidth: Choose op-amps with sufficient Gain Bandwidth Product (GBW) to cover the operating frequency range.
Conclusion:
In the second article of the series, we have seen that the Op-amps aren't just amplifiers. These are the analog workhorses that can do math for you. By simply arranging resistors and capacitors, you can turn an op-amp into:
● An Adder (to sum signals).
● A Subtractor (to measure differences).
● An Integrator (to accumulate signals over time).
● A Differentiator (to measure how fast signals change).
All students should be aware of this type of configuration of the OPAMP. These circuits show the power of negative feedback and component ratios. These will remain practical building blocks for mixers, filters, ADC front ends, and control systems.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
• Design Guidelines for PCB Using FR4 Substrates
Keep Learning
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......
A Practical Guide to Circuit Design from Concept to PCB
Key Takeaways Define clear circuit requirements and select suitable components based on electrical ratings, performance, and availability. Follow a structured design workflow from schematic capture and simulation to PCB layout and validation. Optimize component placement, routing, power distribution, and signal integrity to improve circuit performance. Apply DFM guidelines and complete ERC/DRC checks to prevent design errors and ensure smooth PCB manufacturing. Choose appropriate PCB materials, layer ......
PCB Silkscreen: All You Need to Know
Key Takeaways The PCB Silkscreen Guide demonstrates that a properly designed legend layer is essential to prevent assembly failures and ensure long-term hardware reliability. By mastering modern manufacturing methodologies like Direct Legend Printing (DLP) and aligning layouts with JLCPCB's strict DFM design rules—including the absolute 0.8 mm character height limit and the automated 0.15 mm silkscreen clipping protocol driven by solder mask precedence—engineers can seamlessly eliminate cold joints an......
The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
Note Need a quick reference while reading schematics? Download our free, printable Circuit Symbols Cheat Sheet (PDF), featuring the most common IEC and ANSI symbols organized by category. Keep it on your desktop or print it for easy reference at your workbench. ⬇ Download the Free Circuit Symbols Cheat Sheet (PDF) Every electronic diagram is written in a visual language, and circuit symbols are its alphabet. From your first electrical schematic to a multi-layer board, knowing circuit symbols can make ......
Understanding Electrical Schematics: A Comprehensive Guide
Key Takeaways Schematics vs. Block Diagrams: Schematics detail exact components and connections; block diagrams only show high-level functions. Mark Polarity: Essential to prevent circuit failure and automated SMT placement errors at JLCPCB. Clean Layout: Use modular blocks and net labels (VIN, GND) to eliminate visual clutter. Manufacturing Ready: Follow DFM trace rules and export standard Gerber, BOM (LCSC C-IDs), and CPL files. Fast Troubleshooting: Isolate schematic blocks to test expected voltage......
PCB Board Design: A Step-by-Step Guide for Beginners
Key Takeaways This PCB Design Guide offers beginners a practical step-by-step approach to designing a compact 3A IP2312 lithium battery charger PCB — an upgraded alternative to the popular TP4056 module. It focuses on key techniques like schematic creation, optimized layout, proper trace routing for 3A current, and ground planes to build efficient and reliable boards. Printed Circuit Boards (PCBs) form the backbone of most modern electronic devices, providing a platform to connect electronic component......