Comparing High-Density PCB Stack-Up With Normal PCB
6 min
- What Is PCB Stack-Up?
- What Makes a PCB High-Density?
- Normal PCB Stack-Up Explained
- Key Differences Between HDI and Normal PCB Stack-Up
- Advantages of High-Density PCB Stack-Up
- Design Considerations for Engineers and Students
- Conclusion
High-density printed circuit boards (PCBs)are not the same as simple PCBs. Do you know what the difference is? PCBs with a larger number of layers and a higher density of traces are known as HDIs. These are not as common because they are not used in small prototypes or hobby work, but for more professional application. One of the best examples of an HDI board with a complex stack-up that you can see—or might have—is the motherboard of your PC. HDI changes the story completely when it comes into the picture, a multilayer PCB with a proper stack-up. In this article, we are going to discuss the stack-up/layers used in HDI vs normal PCB boards.
What Is PCB Stack-Up?
A PCB stack-up is the ordered arrangement of board layers and materials. It typically includes copper signal layers, dielectric layers (prepreg and cores), internal ground or power planes, and mechanical thickness specifications. Not all layers arefor routing but to provide better signal or power integrity to the board. The stack-up determines:
- Controlled impedance behavior of the traces
- Crosstalk and return paths
- Power distribution (plane continuity)
- Thermal performance and mechanical rigidity
- Manufacturing complexity and cost
Accurate design of stack-up is key in high-speed circuits, RF systems, power distribution, and thermal management. Poor stack-up optimization commonly leads to signal reflections, EMI issues, thermal stress, and manufacturing defects.
What Makes a PCB High-Density?
An HDI PCB augments routing density and enhances electrical performance with the help of advanced features like:
Microvias: Tiny vias that are laser-drilled in pads, connecting adjacent layers without taking up much space. These vias are not through holes but for signal transition from one layer to another.
Finer traces and spaces: We will see with this PCB design narrower-than-average trace and space widths, often going below 4 mil. Because Due to multiple layers and prepreg, impedance must be calculated accordingly; consult the manufacturer for specifics.
Thinner cores and prepregs: Enabling shorter via aspect ratios and better impedance control. The layer count can go up to 24 starting from 8-layer boards. Standard FR4 is not typically used at this layer count due to the signal degradation issues.
Sequential lamination: Having sequentially laminated stacks permits microvia stacks where microvias can be staggered. It also greatly simplifies the routing of complex structures in several layers.
More microvias and less space result in lower latency and superior return management, which makes HDI perfectly suited for devices such as smartphones, wearables, RF modules, and compact computers.
Normal PCB Stack-Up Explained
A standard PCB stack-up, which we see in traditional design and fabrication, includes:
- Through-hole vias that run the full board thickness.
- Wider traces and spacing, compatible with standard fabrication tolerances.
- Layer counts of 1–6, though larger boards with through-hole vias still fall into this category.
- FR-4 substrates, which have standard dielectric thicknesses.
These boards are very robust, economical, and have strong manufacturer support. They are the preferred choice for low to medium-speed digital circuits, power electronics, and many industrial applications.
Key Differences Between HDI and Normal PCB Stack-Up
| Feature | HDI PCB Stack-Up | Normal PCB Stack-Up |
|---|---|---|
| Layer Count & Thickness | Higher density with thinner cores; stacked microvias allow compact routing | Fewer layers, thicker dielectrics; cost grows linearly with layer count |
| Via Structures | Microvias (blind, buried, stacked) minimize space and parasitics | Through-hole vias take up more area and lengthen signal paths |
| Signal Integrity | Shorter interconnects, controlled impedance, lower EMI | Adequate for many designs, but longer traces can cause reflections |
| Fabrication Complexity | Requires laser drilling, sequential lamination, and microvia filling | Simpler processes, faster, and cheaper to fabricate |
| Thermal/Mechanical | Thinner materials reduce stiffness; thermal vias must be carefully designed | Thicker cores, predictable heat dissipation |
| Typical Applications | Mobile devices, RF, high-speed computing | Industrial, power electronics, cost-driven designs |
Advantages of High-Density PCB Stack-Up
Among the perks of HDIs, a high-density PCB stack-up is the possibility of miniaturization. This advantage enables the development of more compact devices while ensuring high functionality. Also, since the interconnects and controlled impedance paths are shorter in HDI, signal integrity is also improved. Issues such as crosstalk and signal reflection are reduced. Microvias also improve layout flexibility by routing around dense ball grid array (BGA) packages and other fine-pitch components.
In most practical scenarios, a standard PCB stack-up is advantageous, particularly in terms of cost. The ability to fabricate and test standard boards is far more cost-effective than other options in terms of pricing. Furthermore, these boards fit perfectly within a wide variety of control systems and other industrial electronics.
Design Considerations for Engineers and Students
When comparing HDI vs normal PCB, consider:
Signal speed and integrity: HDI is better suited for designs operating above 1 GHz or with high data rates.
Board size: HDI is preferred in designs when size is critical.
Thermal needs: Normal PCBs with thick copper do, in fact, do better for power-heavy designs.
Cost vs volume: HDI is the way to go for mass-produced consumer electronics; for prototypes or industrial boards, normal PCBs are the way to go.
Repairability: With HDI boards, you do struggle with rework, so you need to design for testability.
Conclusion
Opting for a dense PCB stack-up versus a standard PCB stack-up is a question of balancing density with performance, cost, and manufacturability. HDI is unparalleled in miniaturization and signal performance. Conversely, normal PCBs are practical, robust, and economical for a wide range of uses. Some of these are listed below:
Smartphones and tablets: Rely on HDI for multi-layer routing of BGAs and high-speed buses.
IoT and RF modules: Benefit from short, impedance-controlled RF paths in small spaces.
Industrial electronics: Continue to use normal stack-ups for power management and rugged control systems.
What is very important or useful for students and engineers is that the board stack-up design must be tailored to the project at hand, which includes signal velocity, cooling, some of the units, and economic outlay. Early input from manufacturers is important in the development of a reliable design that offers stable performance and practicality.
Keep Learning
How Stacked Vias Enable Higher Density and Better Performance in HDI PCBs
Key Takeaways Stacked vias are a critical technology that enables higher routing density and superior performance in HDI PCBs. By vertically aligning microvias in a single column, often combined with via-in-pad designs, they dramatically reduce breakout area, shorten signal paths, lower parasitic inductance, and improve thermal conductivity compared to traditional staggered vias. While requiring precise sequential lamination, via filling, and strict design rules, stacked vias help designers reduce lay......
HDI PCB vs Standard PCB: Key Differences and Benefits
Printed Circuit Boards (PCBs) constitute the core of any electronic system and provide mechanical and electrical connections to other electronic components. They are in the cars we drive, the capsules we open, and in what we put inside them, and use them in planes and rockets, with ever more unique aerospace solutions. Let’s face it: traditional PCB boards have served as an industry standard for decades; However, the need for smaller, faster products has sparked the rise of High-Density Interconnect (......
Comprehensive Guide to HDI PCBs: Design, Advantages, and Applications
Key Takeaways Core HDI Limits: Standard HDI uses 3/3 mil trace/space and 4 mil laser microvias for optimal yield and density. Via-in-Pad Benefits: Resin-filled microvias on SMT pads (JLCPCB's FPOV) eliminate fan-out and prevent solder wicking. Smart Stack-ups: Symmetrical 1+N+1 or 2+N+2 staggered microvias cut lamination costs and thermal stress. High Density Interconnect (HDI) printed circuit boards (PCBs) are circuit boards with a higher wiring density per unit area than traditional PCBs. HDI PCBs h......
Stack-Up Strategies for Effective HDI PCB Design
Whether you believe Moore's Law is dead or alive, the strong economic incentive to pack more processing power into ever smaller form factors is unlikely to abate any time soon. With the entry of the HDI stackup—a technology at the cutting edge of multilayer PCB design that promises to help PCB designers make smaller complex boards for years to come. The stack-up in a printed circuit board (PCB) design is a critical element that influences the board's performance, manufacturability, and reliability. In......
How to Optimize Layer Stack-Up in HDI PCB Boards
With the introduction of the HDI stackup, a cutting-edge technique in multilayer PCB design, PCB designers should be able to create increasingly complex, smaller boards in the years to come. Establishing your project's needs precisely is the first step in designing a PCB stackup. Determining the number of layers required is the first stage; this depends on the circuit's complexity, signal density, power distribution requirements, and if the design calls for RF or high-speed signals. In the late 1980s,......
High-Density Interconnect (HDI): Revolutionizing PCB Design for Modern Electronics
In the world of advanced electronics, High-Density Interconnect (HDI) technology has become a game-changer. As devices get smaller, faster, and more complex, traditional printed circuit boards (PCBs) often face limitations in handling these demands. That’s where HDI PCBs come into play. This article covers what HDI is, why it’s critical, and how it’s shaping the future of modern electronics. What is High-Density Interconnect (HDI)? A "HDI" printed circuit board (PCB) is one type whose wire count per u......