Q&A Community - JLC3DP
What is the dimension unit you recommend for 3D printing files ?
I have a board which is 16*25 mm, however, in production (100pcs), the minimum size is 70*70 mm. By itself, the jlcpcb cal......
What are the maximum and minimum machining sizes for CNC ?
Hi, what is the thickness of your different anodizing coating ?
Hi, is it possible to tap the small holes in the CNC machined part with M3 threads?
Hello! I'm designing an 8-layer PCB with impedance control. I'd like to know the 8-layer stackup you offer, since in the w......
What is the difference between the surface finish option “Yes-Sanding-General sanding” and “No” when I use your SLA resins......
Do you have any waterproof 3D printing materials ?
I want to 3D print my case. This case is put on outdoors 3-6 hours a day. Do you have any idea of UV resistant material ?
Hello JLCPCB, I'm just wondering if you guys offer multicolored 3d printing at all. Because I am making a 3d model of a ch......
What is the Layer Height for you SLA 3D Printers? Specially for the printer that is assigned to print the 8111X Resin(has ......
How can I order 3D prints with a 135MB file ? Because I noticed that your max supported file size is 80MB.
I would like to test your 3D printing service, can I get some coupons ?
I do not have a 3D file, but only a PDF drawing, can I also get a 3D quotation ?
Good morning, i have made an order using Parts order about Global sourcing parts. Now i have to order a Standard PCBA, i h......
If we can't do blind vias, only PTH in four-layer boards. How can the mid layers of the board be connected?
Hi, What type of shipment should I choose for shipment to EU with duty paid? Regards Henrik
How do I replace wrong gerber datas in running process? I received a mail, that there is a lost of solder mask. Order hsit......
For a multi-layer board, can I specify the thickness of inner layers?
- 1
- 22
- 23
- 24
- 25
- 26
- 30