This website requires JavaScript.
Coupons
Ship to

Q&A Community - JLC3DP

Combine orders

can i combine a pcb order with component order from LCSC?

1 Reply Asked by 26*******4A
Tapered Traces

Greetings, Are you capable of printing tapered traces? Thank you in advance!

1 Reply Asked by 81*******8A
add another board

i have placed an order and already pay for it it still in production i want to add another board and add it to the deliver......

1 Reply Asked by 31*******4A
PCB - Surface Finish

PCB : FR-4 “Can you work without PCB surface finishing?” NO HASL NO LeadFree HASL NO ENIG

1 Reply Asked by 50*******9A
custom svg image as stencil

Can custom SVG image be used as stencil, like image bellow. If i create such a design and export to gerber file will the l......

1 Reply Asked by 25*******7A
1 Reply Asked by 73*******6A
1 Reply Asked by 73*******6A
via-in-pad on flex pcb

is it possible to do via in pad on a flex pcb? https://jlcpcb.com/blog/704-jlcpcb-free-via-in-pad

1 Reply Asked by 69*******7A
What is the dielectric constant for the FR-4

What is the dielectric constant or relative permittivity for the FR-4 material used in JLC's 1 oz, 2 layer PCB?

1 Reply Asked by 80*******9A
PCB data sheet

Hello, For our CE certificates, we need the data sheet of all the components. Can you provide it for PCB? The data needed:......

1 Reply Asked by 22*******5A
Aluminium Stackup Values

Hello, I am working on a LED project which is locate on an aluminium plate. I couldn't find the layer stack values for Alt......

1 Reply Asked by 80*******2A
Gerber file requirements

Hello, I exported the gerber files from my EM solver. It is an RF design. It seems there is a problem with it. I can not s......

1 Reply Asked by 30*******1A
Print size inquiry

What is the maximum size of a model that can be printed?

1 Reply Asked by 51*******7A
After PCBA, PCB can not be soldered. Not solderable.

I used PCBA service only for R,C components, not for ICs. The problem is that I can not solder ICs onto the PCB which is p......

1 Reply Asked by 33*******0A
1 Reply Asked by 73*******6A
THT pcb assembly

Hello, I have a PCB design that I would like to print that has both SMD and THT components. Are you able to accomodate tho......

1 Reply Asked by 79*******6A
Assembly capabilities

Can you assemble boards with surface mount components on both sides ?

1 Reply Asked by 74*******4A
Is there a way for more than one user to work on a PCB project together?

Is there a way for more than one user to work on a PCB project together? e.g. Engineer user submits the PCB designs, while......

1 Reply Asked by 81*******2A
Assembly of different variants

Can you assemble two different variants of the same PCB in one order? Example: I order 30 PCBs with ten 0402 solder pads I......

1 Reply Asked by 62*******9A
business clearance codes

Hello, I would like business clearance on my next order. Does your company accept the business clearance code from Korea C......

1 Reply Asked by 35*******3A
  • 1
  • 15
  • 16
  • 17
  • 18
  • 19
  • 30