Q&A Community - JLC3DP
In KiCad 8, let's say I draw a square outline on the Edge.Cuts layer to define the shape of my PCB. If I want to create an......
Hello! Is it critical if silkscreen printing in gerber files lies on top of copper pads and vias? thanks for the answer!
There are also deliveries in Angola and how can I make one in my country?
Is the minimum via hole size/diameter the finished hole size or drill size, and after plating the finished hole size will ......
In an aluminum PCB, is it possible to use through-hole connectors to connect them to the copper layer, or would they short......
Dear JLCPCB, I am using your online Impedance calculator but still have some confusion: - My application involves a standa......
I want to use 3.2 mm board mounting holes as tooling holes for the solder stencil for my own manual assembly. My first att......
Hello, I would like to know if paste files of panels (Panel by JLCPCB) are sent by mail automatically after ordering ? If ......
hello, I see that the minimum clearance via to via (same nets) is 0.254 mm. And the minimum clearance between "holes" from......
I have a range of .STL &.STEP files, I want to print 10 .stl PA12 nylon and 13 .step ledo6060 resin and how do I combine t......
Can you tap threads on 3D printed 316L parts ?
What is your layer height when printing 316L parts? Can I specify layer height 0.025mm ?
What is the density of your SLM parts?
What are the advantages of SLM printing?
What is the applications of Nylon PA12?
Do you know vapor smoothing process, and if you have that service for your PA12 nylon parts or not?
What is your 3D printing tolerances?
Can FDM models be smoothed and then painted?
Do you have any environmentally friendly 3D printing material?
- 1
- 18
- 19
- 20
- 21
- 22
- 30