This website requires JavaScript.
Coupons
Ship to
Blog

Basic Bridge Circuits

Published Feb 17, 2025, updated Sep 19, 2026

11 min

Table of Contents
  • High-Precision PCB Design Considerations for Bridge Circuits
  • FAQ about Basic Bridge Circuits
  • Conclusion

Key Takeaways

  • Core Principle: Bridge circuits (Wheatstone, Kelvin, H-Bridge, etc.) enable high-precision measurements and power control.
  • Applications: Essential for sensor signal conditioning, AC/DC rectifiers, and motor drivers.
  • JLCPCB Optimization: Maximize circuit stability with JLCPCB’s 3/3 mil traces, 4-layer stackups, and High-TG FR-4.

A bridge circuit splits an input voltage into two paths, compares the voltages across different branches, and provides an output. These circuits are widely valued for their accuracy and versatility in comparing, balancing, or measuring electrical properties. These circuits find applications in sensing, calibration, and even filtering. They consist of a combination of four resistive, capacitive, or inductive elements arranged in a quadrilateral (bridge-like) structure depending upon measuring application. Bridge circuits may be drawn in schematic form in an H-shape or in a diamond shape, although the diamond configuration is more common.

The voltage source powering the bridge circuit is called the excitation source. This source may be DC or AC depending on the application of the bridge circuit. Bridge circuits, first invented in the early 19th century by Samuel Hunter Christie, have been pivotal in technological advancements, from measuring unknown electrical resistances to enabling advanced sensors today. Bridge circuits are used extensively in both the laboratory and industry, these circuits stand testament to the fundamental principles of electrical engineering. Let's dive deep into understanding bridge circuits. See, how the bridges are implemented in a circuit schematics with other components.

Types of Basic Bridge Circuits:

Bridge circuits have remained at the forefront of electrical measurement techniques for generations. Universally acknowledged for their precision and versatility, various topologies cater to specific measurement needs. Here is an overview of the top 10 types of bridge circuits widely used in modern electronics:

1. Wheatstone Bridge:

This bridge is fundamentally a diamond configuration of four resistors and used to measure unknown resistances. When balanced, the ratio of two adjacent resistors equals the ratio of the other two, allowing for the determination of an unknown resistance. In this way if three resistance values are known, a fourth unknown resistance value can be obtained. It finds extensive use in labs for accurate resistance measurements and in industries where sensors change resistance based on some physical parameters.

Wheatstone Bridge

It has applications in strain gauges for mechanical measurements and resistance thermometers for temperature measurement. For example: A strain gauge mounted on a mechanical structure detects deformation by changing its resistance. The Wheatstone Bridge converts this resistance change into a measurable voltage.  

2. Kelvin Bridge:

Similar to the Wheatstone bridge, the Kelvin bridge is specifically designed to measure low resistances (typically below 1 Ω) with exceptional accuracy. By incorporating a four-terminal (Kelvin) sensing configuration, it eliminates errors introduced by lead and contact resistance.

PCB Layout & JLCPCB Manufacturing Tip: When implementing a Kelvin sensing bridge on a PCB, trace resistance can easily distort measurement results (1 oz copper thin trace has ~0.5 mΩ/sq resistance). Designers must route separate Force (Current) and Sense (Voltage) lines directly from the current-shunt or sensing component. JLCPCB's precision PCB manufacturing supports minimum trace width/spacing down to 3/3 mil (0.075mm) and outer copper weights up to 2 oz, ensuring low thermal noise and tight parasitic control for high-precision Kelvin bridge designs.

Kelvin Bridge

3. Maxwell Bridge:

It is used for measurement of unknown inductance. It is given by James C. Maxwell, this bridge specializes in evaluating unknown inductances using known capacitances and resistances. The bridge is balanced by varying resistance and capacitance until the detector shows no deflection. It's particularly adept at measuring inductors with medium quality factors, ranging between 1 and 10.

Maxwell Bridge

4. Hay Bridge:

Hay's bridge is an enhanced version of Maxwell’s bridge, specifically designed for more accurate inductance measurements, especially in cases where the inductor's quality factor is high. This bridge is optimal for high-quality factor inductors, typically those exceeding a factor of 10.

Hay Bridge

5. Schering Bridge:

It is used for measurement of unknown capacitance and dielectric loss. The Schering bridge is vital for high-frequency applications. In a common configuration, a known capacitor and a resistor are connected in series in one arm, while an unknown capacitor and its parallel resistor are placed in another. This arrangement is widely used in capacitor manufacturing for quality checks and in laboratories for precise capacitance measurements.

Schering Bridge

6. AC Bridges:

Used for measuring complex quantities like inductance, capacitance, and impedance. They operate with alternating current and are essential for high-frequency applications.

For example:  A Wien bridge circuit is used for accurate measurement of capacitance in terms of frequency and resistance. It is also used for measuring audio frequencies. It balances when the impedance ratio in one leg matches the other leg's ratio.

7. Diode Bridge:

A diode bridge (or bridge rectifier) uses four diodes in a bridge topology to convert alternating current (AC) into direct current (DC), maintaining a single output polarity regardless of the input AC polarity. Because the active diode pair generates heat under continuous forward current, real-world AC/DC power supply layouts require effective thermal management around the component pads. Designing with wider copper pours, thermal via arrays, or utilizing JLCPCB's 2 oz thick copper and aluminum substrates helps maintain low operating temperatures and extends long-term circuit reliability.

Diode Bridge

8. H Bridge:

An H-bridge circuit uses four switching elements (such as MOSFETs or BJTs) to reverse the current direction through a load, enabling precise bidirectional speed and direction control for DC motors and inverters. High-frequency PWM switching in an H-bridge can generate severe voltage spikes and electromagnetic interference (EMI) due to stray loop inductance. To mitigate this, PCB designers must minimize the current loop area between switching elements and decoupling capacitors—a task easily optimized by using a JLCPCB 4-layer stackup with dedicated internal ground planes for low-impedance current return paths.

H Bridge

9. Fontana Bridge:

The Fontana bridge is an active circuit that integrates a resistive bridge with operational amplifiers to build a wide-frequency-band voltage-to-current converter, preserving impedance balance across broad frequency ranges. Because high-frequency active bridges are exceptionally sensitive to stray parasitic capacitance, maintaining symmetrical signal routing and short trace lengths is essential to prevent operational amplifier instability. Implementing precise 3/3 mil trace/space routing and an ENIG (Electroless Nickel Immersion Gold) surface finish through JLCPCB ensures tight physical matching and flat pad surface planarity for high-precision active bridge designs.

Fontana Bridge

It is commonly employed in testing and calibrating capacitors, offering high sensitivity and reliability. The circuit’s design allows it to handle both high-precision measurements and low-loss capacitor testing. Its versatility makes it a valuable tool in advanced electronics testing.

10. Carey Foster Bridge:

A Carey Foster bridge circuit is used to measure tiny differences between two large resistances to calculate low resistances. It is particularly useful for determining the unknown resistance of wires or components by comparing them with a known standard resistor. The circuit achieves accuracy by balancing the bridge through a null method, eliminating errors from wire resistances in the setup.

Carey Foster Bridge

Collectively, these bridge circuits underline the importance of precise measurements in electrical engineering, each serving a distinct purpose to cater to a myriad of applications.

Why Are Bridge Circuits Important?

Bridge circuits offer exceptional accuracy by nullifying external influences when balanced. Their advantages include:  

1. Precision in Measurement: Essential for laboratory and industrial applications.  

2. Dynamic Range: Can handle low and high electrical properties.  

3. Flexibility: By adjusting components, bridge circuits can measure different parameters.  

4. Simplicity: Despite their effectiveness, the design is straightforward and easily adaptable.

Applications of Bridge Circuits

Bridge circuits have a vast range of applications in electronics, including:  

  • Sensing and Instrumentation: Used in strain gauges, thermistors, and piezoelectric sensors.  
  • Electrical Testing: Capacitance and resistance calibration.  
  • Signal Conditioning: Filtering and signal comparison.  
  • AC/DC Conversions: Used in rectifiers for converting alternating to direct current.  
  • Inductor and Capacitor Testing: Bridges like Maxwell and Schering are widely used in laboratories.  

High-Precision PCB Design Considerations for Bridge Circuits

Designing high-accuracy bridge circuits extends beyond schematic equations; physical PCB layout plays a crucial role in eliminating parasitic interference, thermal drift, and signal degradation. Key layout guidelines aligned with JLCPCB manufacturing capabilities include:

1. Thermal Symmetry & Seebeck Effect:

In Wheatstone strain gauge bridges, uneven thermal distribution across resistors induces thermoelectric voltages (Seebeck Effect). Resistors should be placed in close thermal proximity with symmetrical copper pour patterns. Utilizing JLCPCB's High-TG FR-4 materials (TG170) minimizes thermal expansion and thermal-coefficient of resistance (TCR) drift.

2. Differential Routing & Controlled Impedance:

For AC bridges (such as Maxwell or Schering bridges), parasitic capacitance between traces can imbalance the bridge at high frequencies. Differential signal pairs ($V_{out}$) must be routed symmetrically with matched trace lengths. JLCPCB provides free impedance control calculations and tight manufacturing tolerances (±10% impedance control) to ensure signal fidelity.

3. HDI Technology and Via-in-Pad for Compact Sensor Nodes:

Modern sensor bridges require miniaturized signal chains. Using JLCPCB High-Density Interconnect (HDI) technology with laser-drilled microvias (min. 0.1mm via diameter) and Via-in-Pad (POFV) process, engineers can place precision 0201/0402 bridge resistors directly over ground plane vias without solder wicking issues, drastically reducing loop inductance.

Table: Precision Bridge Circuit Layout Requirements vs. JLCPCB Manufacturing Capabilities

Bridge Circuit Design RequirementKey Impact FactorJLCPCB Process Capabilities
Kelvin 4-Wire SensingIsolation of parasitic resistance between force and sense lines3/3 mil (0.075 mm) min line width/spacing, up to 2 oz outer copper weight
High-Frequency AC Bridge Impedance MatchingUnbalance caused by parasitic capacitance and inductanceSupports 1+N+1 / 2+N+2 HDI structures, multi-layer controlled impedance tolerance within ±10%
Thermal Drift & Seebeck Effect ControlSubstrate Coefficient of Thermal Expansion (CTE) and non-uniform thermal distributionHigh-TG FR-4 (TG170) and Aluminum substrates with superior thermal dissipation
Precision SMT Assembly for Micro Components (0201/0402)Pad planarity and solder wicking on viasENIG (Electroless Nickel Immersion Gold) surface finish, Via-in-Pad (POFV) with resin plugging & copper capping
Ready to Bring Your PCB Ideas to Life?

Turn designs into working hardware with expert fabrication, assembly, and component services from a trusted industry leader. Upload your files, choose your options, and get boards that are ready to test, ready to ship, and ready to scale.

Get Free Quote >

FAQ about Basic Bridge Circuits

Q: What is the main difference between a Wheatstone bridge and a Kelvin bridge?

While both measure resistance, a Wheatstone bridge is designed for medium to high resistance values. A Kelvin bridge uses a 4-terminal (Kelvin) sensing configuration specifically to measure low resistances (under 1 Ω) by eliminating errors caused by lead and contact resistance.

Q: How does PCB thermal management affect Wheatstone strain gauge accuracy?

Temperature gradients across bridge resistors cause resistance imbalance due to Thermal Coefficient of Resistance (TCR) drift and unwanted thermoelectric voltages (Seebeck Effect). Placing resistors in thermal symmetry and using High-TG FR-4 materials (like JLCPCB’s TG170) minimizes measurement errors caused by heat.

Q: Why is a 4-layer PCB stackup recommended for H-bridge motor driver circuits?

High-frequency switching in H-bridges generates stray loop inductance and EMI noise. A 4-layer PCB stackup with a dedicated internal ground plane provides a short, low-impedance current return path, significantly reducing voltage ringing and EMI.

Q: Can JLCPCB handle impedance control for high-frequency AC bridge designs?

Yes. High-frequency AC bridges (such as Maxwell or Schering bridges) require precise differential signal pair impedance matching. JLCPCB provides free impedance calculation tools and tight manufacturing tolerances (±10%) across multi-layer stackups and HDI structures.

Q: Which surface finish is best for precision bridge circuits with micro SMD components?

ENIG (Electroless Nickel Immersion Gold) is ideal. It provides a flat, coplanar surface for precise soldering of high-density Op-Amps and tight-tolerance (0.1%) SMD resistors, preventing tilting or tombstoning during SMT assembly.

Conclusion

Bridge circuits form the backbone of precision measurements and signal processing in electronics. From the Wheatstone Bridge for resistance measurement to the Schering Bridge for capacitance testing, their diversity and utility are unparalleled. Understanding the fundamentals of bridge circuits empowers engineers and technicians to implement accurate and reliable systems across various fields. Whether you're a student, a hobbyist, or a professional, mastering bridge circuits is an essential step in exploring the world of electronics.  

Keep Learning