3D Printing - JLC3DP Q&A
Hello, I wonder how do I find or create models to 3D print? Thanks in advance!
Please explain what oil spraying is. Is it adding a clear coat? Is it vapor smoothing? Is it adding a layer of resin?
How strong are the parts made with SLM technique and your 316L steel? Please provide Yield Strength and Tensile strength
What is the dimension unit you recommend for 3D printing files ?
What is the difference between the surface finish option “Yes-Sanding-General sanding” and “No” when I use your SLA resins......
Do you have any waterproof 3D printing materials ?
I want to 3D print my case. This case is put on outdoors 3-6 hours a day. Do you have any idea of UV resistant material ?
Hello JLCPCB, I'm just wondering if you guys offer multicolored 3d printing at all. Because I am making a 3d model of a ch......
What is the Layer Height for you SLA 3D Printers? Specially for the printer that is assigned to print the 8111X Resin(has ......
How can I order 3D prints with a 135MB file ? Because I noticed that your max supported file size is 80MB.
I would like to test your 3D printing service, can I get some coupons ?
I do not have a 3D file, but only a PDF drawing, can I also get a 3D quotation ?
Can you print multiple parts in 1 file ? I would like to do some prototypes.
Hi, what would be the maximum overhang angle for avoiding support ?
Hi, what is the infill percentage of your FDM printing ?
can you suggest a software I can use for 3D printing
Hello, is there a glossy polish as an option for your 316L metal ?
Do I have to add printing support when using your SLA ?
Hi, I got some files ready for 3D printing, but some of them have thinner walls than your minimum requirement, can they al......
- 1
- 2
- 3
- 4
- 5
- 6
- 7